MSCEMLIB
Detailed Description
Memory System Controller API.
Contains functions to control the MSC, primarily the Flash. Users can perform Flash memory write and erase operations, as well as optimization of the CPU instruction fetch interface for the application. Available instruction fetch features depends on the MCU or SoC family, but features such as instruction pre-fetch, cache, and configurable branch prediction are typically available.
- Note
 - Flash wait-state configuration is handled by CMU module. When core clock configuration is changed by a call to functions such as CMU_ClockSelectSet() or CMU_HFRCOBandSet() , then Flash wait-state configuration is also updated.
 
MSC resets into a safe state. To initialize the instruction interface to recommended settings:
- Note
 - The optimal configuration is highly application dependent. Performance benchmarking is supported by most families. See MSC_StartCacheMeasurement() and MSC_GetCacheMeasurement() for more details.
 
Support for Flash write and erase runs from RAM by default. This code may be allocated to Flash by defining EM_MSC_RUN_FROM_FLASH .
- Note
 - Flash erase may add ms of delay to interrupt latency if executing from Flash.
 
Flash write and erase operations are supported by MSC_WriteWord() , MSC_WriteWordFast(), MSC_ErasePage() , and MSC_MassErase() . Fast write is not supported for EFM32G and mass erase is supported for MCU and SoC families with larger Flash sizes.
- Note
 - MSC_Init() must be called prior to any Flash write or erase operation.
 
The following steps are necessary to perform a page erase and write:
         Data Structures | 
       |
| struct | MSC_ExecConfig_TypeDef | 
         Macros | 
       |
| #define | EM_MSC_RUN_FROM_FLASH | 
| 
         By compiling with define EM_MSC_RUN_FROM_FLASH, functions performing erase or write operations will remain in and execute from Flash. This is useful for targets that don't want to allocate RAM space to hold the flash functions. Without this define, code for Flash operations will be copied into RAM at startup.
          | 
       |
| #define | MSC_EXECCONFIG_DEFAULT | 
| #define | MSC_PROGRAM_TIMEOUT 10000000ul | 
| 
         Timeout used while waiting for Flash to become ready after a write. This number indicates the number of iterations to perform before issuing a timeout.
          | 
       |
| #define | MSC_RAMFUNC_DECLARATOR | 
| 
         Expands to
         
          SL_RAMFUNC_DECLARATOR
         
         if
         
          EM_MSC_RUN_FROM_FLASH
         
         is undefined and to nothing if
         
          EM_MSC_RUN_FROM_FLASH
         
         is defined.
          | 
       |
| #define | MSC_RAMFUNC_DEFINITION_BEGIN | 
| 
         Expands to
         
          SL_RAMFUNC_DEFINITION_BEGIN
         
         if
         
          EM_MSC_RUN_FROM_FLASH
         
         is undefined and to nothing if
         
          EM_MSC_RUN_FROM_FLASH
         
         is defined.
          | 
       |
| #define | MSC_RAMFUNC_DEFINITION_END | 
| 
         Expands to
         
          SL_RAMFUNC_DEFINITION_END
         
         if
         
          EM_MSC_RUN_FROM_FLASH
         
         is undefined and to nothing if
         
          EM_MSC_RUN_FROM_FLASH
         
         is defined.
          | 
       |
         Enumerations | 
       |
| enum | 
         
          MSC_Status_TypeDef
         
         {
          mscReturnOk = 0, mscReturnInvalidAddr = -1, mscReturnLocked = -2, mscReturnTimeOut = -3, mscReturnUnaligned = -4 }  | 
       
         Functions | 
       |
| void | MSC_Deinit (void) | 
| 
         Disables the flash controller for writing.
          | 
       |
| __STATIC_INLINE void | MSC_EnableAutoCacheFlush (bool enable) | 
| 
         Enable or disable instruction cache flushing when writing to flash.
          | 
       |
| __STATIC_INLINE void | MSC_EnableCache (bool enable) | 
| 
         Enable or disable instruction cache functionality.
          | 
       |
| __STATIC_INLINE void | MSC_EnableCacheIRQs (bool enable) | 
| 
         Enable or disable instruction cache functionality in IRQs.
          | 
       |
| MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_ErasePage (uint32_t *startAddress) | 
| 
         Erases a page in flash memory.
          | 
       |
| void | MSC_ExecConfigSet ( MSC_ExecConfig_TypeDef *execConfig) | 
| 
         Set the MSC code execution configuration.
          | 
       |
| __STATIC_INLINE void | MSC_FlushCache (void) | 
| 
         Flush contents of instruction cache.
          | 
       |
| __STATIC_INLINE int32_t | MSC_GetCacheMeasurement (void) | 
| 
         Stops measuring hit rate.
          | 
       |
| void | MSC_Init (void) | 
| 
         Enables the flash controller for writing.
          | 
       |
| __STATIC_INLINE void | MSC_IntClear (uint32_t flags) | 
| 
         Clear one or more pending MSC interrupts.
          | 
       |
| __STATIC_INLINE void | MSC_IntDisable (uint32_t flags) | 
| 
         Disable one or more MSC interrupts.
          | 
       |
| __STATIC_INLINE void | MSC_IntEnable (uint32_t flags) | 
| 
         Enable one or more MSC interrupts.
          | 
       |
| __STATIC_INLINE uint32_t | MSC_IntGet (void) | 
| 
         Get pending MSC interrupt flags.
          | 
       |
| __STATIC_INLINE uint32_t | MSC_IntGetEnabled (void) | 
| 
         Get enabled and pending MSC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
          | 
       |
| __STATIC_INLINE void | MSC_IntSet (uint32_t flags) | 
| 
         Set one or more pending MSC interrupts from SW.
          | 
       |
| MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_MassErase (void) | 
| 
         Writes data to flash memory. This function is faster than
         
          MSC_WriteWord()
         
         , but it disables interrupts. Write data must be aligned to words and contain a number of bytes that is divisible by four.
          | 
       |
| __STATIC_INLINE void | MSC_StartCacheMeasurement (void) | 
| 
         Starts measuring cache hit ratio.
          | 
       |
| MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_WriteWord (uint32_t *address, void const *data, uint32_t numBytes) | 
| 
         Writes data to flash memory. This function is interrupt-safe, but slower than MSC_WriteWordFast(), which writes to flash with interrupts disabled. Write data must be aligned to words and contain a number of bytes that is divisible by four.
          | 
       |
Macro Definition Documentation
| #define EM_MSC_RUN_FROM_FLASH | 
By compiling with define EM_MSC_RUN_FROM_FLASH, functions performing erase or write operations will remain in and execute from Flash. This is useful for targets that don't want to allocate RAM space to hold the flash functions. Without this define, code for Flash operations will be copied into RAM at startup.
- Note
 - This define is not present by default. The MSC controller API will run from RAM by default.
 
        Definition at line
        
         125
        
        of file
        
         em_msc.h
        
        .
       
| #define MSC_EXECCONFIG_DEFAULT | 
Default MSC ExecConfig initialization.
        Definition at line
        
         162
        
        of file
        
         em_msc.h
        
        .
       
| #define MSC_PROGRAM_TIMEOUT 10000000ul | 
Timeout used while waiting for Flash to become ready after a write. This number indicates the number of iterations to perform before issuing a timeout.
- Note
 - Timeout is set very large (in the order of 100x longer than necessary). This is to avoid any corner case.
 
        Definition at line
        
         110
        
        of file
        
         em_msc.h
        
        .
       
Referenced by MSC_ErasePage() .
Enumeration Type Documentation
| enum MSC_Status_TypeDef | 
Return codes for writing/erasing Flash.
        Definition at line
        
         133
        
        of file
        
         em_msc.h
        
        .
       
Function Documentation
| __STATIC_INLINE void MSC_EnableAutoCacheFlush | ( | bool | 
           
            enable
           
           | 
          ) | 
Enable or disable instruction cache flushing when writing to flash.
- Parameters
 - 
         
[in] enableEnable automatic cache flushing. Default is on.  
        Definition at line
        
         436
        
        of file
        
         em_msc.h
        
        .
       
References _MSC_READCTRL_AIDIS_SHIFT , BUS_RegBitWrite() , and MSC .
| __STATIC_INLINE void MSC_EnableCache | ( | bool | 
           
            enable
           
           | 
          ) | 
Enable or disable instruction cache functionality.
- Parameters
 - 
         
[in] enableEnable instruction cache. Default is on.  
        Definition at line
        
         412
        
        of file
        
         em_msc.h
        
        .
       
References _MSC_READCTRL_IFCDIS_SHIFT , BUS_RegBitWrite() , and MSC .
| __STATIC_INLINE void MSC_EnableCacheIRQs | ( | bool | 
           
            enable
           
           | 
          ) | 
Enable or disable instruction cache functionality in IRQs.
- Parameters
 - 
         
[in] enableEnable instruction cache. Default is on.  
        Definition at line
        
         424
        
        of file
        
         em_msc.h
        
        .
       
References _MSC_READCTRL_ICCDIS_SHIFT , BUS_RegBitWrite() , and MSC .
| MSC_RAMFUNC_DEFINITION_BEGIN MSC_Status_TypeDef MSC_ErasePage | ( | uint32_t * | 
           
            startAddress
           
           | 
          ) | 
Erases a page in flash memory.
- Note
 - It is recommended to run this code from RAM. On the Gecko family, it is required to run this function from RAM.
 
For IAR IDE, Rowley IDE, SimplicityStudio IDE, Atollic IDE, and ARM GCC IDE, this is achieved automatically by using attributes in the function proctype. For Keil uVision IDE, define a section called "ram_code" and place this manually in the project's scatter file.
- Parameters
 - 
         
[in] startAddressA pointer to the flash page to erase. Must be aligned to the beginning of the page boundary.  
- Returns
 - 
         Returns the status of erase operation,
         
          MSC_Status_TypeDef
         
         
* mscReturnOk - The operation completed successfully. * mscReturnInvalidAddr - The operation tried to erase a non-flash area. * mscReturnLocked - The operation tried to erase a locked area of the flash. * mscReturnTimeOut - The operation timed out waiting for the flash operation * to complete. *
 
        Definition at line
        
         975
        
        of file
        
         em_msc.c
        
        .
       
References _EMU_STATUS_VSCALE_MASK , _EMU_STATUS_VSCALEBUSY_MASK , EMU , EMU_STATUS_VSCALE_VSCALE2 , FLASH_PAGE_SIZE , MSC , MSC_PROGRAM_TIMEOUT , MSC_STATUS_BUSY , MSC_STATUS_INVADDR , MSC_STATUS_LOCKED , MSC_WRITECMD_ERASEPAGE , MSC_WRITECMD_LADDRIM , MSC_WRITECTRL_WREN , mscReturnInvalidAddr , mscReturnLocked , mscReturnOk , and mscReturnTimeOut .
Referenced by nvm3_halPageErase() , and NVMHAL_PageErase() .
| void MSC_ExecConfigSet | ( | MSC_ExecConfig_TypeDef * | 
           
            execConfig
           
           | 
          ) | 
Set the MSC code execution configuration.
- Parameters
 - 
         
[in] execConfigThe code execution configuration.  
        Definition at line
        
         291
        
        of file
        
         em_msc.c
        
        .
       
References _MSC_READCTRL_MODE_MASK , MSC_ExecConfig_TypeDef::aiDis , MSC_ExecConfig_TypeDef::iccDis , MSC_ExecConfig_TypeDef::ifcDis , MSC , MSC_READCTRL_AIDIS , MSC_READCTRL_ICCDIS , MSC_READCTRL_IFCDIS , MSC_READCTRL_MODE_WS0 , MSC_READCTRL_MODE_WS1 , MSC_READCTRL_PREFETCH , MSC_READCTRL_SCBTP , MSC_READCTRL_USEHPROT , MSC_ExecConfig_TypeDef::prefetchEn , MSC_ExecConfig_TypeDef::scbtEn , and MSC_ExecConfig_TypeDef::useHprot .
| __STATIC_INLINE int32_t MSC_GetCacheMeasurement | ( | void | 
           
           
           | 
          ) | 
Stops measuring hit rate.
- Note
 - 
         Defined inline to minimize the impact of this code on the measurement itself. Only works for relatively short sections of code. To measure longer sections of code, implement an IRQ Handler for the CHOF and CMOF overflow interrupts. These overflows need to be counted and included in the total. Functions can then be implemented as follows:
         
* volatile uint32_t hitOverflows * volatile uint32_t missOverflows * * void MSC_IRQHandler(void) * { * uint32_t flags; * flags = MSC->IF; * if (flags & MSC_IF_CHOF) { * MSC->IFC = MSC_IF_CHOF; * hitOverflows++; * } * if (flags & MSC_IF_CMOF) { * MSC->IFC = MSC_IF_CMOF; * missOverflows++; * } * } * * void startPerformanceCounters(void) * { * hitOverflows = 0; * missOverflows = 0; * * MSC_IntEnable(MSC_IF_CHOF | MSC_IF_CMOF); * NVIC_EnableIRQ(MSC_IRQn); * * MSC_StartCacheMeasurement(); * } * 
- Returns
 - Returns -1 if there has been no cache accesses. Returns -2 if there has been an overflow in the performance counters. If not, it will return the percentage of hits versus misses.
 
        Definition at line
        
         366
        
        of file
        
         em_msc.h
        
        .
       
References MSC , MSC_CACHECMD_STOPPC , MSC_IF_CHOF , and MSC_IF_CMOF .
| void MSC_Init | ( | void | 
           
           
           | 
          ) | 
Enables the flash controller for writing.
- Note
 - This function must be called before flash operations when AUXHFRCO clock has been changed from a default band.
 
        Definition at line
        
         225
        
        of file
        
         em_msc.c
        
        .
       
References _EMU_STATUS_VSCALE_MASK , _EMU_STATUS_VSCALEBUSY_MASK , CMU_ClockFreqGet() , cmuClock_AUX , EMU , EMU_STATUS_VSCALE_VSCALE2 , MSC , MSC_UNLOCK_CODE , and MSC_WRITECTRL_WREN .
Referenced by nvm3_halOpen() , and NVMHAL_Init() .
| __STATIC_INLINE void MSC_IntClear | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Clear one or more pending MSC interrupts.
- Parameters
 - 
         
[in] flagsPending MSC intterupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).  
        Definition at line
        
         213
        
        of file
        
         em_msc.h
        
        .
       
References MSC .
| __STATIC_INLINE void MSC_IntDisable | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Disable one or more MSC interrupts.
- Parameters
 - 
         
[in] flagsMSC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).  
        Definition at line
        
         226
        
        of file
        
         em_msc.h
        
        .
       
References MSC .
| __STATIC_INLINE void MSC_IntEnable | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Enable one or more MSC interrupts.
- Note
 - Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using MSC_IntClear() prior to enabling the interrupt.
 
- Parameters
 - 
         
[in] flagsMSC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).  
        Definition at line
        
         244
        
        of file
        
         em_msc.h
        
        .
       
References MSC .
| __STATIC_INLINE uint32_t MSC_IntGet | ( | void | 
           
           
           | 
          ) | 
Get pending MSC interrupt flags.
- Note
 - The event bits are not cleared by the use of this function.
 
- Returns
 - MSC interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
 
        Definition at line
        
         260
        
        of file
        
         em_msc.h
        
        .
       
References MSC .
| __STATIC_INLINE uint32_t MSC_IntGetEnabled | ( | void | 
           
           
           | 
          ) | 
Get enabled and pending MSC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
 - Interrupt flags are not cleared by the use of this function.
 
- Returns
 - 
         Pending and enabled MSC interrupt sources. The return value is the bitwise AND of
         
- the enabled interrupt sources in MSC_IEN and
 - the pending interrupt flags MSC_IF
 
 
        Definition at line
        
         279
        
        of file
        
         em_msc.h
        
        .
       
References MSC .
| __STATIC_INLINE void MSC_IntSet | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Set one or more pending MSC interrupts from SW.
- Parameters
 - 
         
[in] flagsMSC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).  
        Definition at line
        
         295
        
        of file
        
         em_msc.h
        
        .
       
References MSC .
| MSC_RAMFUNC_DEFINITION_END MSC_RAMFUNC_DEFINITION_BEGIN MSC_Status_TypeDef MSC_MassErase | ( | void | 
           
           
           | 
          ) | 
Writes data to flash memory. This function is faster than MSC_WriteWord() , but it disables interrupts. Write data must be aligned to words and contain a number of bytes that is divisible by four.
- Note
 - It is recommended to erase the flash page before performing a write. It is required to run this function from RAM on parts that include a flash write buffer.
 
For IAR IDE, Rowley IDE, SimplicityStudio IDE, Atollic IDE, and ARM GCC IDE, this is done automatically by using attributes in the function proctype. For Keil uVision IDE, define a section called "ram_code" and place this manually in the project's scatter file.
- Parameters
 - 
         
[in] addressA pointer to the flash word to write to. Must be aligned to words. [in] dataData to write to flash. [in] numBytesA number of bytes to write from the Flash. NB: Must be divisible by four.  
- Returns
 - 
         Returns the status of the write operation.
         
* flashReturnOk - The operation completed successfully. * flashReturnInvalidAddr - The operation tried to erase a non-flash area. * flashReturnLocked - The operation tried to erase a locked area of the flash. * flashReturnTimeOut - The operation timed out waiting for flash operation * to complete. Or the MSC timed out waiting for the software to write * the next word into the DWORD register. *
 
Erase the entire Flash in one operation.
- Note
 - This command will erase the entire contents of the device. Use with care, both a debug session and all contents of the flash will be lost. The lock bit, MLW will prevent this operation from executing and might prevent a successful mass erase.
 
        Definition at line
        
         1127
        
        of file
        
         em_msc.c
        
        .
       
References MSC , MSC_MASSLOCK_LOCKKEY_LOCK , MSC_MASSLOCK_LOCKKEY_UNLOCK , MSC_STATUS_BUSY , MSC_WRITECMD_ERASEMAIN0 , MSC_WRITECTRL_WREN , and mscReturnOk .
| __STATIC_INLINE void MSC_StartCacheMeasurement | ( | void | 
           
           
           | 
          ) | 
Starts measuring cache hit ratio.
Starts performance counters. It is defined inline to minimize the impact of this code on the measurement itself.
        Definition at line
        
         308
        
        of file
        
         em_msc.h
        
        .
       
References MSC , MSC_CACHECMD_STARTPC , MSC_IF_CHOF , and MSC_IF_CMOF .
| MSC_RAMFUNC_DEFINITION_END MSC_RAMFUNC_DEFINITION_BEGIN MSC_Status_TypeDef MSC_WriteWord | ( | uint32_t * | 
           
            address,
           
           | 
         
| void const * | 
           
            data,
           
           | 
         ||
| uint32_t | 
           
            numBytes
           
           | 
         ||
| ) | 
Writes data to flash memory. This function is interrupt-safe, but slower than MSC_WriteWordFast(), which writes to flash with interrupts disabled. Write data must be aligned to words and contain a number of bytes that is divisible by four.
- Note
 - It is recommended to erase the flash page before performing a write.
 
It is recommended to run this code from RAM. On the Gecko family, it is required to run this function from RAM.
For IAR IDE, Rowley IDE, SimplicityStudio IDE, Atollic IDE, and ARM GCC IDE, this is done automatically by using attributes in the function proctype. For Keil uVision IDE, define a section called "ram_code" and place it manually in the project's scatter file.
This function requires a system core clock at 1 MHz or higher.
- Parameters
 - 
         
[in] addressA pointer to the flash word to write to. Must be aligned to words. [in] dataData to write to flash. [in] numBytesA number of bytes to write from flash. NB: Must be divisible by four.  
- Returns
 - 
         Returns the status of the write operation.
         
* flashReturnOk - The operation completed successfully. * flashReturnInvalidAddr - The operation tried to erase a non-flash area. * flashReturnLocked - The operation tried to erase a locked area of the Flash. * flashReturnTimeOut - The operation timed out waiting for the flash operation * to complete, or the MSC module timed out waiting for the software to write * the next word into the DWORD register. *
 
        Definition at line
        
         1061
        
        of file
        
         em_msc.c
        
        .
       
Referenced by nvm3_halWriteWords() , and NVMHAL_Write() .