CSEN_TypeDef Struct ReferenceDevices > CSEN
CSEN Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32bg13p_csen.h
       
       .
      
      
       #include <
       
     
        efr32bg13p_csen.h
       
       >
      
         Data Fields | 
       |
| __IOM uint32_t | ANACTRL | 
| __IM uint32_t | APORTCONFLICT | 
| __IM uint32_t | APORTREQ | 
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CMPTHR | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | DATA | 
| __IOM uint32_t | DMBASELINE | 
| __IOM uint32_t | DMCFG | 
| __IOM uint32_t | EMA | 
| __IOM uint32_t | EMACTRL | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | PRSSEL | 
| uint32_t | RESERVED0 [2] | 
| __IOM uint32_t | SCANINPUTSEL0 | 
| __IOM uint32_t | SCANINPUTSEL1 | 
| __IOM uint32_t | SCANMASK0 | 
| __IOM uint32_t | SCANMASK1 | 
| __IOM uint32_t | SINGLECTRL | 
| __IM uint32_t | STATUS | 
| __IOM uint32_t | TIMCTRL | 
Field Documentation
| __IOM uint32_t CSEN_TypeDef::ANACTRL | 
Analog Control
        Definition at line
        
         68
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IM uint32_t CSEN_TypeDef::APORTCONFLICT | 
APORT Request Conflict
        Definition at line
        
         61
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
| __IM uint32_t CSEN_TypeDef::APORTREQ | 
APORT Request Status
        Definition at line
        
         60
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
| __IOM uint32_t CSEN_TypeDef::CMD | 
| __IOM uint32_t CSEN_TypeDef::CMPTHR | 
Comparator Threshold
        Definition at line
        
         62
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::CTRL | 
Control
        Definition at line
        
         50
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_Disable() , CSEN_Enable() , CSEN_Init() , CSEN_InitMode() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::DATA | 
Output Data
        Definition at line
        
         55
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_DataGet() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::DMBASELINE | 
Delta Modulation Baseline
        Definition at line
        
         66
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_DMBaselineSet() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::DMCFG | 
Delta Modulation Configuration
        Definition at line
        
         67
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::EMA | 
Exponential Moving Average
        Definition at line
        
         63
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_EMAGet() , CSEN_EMASet() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::EMACTRL | 
Exponential Moving Average Control
        Definition at line
        
         64
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::IEN | 
Interrupt Enable
        Definition at line
        
         74
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_IntDisable() , CSEN_IntEnable() , CSEN_IntGetEnabled() , and CSEN_Reset() .
| __IM uint32_t CSEN_TypeDef::IF | 
Interrupt Flag
        Definition at line
        
         71
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_IntGet() , and CSEN_IntGetEnabled() .
| __IOM uint32_t CSEN_TypeDef::IFC | 
Interrupt Flag Clear
        Definition at line
        
         73
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_IntClear() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::IFS | 
| __IOM uint32_t CSEN_TypeDef::PRSSEL | 
PRS Select
        Definition at line
        
         54
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_Init() , and CSEN_Reset() .
| uint32_t CSEN_TypeDef::RESERVED0[2] | 
Reserved for future use
        Definition at line
        
         70
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
| __IOM uint32_t CSEN_TypeDef::SCANINPUTSEL0 | 
Scan Input Selection 0
        Definition at line
        
         57
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_Init() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::SCANINPUTSEL1 | 
Scan Input Selection 1
        Definition at line
        
         59
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_Init() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::SCANMASK0 | 
Scan Channel Mask 0
        Definition at line
        
         56
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::SCANMASK1 | 
Scan Channel Mask 1
        Definition at line
        
         58
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::SINGLECTRL | 
Single Conversion Control
        Definition at line
        
         65
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IM uint32_t CSEN_TypeDef::STATUS | 
| __IOM uint32_t CSEN_TypeDef::TIMCTRL | 
Timing Control
        Definition at line
        
         51
        
        of file
        
         efr32bg13p_csen.h
        
        .
       
Referenced by CSEN_Init() , and CSEN_Reset() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG13P/Include/
       
efr32bg13p_csen.h