LESENSE_TimeCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE
LESENSE timing control descriptor structure.
       Definition at line
       
        547
       
       of file
       
        em_lesense.h
       
       .
      
      
       #include <
       
     
        em_lesense.h
       
       >
      
         Data Fields | 
       |
| bool | delayAuxStartup | 
| uint8_t | startDelay | 
Field Documentation
| bool LESENSE_TimeCtrlDesc_TypeDef::delayAuxStartup | 
Set to true do delay startup of AUXHFRCO until the system enters excite phase. This will reduce the time AUXHFRCO is enabled and reduce power usage.
        Definition at line
        
         556
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| uint8_t LESENSE_TimeCtrlDesc_TypeDef::startDelay | 
Set number of LFACLK cycles to delay sensor interaction on each channel. Valid range: 0-3 (2 bit).
        Definition at line
        
         550
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_lesense.h