VDAC_OPA_TypeDef Struct ReferenceDevicesDevices > | VDAC
VDAC_OPA VDAC OPA Register
.
       Definition at line
       
        47
       
       of file
       
        efr32bg13p_vdac_opa.h
       
       .
      
      
       #include <
       
     
        efr32bg13p_vdac_opa.h
       
       >
      
         Data Fields | 
       |
| __IM uint32_t | APORTCONFLICT | 
| __IM uint32_t | APORTREQ | 
| __IOM uint32_t | CAL | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | MUX | 
| __IOM uint32_t | OUT | 
| uint32_t | RESERVED0 [1] | 
| __IOM uint32_t | TIMER | 
Field Documentation
| __IM uint32_t VDAC_OPA_TypeDef::APORTCONFLICT | 
Operational Amplifier APORT Conflict Status Register
        Definition at line
        
         49
        
        of file
        
         efr32bg13p_vdac_opa.h
        
        .
       
| __IM uint32_t VDAC_OPA_TypeDef::APORTREQ | 
Operational Amplifier APORT Request Status Register
        Definition at line
        
         48
        
        of file
        
         efr32bg13p_vdac_opa.h
        
        .
       
| __IOM uint32_t VDAC_OPA_TypeDef::CAL | 
Operational Amplifier Calibration Register
        Definition at line
        
         54
        
        of file
        
         efr32bg13p_vdac_opa.h
        
        .
       
| __IOM uint32_t VDAC_OPA_TypeDef::CTRL | 
Operational Amplifier Control Register
        Definition at line
        
         50
        
        of file
        
         efr32bg13p_vdac_opa.h
        
        .
       
| __IOM uint32_t VDAC_OPA_TypeDef::MUX | 
Operational Amplifier Mux Configuration Register
        Definition at line
        
         52
        
        of file
        
         efr32bg13p_vdac_opa.h
        
        .
       
| __IOM uint32_t VDAC_OPA_TypeDef::OUT | 
Operational Amplifier Output Configuration Register
        Definition at line
        
         53
        
        of file
        
         efr32bg13p_vdac_opa.h
        
        .
       
| uint32_t VDAC_OPA_TypeDef::RESERVED0[1] | 
Reserved future
        Definition at line
        
         55
        
        of file
        
         efr32bg13p_vdac_opa.h
        
        .
       
| __IOM uint32_t VDAC_OPA_TypeDef::TIMER | 
Operational Amplifier Timer Control Register
        Definition at line
        
         51
        
        of file
        
         efr32bg13p_vdac_opa.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG13P/Include/
       
efr32bg13p_vdac_opa.h