WDOG_TypeDef Struct ReferenceDevices > WDOG
WDOG Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32bg13p_wdog.h
       
       .
      
      
       #include <
       
     
        efr32bg13p_wdog.h
       
       >
      
         Data Fields | 
       |
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| WDOG_PCH_TypeDef | PCH [2] | 
| uint32_t | RESERVED0 [2] | 
| __IM uint32_t | SYNCBUSY | 
Field Documentation
| __IOM uint32_t WDOG_TypeDef::CMD | 
| __IOM uint32_t WDOG_TypeDef::CTRL | 
Control Register
        Definition at line
        
         50
        
        of file
        
         efr32bg13p_wdog.h
        
        .
       
Referenced by WDOGn_Enable() , WDOGn_Feed() , WDOGn_Init() , and WDOGn_Lock() .
| __IOM uint32_t WDOG_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         61
        
        of file
        
         efr32bg13p_wdog.h
        
        .
       
Referenced by WDOGn_IntDisable() , WDOGn_IntEnable() , and WDOGn_IntGetEnabled() .
| __IM uint32_t WDOG_TypeDef::IF | 
Watchdog Interrupt Flags
        Definition at line
        
         58
        
        of file
        
         efr32bg13p_wdog.h
        
        .
       
Referenced by WDOGn_IntGet() , and WDOGn_IntGetEnabled() .
| __IOM uint32_t WDOG_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         60
        
        of file
        
         efr32bg13p_wdog.h
        
        .
       
Referenced by WDOGn_IntClear() .
| __IOM uint32_t WDOG_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         59
        
        of file
        
         efr32bg13p_wdog.h
        
        .
       
Referenced by WDOGn_IntSet() .
| WDOG_PCH_TypeDef WDOG_TypeDef::PCH[2] | 
PCH
        Definition at line
        
         55
        
        of file
        
         efr32bg13p_wdog.h
        
        .
       
| uint32_t WDOG_TypeDef::RESERVED0[2] | 
Reserved for future use
        Definition at line
        
         57
        
        of file
        
         efr32bg13p_wdog.h
        
        .
       
| __IM uint32_t WDOG_TypeDef::SYNCBUSY | 
Synchronization Busy Register
        Definition at line
        
         53
        
        of file
        
         efr32bg13p_wdog.h
        
        .
       
Referenced by WDOGn_Enable() , WDOGn_Feed() , WDOGn_Init() , and WDOGn_Lock() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG13P/Include/
       
efr32bg13p_wdog.h