You are viewing documentation for version:
5.6
|
5.9
(latest) |
Version History
-
globalScope> Global
_SILICON_LABS_32B_PLATFORM
-
Silicon Labs platform name
-
globalScope> Global
_SILICON_LABS_32B_PLATFORM_1
-
Silicon Labs platform name
-
globalScope> Global
EMU_MemPwrDown
(uint32_t blocks)
-
This function is deprecated, use
EMU_RamPowerDown()
instead which maps a user provided memory range into RAM blocks to power down.
-
globalScope> Global
EMU_UpdateOscConfig
(void)
-
Oscillator status is saved in
EMU_EnterEM2()
and
EMU_EnterEM3()
.
-
globalScope> Global
GPIO_IntConfig
(GPIO_Port_TypeDef port, unsigned int pin, bool risingEdge, bool fallingEdge, bool enable)
-
Deprecated function. New code should use
GPIO_ExtIntConfig()
.
-
Module
INT
-
These functions are deprecated and marked for removal in a later release. Use the
CORE
module instead. See
Porting from em_int
for information on how to convert existing code bases to use
CORE
.
-
globalScope> Global
INT_Disable
(void)
-
Deprecated and marked for removal in a later release. Use new CORE module instead.
-
globalScope> Global
INT_Enable
(void)
-
Deprecated and marked for removal in a later release. Use the new CORE module instead.
-
Module
NVM
-
This driver is deprecated and marked for removal in a later release. New code should use
NVM3
.
-
globalScope> Global
setupSWOForPrint
-
Use
RETARGET_SwoInit
instead
-
globalScope> Global
SLEEP_Init
(SLEEP_CbFuncPtr_t pSleepCb, SLEEP_CbFuncPtr_t pWakeUpCb)
-
New code should use the
SLEEP_InitEx
function for initializing the sleep module.
-
globalScope> Global
UARTDRV_Init
(UARTDRV_Handle_t handle,
UARTDRV_InitUart_t
*initData)
-
Deprecated; Use
UARTDRV_InitUart()
instead.
-
globalScope> Global
USART_InitIrDA
(const
USART_InitIrDA_TypeDef
*init)
-
Deprecated function. New code should use
USARTn_InitIrDA()
. This function uses DEFAULT_IRDA_USART, which unless otherwise specified, is USART0 on most devices, and USART1 on devices that don't have a USART0.
-
globalScope> Global
WDOG_Enable
(bool enable)
-
Deprecated function. New code should use
WDOGn_Enable()
. This function uses
DEFAULT_WDOG
.
-
globalScope> Global
WDOG_Feed
(void)
-
Deprecated function. New code should use
WDOGn_Feed()
. This function uses
DEFAULT_WDOG
.
-
globalScope> Global
WDOG_Init
(const
WDOG_Init_TypeDef
*init)
-
Deprecated function. New code should use
WDOGn_Init()
. This function uses
DEFAULT_WDOG
.
-
globalScope> Global
WDOG_IsEnabled
(void)
-
Deprecated function. New code should use
WDOGn_IsEnabled()
. This function uses
DEFAULT_WDOG
.
-
globalScope> Global
WDOG_IsLocked
(void)
-
Deprecated function. New code should use
WDOGn_IsLocked()
. This function uses
DEFAULT_WDOG
.
-
globalScope> Global
WDOG_Lock
(void)
-
Deprecated function. New code should use
WDOGn_Lock()
. This function uses
DEFAULT_WDOG
.