BCP_Packet Struct ReferenceBSP > API for STKs and WSTKs
BCP Packet Structure - Board controller communication protocol version 2.
Definition at line 90
of file bsp_bcp.h
.
#include <
bsp_bcp.h
>
Data Fields | |
uint8_t | data [BSP_BCP_PACKET_SIZE] |
uint8_t | magic |
uint8_t | payloadLength |
uint8_t | reserved |
uint8_t | type |
Field Documentation
uint8_t BCP_Packet::data[BSP_BCP_PACKET_SIZE] |
BCP Packet Data payload
Definition at line 95
of file bsp_bcp.h
.
Referenced by BSP_BccPacketSend(), BSP_CurrentGet(), and BSP_VoltageGet().
uint8_t BCP_Packet::magic |
Magic - start of packet - must be BSP_BCP_MAGIC
Definition at line 91
of file bsp_bcp.h
.
Referenced by BSP_BccPacketReceive(), and BSP_BccPacketSend().
uint8_t BCP_Packet::payloadLength |
Length of data segment >=0 and <=BSP_BCP_PACKET_SIZE
Definition at line 93
of file bsp_bcp.h
.
Referenced by BSP_BccPacketReceive(), BSP_BccPacketSend(), BSP_CurrentGet(), and BSP_VoltageGet().
uint8_t BCP_Packet::reserved |
Reserved for future expansion
Definition at line 94
of file bsp_bcp.h
.
Referenced by BSP_BccPacketSend().
uint8_t BCP_Packet::type |
Type - packet type
Definition at line 92
of file bsp_bcp.h
.
Referenced by BSP_BccPacketReceive(), BSP_BccPacketSend(), BSP_CurrentGet(), and BSP_VoltageGet().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/hardware/kit/common/bsp/
bsp_bcp.h