MTB_TypeDef Struct ReferenceDevices > EFM32HG_MTB

Definition at line 48 of file efm32hg_mtb.h .

Data Fields

__IOM uint32_t BASE
__IOM uint32_t FLOW
__IOM uint32_t MASTER
__IOM uint32_t POSITION

Field Documentation

__IOM uint32_t MTB_TypeDef::BASE

MTB Trace Base Register

Definition at line 52 of file efm32hg_mtb.h .

__IOM uint32_t MTB_TypeDef::FLOW

MTB Trace Flow Register

Definition at line 51 of file efm32hg_mtb.h .

__IOM uint32_t MTB_TypeDef::MASTER

MTB Trace Control Register

Definition at line 50 of file efm32hg_mtb.h .

__IOM uint32_t MTB_TypeDef::POSITION

MTB Trace Position Register.

Definition at line 49 of file efm32hg_mtb.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32HG/Include/ efm32hg_mtb.h