BURTC_Init_TypeDef Struct ReferenceEMLIB > BURTC

BURTC initialization structure for Series 0 devices.

Definition at line 115 of file em_burtc.h .

#include < em_burtc.h >

Data Fields

uint32_t clkDiv
BURTC_ClkSel_TypeDef clkSel
bool compare0Top
bool debugRun
bool enable
uint32_t lowPowerComp
BURTC_LP_TypeDef lowPowerMode
BURTC_Mode_TypeDef mode
bool timeStamp

Field Documentation

uint32_t BURTC_Init_TypeDef::clkDiv

Clock divider; for ULFRCO 1Khz or 2kHz operation.

Definition at line 121 of file em_burtc.h .

Referenced by BURTC_Init() .

BURTC_ClkSel_TypeDef BURTC_Init_TypeDef::clkSel

Select clock source.

Definition at line 120 of file em_burtc.h .

Referenced by BURTC_Init() .

bool BURTC_Init_TypeDef::compare0Top

Set if Compare Value 0 is also top value (counter restart).

Definition at line 126 of file em_burtc.h .

Referenced by BURTC_Init() .

bool BURTC_Init_TypeDef::debugRun

If true, counter will keep running under debug halt.

Definition at line 119 of file em_burtc.h .

Referenced by BURTC_Init() .

bool BURTC_Init_TypeDef::enable

Enable BURTC after initialization (starts counter).

Definition at line 116 of file em_burtc.h .

Referenced by BURTC_Init() .

uint32_t BURTC_Init_TypeDef::lowPowerComp

Number of least significantt clock bits to ignore in low power mode.

Definition at line 123 of file em_burtc.h .

Referenced by BURTC_Init() .

BURTC_LP_TypeDef BURTC_Init_TypeDef::lowPowerMode

Low power operation mode, requires LFXO or LFRCO.

Definition at line 128 of file em_burtc.h .

Referenced by BURTC_Init() .

BURTC_Mode_TypeDef BURTC_Init_TypeDef::mode

Configure energy mode operation.

Definition at line 118 of file em_burtc.h .

Referenced by BURTC_Init() .

bool BURTC_Init_TypeDef::timeStamp

Enable time stamp on entering backup power domain.

Definition at line 124 of file em_burtc.h .

Referenced by BURTC_Init() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_burtc.h