USB_DeviceDescriptor_TypeDef Struct ReferencePlatform Middleware > USB > USB_COMMON

USB Device Descriptor.

Definition at line 402 of file em_usb.h.

#include <em_usb.h>

Data Fields

uint16_t bcdDevice
 
uint16_t bcdUSB
 
uint8_t bDescriptorType
 
uint8_t bDeviceClass
 
uint8_t bDeviceProtocol
 
uint8_t bDeviceSubClass
 
uint8_t bLength
 
uint8_t bMaxPacketSize0
 
uint8_t bNumConfigurations
 
uint16_t idProduct
 
uint16_t idVendor
 
uint8_t iManufacturer
 
uint8_t iProduct
 
uint8_t iSerialNumber
 

Field Documentation

uint16_t USB_DeviceDescriptor_TypeDef::bcdDevice

Device release number in binary-coded decimal

Definition at line 413 of file em_usb.h.

Referenced by