EBI_TypeDef Struct ReferenceDevices > EFM32LG_EBI

Definition at line 48 of file efm32lg_ebi.h .

Data Fields

__IOM uint32_t ADDRTIMING
__IOM uint32_t ADDRTIMING1
__IOM uint32_t ADDRTIMING2
__IOM uint32_t ADDRTIMING3
__IOM uint32_t CMD
__IOM uint32_t CTRL
__IM uint32_t ECCPARITY
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t NANDCTRL
__IOM uint32_t PAGECTRL
__IOM uint32_t POLARITY
__IOM uint32_t POLARITY1
__IOM uint32_t POLARITY2
__IOM uint32_t POLARITY3
__IOM uint32_t RDTIMING
__IOM uint32_t RDTIMING1
__IOM uint32_t RDTIMING2
__IOM uint32_t RDTIMING3
__IOM uint32_t ROUTE
__IM uint32_t STATUS
__IOM uint32_t TFTALPHA
__IOM uint32_t TFTCTRL
__IOM uint32_t TFTDD
__IOM uint32_t TFTFRAMEBASE
__IOM uint32_t TFTHPORCH
__IOM uint32_t TFTMASK
__IM uint32_t TFTPIXEL
__IOM uint32_t TFTPIXEL0
__IOM uint32_t TFTPIXEL1
__IOM uint32_t TFTPOLARITY
__IOM uint32_t TFTSIZE
__IM uint32_t TFTSTATUS
__IOM uint32_t TFTSTRIDE
__IOM uint32_t TFTTIMING
__IOM uint32_t TFTVPORCH
__IOM uint32_t WRTIMING
__IOM uint32_t WRTIMING1
__IOM uint32_t WRTIMING2
__IOM uint32_t WRTIMING3

Field Documentation

__IOM uint32_t EBI_TypeDef::ADDRTIMING

Address Timing Register

Definition at line 50 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::ADDRTIMING1

Address Timing Register 1

Definition at line 55 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::ADDRTIMING2

Address Timing Register 2

Definition at line 59 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::ADDRTIMING3

Address Timing Register 3

Definition at line 63 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::CMD

Command Register

Definition at line 69 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32lg_ebi.h .

__IM uint32_t EBI_TypeDef::ECCPARITY

ECC Parity register

Definition at line 71 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::IEN

Interrupt Enable Register

Definition at line 90 of file efm32lg_ebi.h .

__IM uint32_t EBI_TypeDef::IF

Interrupt Flag Register

Definition at line 87 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 89 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 88 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::NANDCTRL

NAND Control Register

Definition at line 68 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::PAGECTRL

Page Control Register

Definition at line 67 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::POLARITY

Polarity Register

Definition at line 53 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::POLARITY1

Polarity Register 1

Definition at line 58 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::POLARITY2

Polarity Register 2

Definition at line 62 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::POLARITY3

Polarity Register 3

Definition at line 66 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::RDTIMING

Read Timing Register

Definition at line 51 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::RDTIMING1

Read Timing Register 1

Definition at line 56 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::RDTIMING2

Read Timing Register 2

Definition at line 60 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::RDTIMING3

Read Timing Register 3

Definition at line 64 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::ROUTE

I/O Routing Register

Definition at line 54 of file efm32lg_ebi.h .

__IM uint32_t EBI_TypeDef::STATUS

Status Register

Definition at line 70 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::TFTALPHA

TFT Alpha Blending Register

Definition at line 82 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::TFTCTRL

TFT Control Register

Definition at line 72 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::TFTDD

TFT Direct Drive Data Register

Definition at line 81 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::TFTFRAMEBASE

TFT Frame Base Register

Definition at line 74 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::TFTHPORCH

TFT Horizontal Porch Register

Definition at line 77 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::TFTMASK

TFT Masking Register

Definition at line 86 of file efm32lg_ebi.h .

__IM uint32_t EBI_TypeDef::TFTPIXEL

TFT Alpha Blending Result Pixel Register

Definition at line 85 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::TFTPIXEL0

TFT Pixel 0 Register

Definition at line 83 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::TFTPIXEL1

TFT Pixel 1 Register

Definition at line 84 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::TFTPOLARITY

TFT Polarity Register

Definition at line 80 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::TFTSIZE

TFT Size Register

Definition at line 76 of file efm32lg_ebi.h .

__IM uint32_t EBI_TypeDef::TFTSTATUS

TFT Status Register

Definition at line 73 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::TFTSTRIDE

TFT Stride Register

Definition at line 75 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::TFTTIMING

TFT Timing Register

Definition at line 79 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::TFTVPORCH

TFT Vertical Porch Register

Definition at line 78 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::WRTIMING

Write Timing Register

Definition at line 52 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::WRTIMING1

Write Timing Register 1

Definition at line 57 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::WRTIMING2

Write Timing Register 2

Definition at line 61 of file efm32lg_ebi.h .

__IOM uint32_t EBI_TypeDef::WRTIMING3

Write Timing Register 3

Definition at line 65 of file efm32lg_ebi.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32LG/Include/ efm32lg_ebi.h