EZRADIODRV_PacketTxHandle Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Transmit_Plugin

EzRadio transmit plug-in instance initialization and handler structure.

Definition at line 100 of file ezradio_transmit_plugin.h .

#include < ezradio_transmit_plugin.h >

Data Fields

uint8_t channel
Transmission channel.
EZRADIODRV_PacketLengthConfig_t lenConfig
Packet length configuration.
uint16_t pktId
Packet ID.
EZRADIODRV_TransmitPacketType_t pktType
Packet type.
EZRADIODRV_Callback_t userCallback
User callback.

The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emdrv/ezradiodrv/plugins/inc/ ezradio_transmit_plugin.h