SMU_PrivilegedAccess_TypeDef Struct ReferenceEMLIB > SMU

SMU peripheral privileged access enablers.

Definition at line 379 of file em_smu.h .

#include < em_smu.h >

Data Fields

bool privilegedACMP0 : 1
bool privilegedACMP1 : 1
bool privilegedADC0 : 1
bool privilegedCMU : 1
bool privilegedCRYOTIMER : 1
bool privilegedCRYPTO0 : 1
bool privilegedCRYPTO1 : 1
bool privilegedCSEN : 1
bool privilegedEMU : 1
bool privilegedFPUEH : 1
bool privilegedGPCRC : 1
bool privilegedGPIO : 1
bool privilegedI2C0 : 1
bool privilegedI2C1 : 1
bool privilegedIDAC0 : 1
bool privilegedLDMA : 1
bool privilegedLESENSE : 1
bool privilegedLETIMER0 : 1
bool privilegedLEUART0 : 1
bool privilegedMSC : 1
bool privilegedPCNT0 : 1
bool privilegedPRS : 1
bool privilegedReserved0 : 1
bool privilegedReserved1 : 1
bool privilegedReserved2 : 1
bool privilegedReserved3 : 1
bool privilegedReserved4 : 1
bool privilegedReserved5 : 1
bool privilegedReserved6 : 1
bool privilegedReserved7 : 1
bool privilegedReserved8 : 1
bool privilegedReserved9 : 1
bool privilegedRMU : 1
bool privilegedRTCC : 1
bool privilegedSMU : 1
bool privilegedTIMER0 : 1
bool privilegedTIMER1 : 1
bool privilegedTRNG0 : 1
bool privilegedUSART0 : 1
bool privilegedUSART1 : 1
bool privilegedUSART2 : 1
bool privilegedVDAC0 : 1
bool privilegedWDOG0 : 1
bool privilegedWDOG1 : 1
bool privilegedWTIMER0 : 1

Field Documentation

bool SMU_PrivilegedAccess_TypeDef::privilegedACMP0

Privileged access enabler for ACMP0.

Definition at line 431 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedACMP1

Privileged access enabler for ACMP1.

Definition at line 432 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedADC0

Privileged access enabler for ADC0.

Definition at line 433 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedCMU

Privileged access enabler for CMU.

Definition at line 436 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedCRYOTIMER

Privileged access enabler for CRYOTIMER.

Definition at line 438 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedCRYPTO0

Privileged access enabler for CRYPTO0.

Definition at line 439 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedCRYPTO1

Privileged access enabler for CRYPTO1.

Definition at line 440 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedCSEN

Privileged access enabler for CSEN.

Definition at line 441 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedEMU

Privileged access enabler for EMU.

Definition at line 444 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedFPUEH

Privileged access enabler for FPUEH.

Definition at line 445 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedGPCRC

Privileged access enabler for GPCRC.

Definition at line 447 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedGPIO

Privileged access enabler for GPIO.

Definition at line 448 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedI2C0

Privileged access enabler for I2C0.

Definition at line 449 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedI2C1

Privileged access enabler for I2C1.

Definition at line 450 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedIDAC0

Privileged access enabler for IDAC0.

Definition at line 451 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedLDMA

Privileged access enabler for LDMA.

Definition at line 453 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedLESENSE

Privileged access enabler for LESENSE.

Definition at line 454 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedLETIMER0

Privileged access enabler for LETIMER0.

Definition at line 455 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedLEUART0

Privileged access enabler for LEUART0.

Definition at line 456 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedMSC

Privileged access enabler for MSC.

Definition at line 452 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedPCNT0

Privileged access enabler for PCNT0.

Definition at line 458 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedPRS

Privileged access enabler for PRS.

Definition at line 443 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved0

Reserved privileged access enabler.

Definition at line 434 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved1

Reserved privileged access enabler.

Definition at line 435 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved2

Reserved privileged access enabler.

Definition at line 437 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved3

Reserved privileged access enabler.

Definition at line 446 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved4

Reserved privileged access enabler.

Definition at line 457 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved5

Reserved privileged access enabler.

Definition at line 459 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved6

Reserved privileged access enabler.

Definition at line 460 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved7

Reserved privileged access enabler.

Definition at line 461 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved8

Reserved privileged access enabler.

Definition at line 462 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved9

Reserved privileged access enabler.

Definition at line 466 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedRMU

Privileged access enabler for RMU.

Definition at line 463 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedRTCC

Privileged access enabler for RTCC.

Definition at line 464 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedSMU

Privileged access enabler for SMU.

Definition at line 465 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER0

Privileged access enabler for TIMER0.

Definition at line 467 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER1

Privileged access enabler for TIMER1.

Definition at line 468 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedTRNG0

Privileged access enabler for TRNG0.

Definition at line 469 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART0

Privileged access enabler for USART0.

Definition at line 470 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART1

Privileged access enabler for USART1.

Definition at line 471 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART2

Privileged access enabler for USART2.

Definition at line 472 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedVDAC0

Privileged access enabler for VDAC0.

Definition at line 442 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedWDOG0

Privileged access enabler for WDOG0.

Definition at line 473 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedWDOG1

Privileged access enabler for WDOG1.

Definition at line 474 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedWTIMER0

Privileged access enabler for WTIMER0.

Definition at line 475 of file em_smu.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_smu.h