SPIDRV_Init Struct ReferenceEMDRV > SPIDRV

An SPI driver instance initialization structure. Contains a number of SPIDRV configuration options. This structure is passed to SPIDRV_Init() when initializing a SPIDRV instance. Some common initialization data sets are predefined in SPIDRV_MASTER_USART0 and friends.

Definition at line 118 of file spidrv.h .

#include < spidrv.h >

Data Fields

SPIDRV_BitOrder_t bitOrder
A bit order on the SPI bus, MSB or LSB first.
uint32_t bitRate
An SPI bitrate.
SPIDRV_ClockMode_t clockMode
SPI mode, CLKPOL/CLKPHASE setting.
SPIDRV_CsControl_t csControl
A select master mode chip select (CS) control scheme.
uint32_t dummyTxValue
The value to transmit when using SPI receive API functions.
uint32_t frameLength
An SPI framelength, valid numbers are 4..16.
USART_TypeDef * port
The USART used for SPI.
uint8_t portLocationClk
A location number for the SPI Clk pin.
uint8_t portLocationCs
A location number for the SPI Cs pin.
uint8_t portLocationRx
A location number for the SPI Rx pin.
uint8_t portLocationTx
A location number for the SPI Tx pin.
SPIDRV_SlaveStart_t slaveStartMode
A slave mode transfer start scheme.
SPIDRV_Type_t type
An SPI type, master or slave.

The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emdrv/spidrv/inc/ spidrv.h