PCNT_TCC_TypeDef Struct ReferenceEMLIB > PCNT

TCC initialization structure.

Definition at line 327 of file em_pcnt.h .

#include < em_pcnt.h >

Data Fields

PCNT_TCCComp_Typedef compare
PCNT_TCCMode_TypeDef mode
PCNT_TCCPresc_Typedef prescaler
bool prsGateEnable
bool prsPolarity
PCNT_PRSSel_TypeDef tccPRS

Field Documentation

PCNT_TCCComp_Typedef PCNT_TCC_TypeDef::compare

Choose the event that will trigger a clear.

Definition at line 335 of file em_pcnt.h .

Referenced by PCNT_TCCConfiguration() .

PCNT_TCCMode_TypeDef PCNT_TCC_TypeDef::mode

Mode to operate in.

Definition at line 329 of file em_pcnt.h .

Referenced by PCNT_TCCConfiguration() .

PCNT_TCCPresc_Typedef PCNT_TCC_TypeDef::prescaler

Prescaler value for LFACLK in LFA mode.

Definition at line 332 of file em_pcnt.h .

Referenced by PCNT_TCCConfiguration() .

bool PCNT_TCC_TypeDef::prsGateEnable

Enable gating PCNT input clock through TCC PRS signal. Polarity selection is done through prsPolarity.

Definition at line 347 of file em_pcnt.h .

Referenced by PCNT_TCCConfiguration() .

bool PCNT_TCC_TypeDef::prsPolarity

TCC PRS input polarity.
False = Rising edge for comparison trigger, and PCNT clock gated when PRS signal is high.
True = Falling edge for comparison trigger, and PCNT clock gated when PRS signal is low.

Definition at line 343 of file em_pcnt.h .

Referenced by PCNT_TCCConfiguration() .

PCNT_PRSSel_TypeDef PCNT_TCC_TypeDef::tccPRS

PRS input to TCC module, either for gating the PCNT clock, triggering the TCC comparison, or both.

Definition at line 338 of file em_pcnt.h .

Referenced by PCNT_TCCConfiguration() .


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/emlib/inc/ em_pcnt.h