EMU_TypeDef Struct ReferenceDevices > EZR32HG_EMU
Definition at line
47
of file
ezr32hg_emu.h
.
Data Fields |
|
| __IOM uint32_t | AUXCTRL |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | LOCK |
| uint32_t | RESERVED0 [1U] |
| uint32_t | RESERVED1 [6U] |
Field Documentation
| __IOM uint32_t EMU_TypeDef::AUXCTRL |
Auxiliary Control Register
Definition at line
54
of file
ezr32hg_emu.h
.
| __IOM uint32_t EMU_TypeDef::CTRL |
Control Register
Definition at line
48
of file
ezr32hg_emu.h
.
| __IOM uint32_t EMU_TypeDef::LOCK |
Configuration Lock Register
Definition at line
51
of file
ezr32hg_emu.h
.
| uint32_t EMU_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
50
of file
ezr32hg_emu.h
.
| uint32_t EMU_TypeDef::RESERVED1[6U] |
Reserved for future use
Definition at line
53
of file
ezr32hg_emu.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EZR32HG/Include/
ezr32hg_emu.h