PRS_TypeDef Struct ReferenceDevices > EZR32HG_PRS
Definition at line
47
of file
ezr32hg_prs.h
.
Data Fields |
|
| PRS_CH_TypeDef | CH [6U] |
| uint32_t | RESERVED0 [1U] |
| uint32_t | RESERVED1 [6U] |
| __IOM uint32_t | ROUTE |
| __IOM uint32_t | SWLEVEL |
| __IOM uint32_t | SWPULSE |
| __IOM uint32_t | TRACECTRL |
Field Documentation
| PRS_CH_TypeDef PRS_TypeDef::CH[6U] |
Channel registers
Definition at line
53
of file
ezr32hg_prs.h
.
| uint32_t PRS_TypeDef::RESERVED0[1U] |
Reserved registers
Definition at line
52
of file
ezr32hg_prs.h
.
| uint32_t PRS_TypeDef::RESERVED1[6U] |
Reserved for future use
Definition at line
55
of file
ezr32hg_prs.h
.
| __IOM uint32_t PRS_TypeDef::ROUTE |
I/O Routing Register
Definition at line
50
of file
ezr32hg_prs.h
.
| __IOM uint32_t PRS_TypeDef::SWLEVEL |
Software Level Register
Definition at line
49
of file
ezr32hg_prs.h
.
| __IOM uint32_t PRS_TypeDef::SWPULSE |
Software Pulse Register
Definition at line
48
of file
ezr32hg_prs.h
.
| __IOM uint32_t PRS_TypeDef::TRACECTRL |
MTB Trace Control Register
Definition at line
56
of file
ezr32hg_prs.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EZR32HG/Include/
ezr32hg_prs.h