MTB_TypeDef Struct ReferenceDevices > EZR32HG_MTB
Definition at line
47
of file
ezr32hg_mtb.h
.
Data Fields |
|
| __IOM uint32_t | BASE |
| __IOM uint32_t | FLOW |
| __IOM uint32_t | MASTER |
| __IOM uint32_t | POSITION |
Field Documentation
| __IOM uint32_t MTB_TypeDef::BASE |
MTB Trace Base Register
Definition at line
51
of file
ezr32hg_mtb.h
.
| __IOM uint32_t MTB_TypeDef::FLOW |
MTB Trace Flow Register
Definition at line
50
of file
ezr32hg_mtb.h
.
| __IOM uint32_t MTB_TypeDef::MASTER |
MTB Trace Control Register
Definition at line
49
of file
ezr32hg_mtb.h
.
| __IOM uint32_t MTB_TypeDef::POSITION |
MTB Trace Position Register.
Definition at line
48
of file
ezr32hg_mtb.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EZR32HG/Include/
ezr32hg_mtb.h