Device InitializationBSP

Detailed Description

Device Initialization using HAL configuration.

The BSP Device Initialization APIs provide functionality to initialize the device for a specific application and board based on a HAL configuration header file. The BSP Device Initialization module provides APIs that perform

  • EFM32/EZR32/EFR32 errata workaround
  • DC-to-DC converter initialization on devices with DCDC
  • Clock initialization for crystal oscillators and clock selection for HF and LF clock trees

Functions

void BSP_initBoard (void)
Initialize board based on HAL configuration.
void BSP_initClocks (void)
Initialize crystal oscillators and configure clock trees.
void BSP_initDcdc (void)
Configure and initialize the DC-to-DC converter.
void BSP_initDevice (void)
Initialize the device using HAL config settings.
void BSP_initEmu (void)
Configure EMU energy modes.

Function Documentation

void BSP_initBoard ( void )

Initialize board based on HAL configuration.

Initialize peripherals to communicate with board components

Definition at line 361 of file bsp_init.c .

References BSP_Init() , BSP_INIT_IOEXP , BSP_IOEXP_LEDS , BSP_IOEXP_SENSORS , BSP_IOEXP_VCOM , BSP_LedsInit() , BSP_PeripheralAccess() , CMU_ClockEnable() , cmuClock_GPIO , GPIO_PinModeSet() , gpioModePushPull , i2cInit() , I2CSPM_Init() , and RETARGET_SerialInit() .

void BSP_initDcdc ( void )

Configure and initialize the DC-to-DC converter.

Initialize the DC-to-DC converter if the board is wired for DCDC operation. Power down the DC-to-DC converter if the board is not wired for DCDC operation.

Definition at line 68 of file bsp_init.c .

References EMU_DCDCInit_TypeDef::dcdcMode , and emuDcdcMode_Bypass .

Referenced by BSP_initDevice() .

void BSP_initDevice ( void )

Initialize the device using HAL config settings.

Perform errata workarounds, DC-to-DC converter initialization and clock initialization and selection

Definition at line 44 of file bsp_init.c .

References BSP_initClocks() , BSP_initDcdc() , BSP_initEmu() , and CHIP_Init() .