EZRADIODRV_PacketRxHandle Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Receive_Plugin

EzRadio receive plug-in instance initialization and handler structure.

Definition at line 50 of file ezradio_receive_plugin.h .

#include < ezradio_receive_plugin.h >

Data Fields

uint8_t channel
Reception channel.
uint8_t * pktBuf
Pointer to the receive buffer.
EZRADIODRV_Callback_t userCallback
User callback.

The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emdrv/ezradiodrv/plugins/inc/ ezradio_receive_plugin.h