SMU_PrivilegedAccess_TypeDef Struct ReferenceEMLIB > SMU

SMU peripheral privileged access enablers.

Definition at line 485 of file em_smu.h.

#include <em_smu.h>

Data Fields

bool privilegedACMP0: 1
 
bool privilegedACMP1: 1
 
bool privilegedADC0: 1
 
bool privilegedCMU: 1
 
bool privilegedCRYOTIMER: 1
 
bool privilegedCRYPTO0: 1
 
bool privilegedCRYPTO1: 1
 
bool privilegedCSEN: 1
 
bool privilegedEMU: 1
 
bool privilegedFPUEH: 1
 
bool privilegedGPCRC: 1
 
bool privilegedGPIO: 1
 
bool privilegedI2C0: 1
 
bool privilegedI2C1: 1
 
bool privilegedIDAC0: 1
 
bool privilegedLDMA: 1
 
bool privilegedLESENSE: 1
 
bool privilegedLETIMER0: 1
 
bool privilegedLEUART0: 1
 
bool privilegedMSC: 1
 
bool privilegedPCNT0: 1
 
bool privilegedPRS: 1
 
bool privilegedReserved0: 1
 
bool privilegedReserved1: 1
 
bool privilegedReserved2: 1
 
bool privilegedReserved3: 1
 
bool privilegedReserved4: 1
 
bool privilegedReserved5: 1
 
bool privilegedReserved6: 1
 
bool privilegedReserved7: 1
 
bool privilegedReserved8: 1
 
bool privilegedReserved9: 1
 
bool privilegedRMU: 1
 
bool privilegedRTCC: 1
 
bool privilegedSMU: 1
 
bool privilegedTIMER0: 1
 
bool privilegedTIMER1: 1
 
bool privilegedTRNG0: 1
 
bool privilegedUSART0: 1
 
bool privilegedUSART1: 1
 
bool privilegedUSART2: 1
 
bool privilegedVDAC0: 1
 
bool privilegedWDOG0: 1
 
bool privilegedWDOG1: 1
 
bool privilegedWTIMER0: 1
 

Field Documentation

bool SMU_PrivilegedAccess_TypeDef::privilegedACMP0

Privileged access enabler for ACMP0.

Definition at line 537 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedACMP1

Privileged access enabler for ACMP1.

Definition at line 538 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedADC0

Privileged access enabler for ADC0.

Definition at line 539 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCMU

Privileged access enabler for CMU.

Definition at line 542 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCRYOTIMER

Privileged access enabler for CRYOTIMER.

Definition at line 544 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCRYPTO0

Privileged access enabler for CRYPTO0.

Definition at line 545 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCRYPTO1

Privileged access enabler for CRYPTO1.

Definition at line 546 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCSEN

Privileged access enabler for CSEN.

Definition at line 547 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedEMU

Privileged access enabler for EMU.

Definition at line 550 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedFPUEH

Privileged access enabler for FPUEH.

Definition at line 551 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedGPCRC

Privileged access enabler for GPCRC.

Definition at line 553 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedGPIO

Privileged access enabler for GPIO.

Definition at line 554 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedI2C0

Privileged access enabler for I2C0.

Definition at line 555 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedI2C1

Privileged access enabler for I2C1.

Definition at line 556 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedIDAC0

Privileged access enabler for IDAC0.

Definition at line 557 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLDMA

Privileged access enabler for LDMA.

Definition at line 559 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLESENSE

Privileged access enabler for LESENSE.

Definition at line 560 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLETIMER0

Privileged access enabler for LETIMER0.

Definition at line 561 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLEUART0

Privileged access enabler for LEUART0.

Definition at line 562 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedMSC

Privileged access enabler for MSC.

Definition at line 558 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedPCNT0

Privileged access enabler for PCNT0.

Definition at line 564 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedPRS

Privileged access enabler for PRS.

Definition at line 549 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved0

Reserved privileged access enabler.

Definition at line 540 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved1

Reserved privileged access enabler.

Definition at line 541 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved2

Reserved privileged access enabler.

Definition at line 543 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved3

Reserved privileged access enabler.

Definition at line 552 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved4

Reserved privileged access enabler.

Definition at line 563 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved5

Reserved privileged access enabler.

Definition at line 565 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved6

Reserved privileged access enabler.

Definition at line 566 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved7

Reserved privileged access enabler.

Definition at line 567 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved8

Reserved privileged access enabler.

Definition at line 568 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved9

Reserved privileged access enabler.

Definition at line 572 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedRMU

Privileged access enabler for RMU.

Definition at line 569 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedRTCC

Privileged access enabler for RTCC.

Definition at line 570 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedSMU

Privileged access enabler for SMU.

Definition at line 571 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER0

Privileged access enabler for TIMER0.

Definition at line 573 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER1

Privileged access enabler for TIMER1.

Definition at line 574 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedTRNG0

Privileged access enabler for TRNG0.

Definition at line 575 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART0

Privileged access enabler for USART0.

Definition at line 576 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART1

Privileged access enabler for USART1.

Definition at line 577 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART2

Privileged access enabler for USART2.

Definition at line 578 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedVDAC0

Privileged access enabler for VDAC0.

Definition at line 548 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedWDOG0

Privileged access enabler for WDOG0.

Definition at line 579 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedWDOG1

Privileged access enabler for WDOG1.

Definition at line 580 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedWTIMER0

Privileged access enabler for WTIMER0.

Definition at line 581 of file em_smu.h.


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emlib/inc/em_smu.h