DMADRVEMDRV

Detailed Description

DMADRV Direct Memory Access Driver.


Introduction

The DMADRV driver supports writing code using DMA which will work regardless of the type of the DMA controller on the underlying microcontroller. Additionally, DMA can be used in several modules that are completely unaware of each other. The driver does not preclude use of the native emlib API of the underlying DMA controller. On the contrary, it will often result in more efficient code and is necessary for complex DMA operations. The housekeeping functions of this driver are valuable even in this use-case.

The dmadrv.c and dmadrv.h source files are in the emdrv/dmadrv folder.

Note
DMA transfer completion callback functions are called from within the DMA interrupt handler.


Configuration Options

Some properties of the DMADRV driver are compile-time configurable. These properties are stored in a file named dmadrv_config.h. A template for this file, containing default values, is in the emdrv/config folder. Currently the configuration options are as follows:

  • The interrupt priority of the DMA peripheral.
  • A number of DMA channels to support.
  • Use the native emlib API belonging to the underlying DMA hardware in combination with the DMADRV API.

Both configuration options will help reduce the driver's RAM footprint.

To configure DMADRV, provide a custom configuration file. This is an example dmadrv_config.h file:

#ifndef __SILICON_LABS_DMADRV_CONFIG_H__
#define __SILICON_LABS_DMADRV_CONFIG_H__
// DMADRV DMA interrupt priority configuration option.
// Set DMA interrupt priority. Range is 0..7, 0 is the highest priority.
#define EMDRV_DMADRV_DMA_IRQ_PRIORITY 4
// DMADRV channel count configuration option.
// A number of DMA channels to support. A lower DMA channel count will reduce
// RAM footprint.
#define EMDRV_DMADRV_DMA_CH_COUNT 4
// DMADRV native API configuration option.
// Use the native emlib API of the DMA controller in addition to DMADRV
// housekeeping functions, such as AllocateChannel/FreeChannel, and so on.
#define EMDRV_DMADRV_USE_NATIVE_API
#endif


The API

This section contains brief descriptions of the API functions. For more information about input and output parameters and return values, click on the hyperlinked function names. Most functions return an error code, ECODE_EMDRV_DMADRV_OK is returned on success, see ecode.h and dmadrv.h for other error codes.

The application code must include dmadrv.h header file.

DMADRV_Init(), DMADRV_DeInit()
These functions initialize or deinitialize the DMADRV driver. Typically, DMADRV_Init() is called once in the startup code.

DMADRV_AllocateChannel(), DMADRV_FreeChannel()
DMA channel reserve and release functions. It is recommended that application code check that DMADRV_AllocateChannel() returns ECODE_EMDRV_DMADRV_OK before starting a DMA transfer.

DMADRV_MemoryPeripheral()
Start a DMA transfer from memory to a peripheral.

DMADRV_PeripheralMemory()
Start a DMA transfer from a peripheral to memory.

DMADRV_MemoryPeripheralPingPong()
Start a DMA ping-pong transfer from memory to a peripheral.

DMADRV_PeripheralMemoryPingPong()
Start a DMA ping-pong transfer from a peripheral to memory.

DMADRV_LdmaStartTransfer()
Start a DMA transfer on an LDMA controller. This function can only be used when configuration option EMDRV_DMADRV_USE_NATIVE_API is defined. It is a wrapper similar to the emlib LDMA function, but adds support for completion callback and user-defined callback function parameter.

DMADRV_StopTransfer()
Stop an ongoing DMA transfer.

DMADRV_TransferActive()
Check if a transfer is ongoing.

DMADRV_TransferCompletePending()
Check if a transfer completion is pending.

DMADRV_TransferDone()
Check if a transfer has completed.

DMADRV_TransferRemainingCount()
Get number of items remaining in a transfer.


Example

Transfer a text string to USART1.

#include "dmadrv.h"
char str[] = "Hello DMA !";
unsigned int channel;
int main( void )
{
// Initialize DMA.
// Request a DMA channel.
DMADRV_AllocateChannel( &channel, NULL );
// Start the DMA transfer.
(void*)&(USART1->TXDATA),
str,
true,
sizeof( str ),
NULL,
NULL );
return 0;
}

Macros

#define DMADRV_MAX_XFER_COUNT   ((int)((_LDMA_CH_CTRL_XFERCNT_MASK >> _LDMA_CH_CTRL_XFERCNT_SHIFT) + 1))
 Maximum length of one DMA transfer.
 
#define ECODE_EMDRV_DMADRV_ALREADY_FREED   (ECODE_EMDRV_DMADRV_BASE | 0x00000006)
 A DMA channel was free.
 
#define ECODE_EMDRV_DMADRV_ALREADY_INITIALIZED   (ECODE_EMDRV_DMADRV_BASE | 0x00000003)
 DMA has already been initialized.
 
#define ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED   (ECODE_EMDRV_DMADRV_BASE | 0x00000007)
 A channel is not reserved.
 
#define ECODE_EMDRV_DMADRV_CHANNELS_EXHAUSTED   (ECODE_EMDRV_DMADRV_BASE | 0x00000004)
 No DMA channels available.
 
#define ECODE_EMDRV_DMADRV_IN_USE   (ECODE_EMDRV_DMADRV_BASE | 0x00000005)
 DMA is in use.
 
#define ECODE_EMDRV_DMADRV_NOT_INITIALIZED   (ECODE_EMDRV_DMADRV_BASE | 0x00000002)
 DMA is not initialized.
 
#define ECODE_EMDRV_DMADRV_OK   (ECODE_OK)
 A successful return value.
 
#define ECODE_EMDRV_DMADRV_PARAM_ERROR   (ECODE_EMDRV_DMADRV_BASE | 0x00000001)
 An illegal input parameter.
 

Typedefs

typedef bool(* DMADRV_Callback_t) (unsigned int channel, unsigned int sequenceNo, void *userParam)
 DMADRV transfer completion callback function.
 

Enumerations

enum  DMADRV_DataSize_t {
  dmadrvDataSize1 = ldmaCtrlSizeByte,
  dmadrvDataSize2 = ldmaCtrlSizeHalf,
  dmadrvDataSize4 = ldmaCtrlSizeWord
}
 Data size of one LDMA transfer item.
 
enum  DMADRV_PeripheralSignal_t {
  dmadrvPeripheralSignal_NONE = LDMA_CH_REQSEL_SOURCESEL_NONE,
  dmadrvPeripheralSignal_ADC0_SCAN = LDMA_CH_REQSEL_SIGSEL_ADC0SCAN | LDMA_CH_REQSEL_SOURCESEL_ADC0,
  dmadrvPeripheralSignal_ADC0_SINGLE = LDMA_CH_REQSEL_SIGSEL_ADC0SINGLE | LDMA_CH_REQSEL_SOURCESEL_ADC0,
  dmadrvPeripheralSignal_VDAC0_CH0 = LDMA_CH_REQSEL_SIGSEL_VDAC0CH0 | LDMA_CH_REQSEL_SOURCESEL_VDAC0,
  dmadrvPeripheralSignal_VDAC0_CH1 = LDMA_CH_REQSEL_SIGSEL_VDAC0CH1 | LDMA_CH_REQSEL_SOURCESEL_VDAC0,
  dmadrvPeripheralSignal_CRYPTO0_DATA0RD = LDMA_CH_REQSEL_SIGSEL_CRYPTO0DATA0RD | LDMA_CH_REQSEL_SOURCESEL_CRYPTO0,
  dmadrvPeripheralSignal_CRYPTO0_DATA0WR = LDMA_CH_REQSEL_SIGSEL_CRYPTO0DATA0WR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO0,
  dmadrvPeripheralSignal_CRYPTO0_DATA0XWR = LDMA_CH_REQSEL_SIGSEL_CRYPTO0DATA0XWR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO0,
  dmadrvPeripheralSignal_CRYPTO0_DATA1RD = LDMA_CH_REQSEL_SIGSEL_CRYPTO0DATA1RD | LDMA_CH_REQSEL_SOURCESEL_CRYPTO0,
  dmadrvPeripheralSignal_CRYPTO0_DATA1WR = LDMA_CH_REQSEL_SIGSEL_CRYPTO0DATA1WR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO0,
  dmadrvPeripheralSignal_CRYPTO1_DATA0RD = LDMA_CH_REQSEL_SIGSEL_CRYPTO1DATA0RD | LDMA_CH_REQSEL_SOURCESEL_CRYPTO1,
  dmadrvPeripheralSignal_CRYPTO1_DATA0WR = LDMA_CH_REQSEL_SIGSEL_CRYPTO1DATA0WR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO1,
  dmadrvPeripheralSignal_CRYPTO1_DATA0XWR = LDMA_CH_REQSEL_SIGSEL_CRYPTO1DATA0XWR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO1,
  dmadrvPeripheralSignal_CRYPTO1_DATA1RD = LDMA_CH_REQSEL_SIGSEL_CRYPTO1DATA1RD | LDMA_CH_REQSEL_SOURCESEL_CRYPTO1,
  dmadrvPeripheralSignal_CRYPTO1_DATA1WR = LDMA_CH_REQSEL_SIGSEL_CRYPTO1DATA1WR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO1,
  dmadrvPeripheralSignal_CSEN_DATA = LDMA_CH_REQSEL_SIGSEL_CSENDATA | LDMA_CH_REQSEL_SOURCESEL_CSEN,
  dmadrvPeripheralSignal_CSEN_BSLN = LDMA_CH_REQSEL_SIGSEL_CSENBSLN | LDMA_CH_REQSEL_SOURCESEL_CSEN,
  dmadrvPeripheralSignal_I2C0_RXDATAV = LDMA_CH_REQSEL_SIGSEL_I2C0RXDATAV | LDMA_CH_REQSEL_SOURCESEL_I2C0,
  dmadrvPeripheralSignal_I2C0_TXBL = LDMA_CH_REQSEL_SIGSEL_I2C0TXBL | LDMA_CH_REQSEL_SOURCESEL_I2C0,
  dmadrvPeripheralSignal_I2C1_RXDATAV = LDMA_CH_REQSEL_SIGSEL_I2C1RXDATAV | LDMA_CH_REQSEL_SOURCESEL_I2C1,
  dmadrvPeripheralSignal_I2C1_TXBL = LDMA_CH_REQSEL_SIGSEL_I2C1TXBL | LDMA_CH_REQSEL_SOURCESEL_I2C1,
  dmadrvPeripheralSignal_LEUART0_RXDATAV = LDMA_CH_REQSEL_SIGSEL_LEUART0RXDATAV | LDMA_CH_REQSEL_SOURCESEL_LEUART0,
  dmadrvPeripheralSignal_LEUART0_TXBL = LDMA_CH_REQSEL_SIGSEL_LEUART0TXBL | LDMA_CH_REQSEL_SOURCESEL_LEUART0,
  dmadrvPeripheralSignal_LEUART0_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_LEUART0TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_LEUART0,
  dmadrvPeripheralSignal_MSC_WDATA = LDMA_CH_REQSEL_SIGSEL_MSCWDATA | LDMA_CH_REQSEL_SOURCESEL_MSC,
  dmadrvPeripheralSignal_PRS_REQ0 = LDMA_CH_REQSEL_SIGSEL_PRSREQ0 | LDMA_CH_REQSEL_SOURCESEL_PRS,
  dmadrvPeripheralSignal_PRS_REQ1 = LDMA_CH_REQSEL_SIGSEL_PRSREQ1 | LDMA_CH_REQSEL_SOURCESEL_PRS,
  dmadrvPeripheralSignal_TIMER0_CC0 = LDMA_CH_REQSEL_SIGSEL_TIMER0CC0 | LDMA_CH_REQSEL_SOURCESEL_TIMER0,
  dmadrvPeripheralSignal_TIMER0_CC1 = LDMA_CH_REQSEL_SIGSEL_TIMER0CC1 | LDMA_CH_REQSEL_SOURCESEL_TIMER0,
  dmadrvPeripheralSignal_TIMER0_CC2 = LDMA_CH_REQSEL_SIGSEL_TIMER0CC2 | LDMA_CH_REQSEL_SOURCESEL_TIMER0,
  dmadrvPeripheralSignal_TIMER0_UFOF = LDMA_CH_REQSEL_SIGSEL_TIMER0UFOF | LDMA_CH_REQSEL_SOURCESEL_TIMER0,
  dmadrvPeripheralSignal_TIMER1_CC0 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC0 | LDMA_CH_REQSEL_SOURCESEL_TIMER1,
  dmadrvPeripheralSignal_TIMER1_CC1 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC1 | LDMA_CH_REQSEL_SOURCESEL_TIMER1,
  dmadrvPeripheralSignal_TIMER1_CC2 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC2 | LDMA_CH_REQSEL_SOURCESEL_TIMER1,
  dmadrvPeripheralSignal_TIMER1_CC3 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC3 | LDMA_CH_REQSEL_SOURCESEL_TIMER1,
  dmadrvPeripheralSignal_TIMER1_UFOF = LDMA_CH_REQSEL_SIGSEL_TIMER1UFOF | LDMA_CH_REQSEL_SOURCESEL_TIMER1,
  dmadrvPeripheralSignal_WTIMER0_CC0 = LDMA_CH_REQSEL_SIGSEL_WTIMER0CC0 | LDMA_CH_REQSEL_SOURCESEL_WTIMER0,
  dmadrvPeripheralSignal_WTIMER0_CC1 = LDMA_CH_REQSEL_SIGSEL_WTIMER0CC1 | LDMA_CH_REQSEL_SOURCESEL_WTIMER0,
  dmadrvPeripheralSignal_WTIMER0_CC2 = LDMA_CH_REQSEL_SIGSEL_WTIMER0CC2 | LDMA_CH_REQSEL_SOURCESEL_WTIMER0,
  dmadrvPeripheralSignal_WTIMER0_UFOF = LDMA_CH_REQSEL_SIGSEL_WTIMER0UFOF | LDMA_CH_REQSEL_SOURCESEL_WTIMER0,
  dmadrvPeripheralSignal_USART0_RXDATAV = LDMA_CH_REQSEL_SIGSEL_USART0RXDATAV | LDMA_CH_REQSEL_SOURCESEL_USART0,
  dmadrvPeripheralSignal_USART0_TXBL = LDMA_CH_REQSEL_SIGSEL_USART0TXBL | LDMA_CH_REQSEL_SOURCESEL_USART0,
  dmadrvPeripheralSignal_USART0_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_USART0TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_USART0,
  dmadrvPeripheralSignal_USART1_RXDATAV = LDMA_CH_REQSEL_SIGSEL_USART1RXDATAV | LDMA_CH_REQSEL_SOURCESEL_USART1,
  dmadrvPeripheralSignal_USART1_RXDATAVRIGHT = LDMA_CH_REQSEL_SIGSEL_USART1RXDATAVRIGHT | LDMA_CH_REQSEL_SOURCESEL_USART1,
  dmadrvPeripheralSignal_USART1_TXBL = LDMA_CH_REQSEL_SIGSEL_USART1TXBL | LDMA_CH_REQSEL_SOURCESEL_USART1,
  dmadrvPeripheralSignal_USART1_TXBLRIGHT = LDMA_CH_REQSEL_SIGSEL_USART1TXBLRIGHT | LDMA_CH_REQSEL_SOURCESEL_USART1,
  dmadrvPeripheralSignal_USART1_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_USART1TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_USART1,
  dmadrvPeripheralSignal_USART2_RXDATAV = LDMA_CH_REQSEL_SIGSEL_USART2RXDATAV | LDMA_CH_REQSEL_SOURCESEL_USART2,
  dmadrvPeripheralSignal_USART2_TXBL = LDMA_CH_REQSEL_SIGSEL_USART2TXBL | LDMA_CH_REQSEL_SOURCESEL_USART2,
  dmadrvPeripheralSignal_USART2_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_USART2TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_USART2
}
 Peripherals that can trigger LDMA transfers.
 

Functions

Ecode_t DMADRV_AllocateChannel (unsigned int *channelId, void *capabilities)
 Allocate (reserve) a DMA channel.
 
Ecode_t DMADRV_DeInit (void)
 Deinitialize DMADRV.
 
Ecode_t DMADRV_FreeChannel (unsigned int channelId)
 Free an allocated (reserved) DMA channel.
 
Ecode_t DMADRV_Init (void)
 Initialize DMADRV.
 
Ecode_t DMADRV_LdmaStartTransfer (int channelId, LDMA_TransferCfg_t *transfer, LDMA_Descriptor_t *descriptor, DMADRV_Callback_t callback, void *cbUserParam)
 Start an LDMA transfer.
 
Ecode_t DMADRV_MemoryPeripheral (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst, void *src, bool srcInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam)
 Start a memory to a peripheral DMA transfer.
 
Ecode_t DMADRV_MemoryPeripheralPingPong (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst, void *src0, void *src1, bool srcInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam)
 Start a memory to a peripheral ping-pong DMA transfer.
 
Ecode_t DMADRV_PauseTransfer (unsigned int channelId)
 Pause an ongoing DMA transfer.
 
Ecode_t DMADRV_PeripheralMemory (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst, void *src, bool dstInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam)
 Start a peripheral to memory DMA transfer.
 
Ecode_t DMADRV_PeripheralMemoryPingPong (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst0, void *dst1, void *src, bool dstInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam)
 Start a peripheral to memory ping-pong DMA transfer.
 
Ecode_t DMADRV_ResumeTransfer (unsigned int channelId)
 Resume an ongoing DMA transfer.
 
Ecode_t DMADRV_StopTransfer (unsigned int channelId)
 Stop an ongoing DMA transfer.
 
Ecode_t DMADRV_TransferActive (unsigned int channelId, bool *active)
 Check if a transfer is running.
 
Ecode_t DMADRV_TransferCompletePending (unsigned int channelId, bool *pending)
 Check if a transfer complete is pending.
 
Ecode_t DMADRV_TransferDone (unsigned int channelId, bool *done)
 Check if a transfer has completed.
 
Ecode_t DMADRV_TransferRemainingCount (unsigned int channelId, int *remaining)
 Get number of items remaining in a transfer.
 

Typedef Documentation

typedef bool(* DMADRV_Callback_t) (unsigned int channel, unsigned int sequenceNo, void *userParam)

DMADRV transfer completion callback function.

The callback function is called when a transfer is complete.

Parameters
[in]channelThe DMA channel number.
[in]sequenceNoThe number of times the callback was called. Useful on long chains of linked transfers or on endless ping-pong type transfers.
[in]userParamOptional user parameter supplied on DMA invocation.
Returns
When doing ping-pong transfers, return true to continue or false to stop transfers.

Definition at line 82 of file dmadrv.h.

Enumeration Type Documentation

Data size of one LDMA transfer item.

Enumerator
dmadrvDataSize1 

Byte.

dmadrvDataSize2 

Halfword.

dmadrvDataSize4 

Word.

Definition at line 909 of file dmadrv.h.

Peripherals that can trigger LDMA transfers.

Enumerator
dmadrvPeripheralSignal_NONE 

No peripheral selected for DMA triggering.

dmadrvPeripheralSignal_ADC0_SCAN 

Trig on ADC0_SCAN.

dmadrvPeripheralSignal_ADC0_SINGLE 

Trig on ADC0_SINGLE.

dmadrvPeripheralSignal_VDAC0_CH0 

Trig on VDAC0_CH0.

dmadrvPeripheralSignal_VDAC0_CH1 

Trig on VDAC0_CH1.

dmadrvPeripheralSignal_CRYPTO0_DATA0RD 

Trig on CRYPTO0_DATA0RD.

dmadrvPeripheralSignal_CRYPTO0_DATA0WR 

Trig on CRYPTO0_DATA0WR.

dmadrvPeripheralSignal_CRYPTO0_DATA0XWR 

Trig on CRYPTO0_DATA0XWR.

dmadrvPeripheralSignal_CRYPTO0_DATA1RD 

Trig on CRYPTO0_DATA1RD.

dmadrvPeripheralSignal_CRYPTO0_DATA1WR 

Trig on CRYPTO0_DATA1WR.

dmadrvPeripheralSignal_CRYPTO1_DATA0RD 

Trig on CRYPTO1_DATA0RD.

dmadrvPeripheralSignal_CRYPTO1_DATA0WR 

Trig on CRYPTO1_DATA0WR.

dmadrvPeripheralSignal_CRYPTO1_DATA0XWR 

Trig on CRYPTO1_DATA0XWR.

dmadrvPeripheralSignal_CRYPTO1_DATA1RD 

Trig on CRYPTO1_DATA1RD.

dmadrvPeripheralSignal_CRYPTO1_DATA1WR 

Trig on CRYPTO1_DATA1WR.

dmadrvPeripheralSignal_CSEN_DATA 

Trig on CSEN_DATA.

dmadrvPeripheralSignal_CSEN_BSLN 

Trig on CSEN_BSLN.

dmadrvPeripheralSignal_I2C0_RXDATAV 

Trig on I2C0_RXDATAV.

dmadrvPeripheralSignal_I2C0_TXBL 

Trig on I2C0_TXBL.

dmadrvPeripheralSignal_I2C1_RXDATAV 

Trig on I2C1_RXDATAV.

dmadrvPeripheralSignal_I2C1_TXBL 

Trig on I2C1_TXBL.

dmadrvPeripheralSignal_LEUART0_RXDATAV 

Trig on LEUART0_RXDATAV.

dmadrvPeripheralSignal_LEUART0_TXBL 

Trig on LEUART0_TXBL.

dmadrvPeripheralSignal_LEUART0_TXEMPTY 

Trig on LEUART0_TXEMPTY.

dmadrvPeripheralSignal_MSC_WDATA 

Trig on MSC_WDATA.

dmadrvPeripheralSignal_PRS_REQ0 

Trig on PRS_REQ0.

dmadrvPeripheralSignal_PRS_REQ1 

Trig on PRS_REQ1.

dmadrvPeripheralSignal_TIMER0_CC0 

Trig on TIMER0_CC0.

dmadrvPeripheralSignal_TIMER0_CC1 

Trig on TIMER0_CC1.

dmadrvPeripheralSignal_TIMER0_CC2 

Trig on TIMER0_CC2.

dmadrvPeripheralSignal_TIMER0_UFOF 

Trig on TIMER0_UFOF.

dmadrvPeripheralSignal_TIMER1_CC0 

Trig on TIMER1_CC0.

dmadrvPeripheralSignal_TIMER1_CC1 

Trig on TIMER1_CC1.

dmadrvPeripheralSignal_TIMER1_CC2 

Trig on TIMER1_CC2.

dmadrvPeripheralSignal_TIMER1_CC3 

Trig on TIMER1_CC3.

dmadrvPeripheralSignal_TIMER1_UFOF 

Trig on TIMER1_UFOF.

dmadrvPeripheralSignal_WTIMER0_CC0 

Trig on WTIMER0_CC0.

dmadrvPeripheralSignal_WTIMER0_CC1 

Trig on WTIMER0_CC1.

dmadrvPeripheralSignal_WTIMER0_CC2 

Trig on WTIMER0_CC2.

dmadrvPeripheralSignal_WTIMER0_UFOF 

Trig on WTIMER0_UFOF.

dmadrvPeripheralSignal_USART0_RXDATAV 

Trig on USART0_RXDATAV.

dmadrvPeripheralSignal_USART0_TXBL 

Trig on USART0_TXBL.

dmadrvPeripheralSignal_USART0_TXEMPTY 

Trig on USART0_TXEMPTY.

dmadrvPeripheralSignal_USART1_RXDATAV 

Trig on USART1_RXDATAV.

dmadrvPeripheralSignal_USART1_RXDATAVRIGHT 

Trig on USART1_RXDATAVRIGHT.

dmadrvPeripheralSignal_USART1_TXBL 

Trig on USART1_TXBL.

dmadrvPeripheralSignal_USART1_TXBLRIGHT 

Trig on USART1_TXBLRIGHT.

dmadrvPeripheralSignal_USART1_TXEMPTY 

Trig on USART1_TXEMPTY.

dmadrvPeripheralSignal_USART2_RXDATAV 

Trig on USART2_RXDATAV.

dmadrvPeripheralSignal_USART2_TXBL 

Trig on USART2_TXBL.

dmadrvPeripheralSignal_USART2_TXEMPTY 

Trig on USART2_TXEMPTY.

Definition at line 471 of file dmadrv.h.

Function Documentation

Ecode_t DMADRV_AllocateChannel ( unsigned int *  channelId,
void *  capabilities 
)

Allocate (reserve) a DMA channel.

Parameters
[out]channelIdThe channel ID assigned by DMADRV.
[in]capabilitiesNot used.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 127 of file dmadrv.c.

References CORE_DECLARE_IRQ_STATE, CORE_ENTER_ATOMIC, CORE_EXIT_ATOMIC, ECODE_EMDRV_DMADRV_CHANNELS_EXHAUSTED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, and initialized.

Referenced by MIC_init(), and SPIDRV_Init().

Ecode_t DMADRV_DeInit ( void  )

Deinitialize DMADRV.

If DMA channels are not currently allocated, it will disable DMA hardware and mask associated interrupts.

Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 169 of file dmadrv.c.

References CMU_ClockEnable(), CORE_DECLARE_IRQ_STATE, CORE_ENTER_ATOMIC, CORE_EXIT_ATOMIC, ECODE_EMDRV_DMADRV_IN_USE, ECODE_EMDRV_DMADRV_OK, initialized, and LDMA_DeInit().

Referenced by SPIDRV_DeInit(), and UARTDRV_DeInit().

Ecode_t DMADRV_FreeChannel ( unsigned int  channelId)

Free an allocated (reserved) DMA channel.

Parameters
[in]channelIdThe channel ID to free.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 214 of file dmadrv.c.

References CORE_DECLARE_IRQ_STATE, CORE_ENTER_ATOMIC, CORE_EXIT_ATOMIC, ECODE_EMDRV_DMADRV_ALREADY_FREED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, and initialized.

Referenced by MIC_deInit(), SPIDRV_DeInit(), and UARTDRV_DeInit().

Ecode_t DMADRV_Init ( void  )

Initialize DMADRV.

The DMA hardware is initialized.

Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 248 of file dmadrv.c.

References CORE_DECLARE_IRQ_STATE, CORE_ENTER_ATOMIC, CORE_EXIT_ATOMIC, ECODE_EMDRV_DMADRV_ALREADY_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, LDMA_Init(), LDMA_INIT_DEFAULT, LDMA_Init_t::ldmaInitCtrlNumFixed, and LDMA_Init_t::ldmaInitIrqPriority.

Referenced by MIC_init(), and SPIDRV_Init().

Ecode_t DMADRV_LdmaStartTransfer ( int  channelId,
LDMA_TransferCfg_t transfer,
LDMA_Descriptor_t descriptor,
DMADRV_Callback_t  callback,
void *  cbUserParam 
)

Start an LDMA transfer.

This function can only be used on LDMA when EMDRV_DMADRV_USE_NATIVE_API is defined. It is a wrapper similar to emlib LDMA function.

Parameters
[in]channelIdThe channel ID to use.
[in]transferA DMA transfer configuration data structure.
[in]descriptorA DMA transfer descriptor, can be an array of descriptors linked together.
[in]callbackAn optional callback function for signalling completion. May be NULL if not needed.
[in]cbUserParamAn optional user parameter to feed to the callback function. May be NULL if not needed.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 318 of file dmadrv.c.

References ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_StartTransfer().

Referenced by MIC_init().

Ecode_t DMADRV_MemoryPeripheral ( unsigned int  channelId,
DMADRV_PeripheralSignal_t  peripheralSignal,
void *  dst,
void *  src,
bool  srcInc,
int  len,
DMADRV_DataSize_t  size,
DMADRV_Callback_t  callback,
void *  cbUserParam 
)

Start a memory to a peripheral DMA transfer.

Parameters
[in]channelIdThe channel ID to use for the transfer.
[in]peripheralSignalSelects which peripheral/peripheralsignal to use.
[in]dstA destination (peripheral register) memory address.
[in]srcA source memory address.
[in]srcIncSet to true to enable source address increment (increments according to size parameter).
[in]lenA number of items (of size size) to transfer.
[in]sizeAn item size, byte, halfword or word.
[in]callbackA function to call on DMA completion, use NULL if not needed.
[in]cbUserParamAn optional user parameter to feed to the callback function. Use NULL if not needed.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 386 of file dmadrv.c.

Ecode_t DMADRV_MemoryPeripheralPingPong ( unsigned int  channelId,
DMADRV_PeripheralSignal_t  peripheralSignal,
void *  dst,
void *  src0,
void *  src1,
bool  srcInc,
int  len,
DMADRV_DataSize_t  size,
DMADRV_Callback_t  callback,
void *  cbUserParam 
)

Start a memory to a peripheral ping-pong DMA transfer.

Parameters
[in]channelIdThe channel ID to use for the transfer.
[in]peripheralSignalSelects which peripheral/peripheralsignal to use.
[in]dstA destination (peripheral register) memory address.
[in]src0A source memory address of the first (ping) buffer.
[in]src1A source memory address of the second (pong) buffer.
[in]srcIncSet to true to enable source address increment (increments according to size parameter).
[in]lenA number of items (of size size) to transfer.
[in]sizeAn item size, byte, halfword or word.
[in]callbackA function to call on DMA completion, use NULL if not needed.
[in]cbUserParamAn optional user parameter to feed to the callback function. Use NULL if not needed.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 453 of file dmadrv.c.

Ecode_t DMADRV_PauseTransfer ( unsigned int  channelId)

Pause an ongoing DMA transfer.

Parameters
[in]channelIdThe channel ID of the transfer to pause.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 625 of file dmadrv.c.

References ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_EnableChannelRequest().

Referenced by UARTDRV_PauseTransmit().

Ecode_t DMADRV_PeripheralMemory ( unsigned int  channelId,
DMADRV_PeripheralSignal_t  peripheralSignal,
void *  dst,
void *  src,
bool  dstInc,
int  len,
DMADRV_DataSize_t  size,
DMADRV_Callback_t  callback,
void *  cbUserParam 
)

Start a peripheral to memory DMA transfer.

Parameters
[in]channelIdThe channel ID to use for the transfer.
[in]peripheralSignalSelects which peripheral/peripheralsignal to use.
[in]dstA destination memory address.
[in]srcA source memory (peripheral register) address.
[in]dstIncSet to true to enable destination address increment (increments according to size parameter).
[in]lenA number of items (of size size) to transfer.
[in]sizeAn item size, byte, halfword or word.
[in]callbackA function to call on DMA completion, use NULL if not needed.
[in]cbUserParamAn optional user parameter to feed to the callback function. Use NULL if not needed.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 519 of file dmadrv.c.

Referenced by MIC_start().

Ecode_t DMADRV_PeripheralMemoryPingPong ( unsigned int  channelId,
DMADRV_PeripheralSignal_t  peripheralSignal,
void *  dst0,
void *  dst1,
void *  src,
bool  dstInc,
int  len,
DMADRV_DataSize_t  size,
DMADRV_Callback_t  callback,
void *  cbUserParam 
)

Start a peripheral to memory ping-pong DMA transfer.

Parameters
[in]channelIdThe channel ID to use for the transfer.
[in]peripheralSignalSelects which peripheral/peripheralsignal to use.
[in]dst0A destination memory address of the first (ping) buffer.
[in]dst1A destination memory address of the second (pong) buffer.
[in]srcA source memory (peripheral register) address.
[in]dstIncSet to true to enable destination address increment (increments according to size parameter).
[in]lenA number of items (of size size) to transfer.
[in]sizeAn item size, byte, halfword or word.
[in]callbackA function to call on DMA completion, use NULL if not needed.
[in]cbUserParamAn optional user parameter to feed to the callback function. Use NULL if not needed.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 586 of file dmadrv.c.

Ecode_t DMADRV_ResumeTransfer ( unsigned int  channelId)

Resume an ongoing DMA transfer.

Parameters
[in]channelIdThe channel ID of the transfer to resume.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 659 of file dmadrv.c.

References ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_EnableChannelRequest().

Referenced by UARTDRV_ResumeTransmit().

Ecode_t DMADRV_StopTransfer ( unsigned int  channelId)

Stop an ongoing DMA transfer.

Parameters
[in]channelIdThe channel ID of the transfer to stop.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 693 of file dmadrv.c.

References ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_StopTransfer().

Referenced by MIC_deInit(), SPIDRV_AbortTransfer(), SPIDRV_DeInit(), and UARTDRV_Abort().

Ecode_t DMADRV_TransferActive ( unsigned int  channelId,
bool *  active 
)

Check if a transfer is running.

Parameters
[in]channelIdThe channel ID of the transfer to check.
[out]activeTrue if transfer is running, false otherwise.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 730 of file dmadrv.c.

References ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_ChannelEnabled().

Ecode_t DMADRV_TransferCompletePending ( unsigned int  channelId,
bool *  pending 
)

Check if a transfer complete is pending.

Will check the channel interrupt flag. This assumes that the DMA is configured to give a completion interrupt.

Parameters
[in]channelIdThe channel ID of the transfer to check.
[out]pendingTrue if a transfer complete is pending, false otherwise.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 777 of file dmadrv.c.

References ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, and initialized.

Ecode_t DMADRV_TransferDone ( unsigned int  channelId,
bool *  done 
)

Check if a transfer has completed.

Note
This function should be used in a polled environment. Will only work reliably for transfers NOT using the completion interrupt. On UDMA, it will only work on basic transfers on the primary channel.
Parameters
[in]channelIdThe channel ID of the transfer to check.
[out]doneTrue if a transfer has completed, false otherwise.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 825 of file dmadrv.c.

References CORE_ATOMIC_SECTION, ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_TransferDone().

Ecode_t DMADRV_TransferRemainingCount ( unsigned int  channelId,
int *  remaining 
)

Get number of items remaining in a transfer.

Note
This function does not take into account that a DMA transfer with a chain of linked transfers might be ongoing. It will only check the count for the current transfer. On UDMA, it will only work on the primary channel.
Parameters
[in]channelIdThe channel ID of the transfer to check.
[out]remainingA number of items remaining in the transfer.
Returns
ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.

Definition at line 885 of file dmadrv.c.

References CORE_ATOMIC_SECTION, ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_TransferRemainingCount().

Referenced by SPIDRV_AbortTransfer(), UARTDRV_Abort(), UARTDRV_GetReceiveStatus(), and UARTDRV_GetTransmitStatus().