Direct_Receive_PluginEMDRV > EZRADIODRV > Plugin_System

Detailed Description

Direct receive plugin, see Plugin System Layer for detailed documentation.

.

Data Structures

struct  EZRADIODRV_DirectRxHandle
 EzRadio direct rx plug-in instance initialization and handler structure.
 

Macros

#define EZRADIODRV_DIRECT_RECEIVE_PLUGIN_INIT_DEFAULT
 Configuration data for EzRadio direct rx plug-in.
 

Typedefs

typedef struct EZRADIODRV_DirectRxHandle EZRADIODRV_DirectRxHandle_t
 EzRadio direct rx plug-in instance initialization and handler structure.
 

Functions

Ecode_t ezradioStartDirectReceive (EZRADIODRV_Handle_t radioHandle)
 Starts direct reception with the radio configurations from the radioHandle parameter.
 
Ecode_t ezradioStopDirectReceive (void)
 Stops direct reception.
 

Macro Definition Documentation

#define EZRADIODRV_DIRECT_RECEIVE_PLUGIN_INIT_DEFAULT
Value:
{ /* PN9 */ \
0, /* Channel */ \
},

Configuration data for EzRadio direct rx plug-in.

Definition at line 58 of file ezradio_direct_receive_plugin.h.

Function Documentation

Ecode_t ezradioStartDirectReceive ( EZRADIODRV_Handle_t  radioHandle)

Starts direct reception with the radio configurations from the radioHandle parameter.

Parameters
radioHandleHandler of the EzRadio driver instance where channel configuration is set.
Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 41 of file ezradio_direct_receive_plugin.c.

References EZRADIODRV_DirectRxHandle::channel, EZRADIODRV_HandleData::directRx, ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE, ECODE_EMDRV_EZRADIODRV_OK, ezradio_get_int_status(), and ezradio_start_rx().

Ecode_t ezradioStopDirectReceive ( void  )

Stops direct reception.

Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 66 of file ezradio_direct_receive_plugin.c.

References ECODE_EMDRV_EZRADIODRV_OK, and ezradio_change_state().