INTEMLIB
Detailed Description
Safe nesting of interrupt disable/enable API.
-
Deprecated: - These functions are deprecated and marked for removal in a later release. Use the CORE module instead. See Porting from em_int for information on how to convert existing code bases to use CORE .
This module contains functions to safely disable and enable interrupts at the CPU level. INT_Disable() disables interrupts globally and increments a lock level counter (counting semaphore). INT_Enable() decrements the lock level counter and enables interrupts if the counter reaches zero.
These functions would normally be used to secure critical regions and to make sure that a critical section that calls into another critical section does not unintentionally terminate the callee critical section.
These functions should also be used inside interrupt handlers:
* void SysTick_Handler(void)
* {
* INT_Disable();
* .
* .
* .
* INT_Enable();
* }
*
Functions |
|
| __STATIC_INLINE uint32_t | INT_Disable (void) |
|
Disable interrupts.
|
|
| __STATIC_INLINE uint32_t | INT_Enable (void) |
|
Enable interrupts.
|
|
Variables |
|
| uint32_t | INT_LockCnt = 0 |
Function Documentation
| __STATIC_INLINE uint32_t INT_Disable | ( | void |
|
) |
Disable interrupts.
-
Deprecated: - Deprecated and marked for removal in a later release. Use new CORE module instead.
Disable interrupts and increment lock level counter.
- Returns
- Resulting interrupt disable nesting level.
Definition at line
77
of file
em_int.h
.
References INT_LockCnt .
| __STATIC_INLINE uint32_t INT_Enable | ( | void |
|
) |
Enable interrupts.
-
Deprecated: - Deprecated and marked for removal in a later release. Use the new CORE module instead.
- Returns
- Resulting interrupt disable nesting level.
Decrement interrupt lock level counter and enable interrupts if counter reached zero.
Definition at line
103
of file
em_int.h
.
References INT_LockCnt .
Variable Documentation
| uint32_t INT_LockCnt = 0 |
An interrupt lock level counter. Set to zero initially because main is normally entered with interrupts enabled.
Definition at line
74
of file
em_int.c
.
Referenced by INT_Disable() , and INT_Enable() .