TIMER_InitDTI_TypeDef Struct ReferenceEMLIB > TIMER
TIMER Dead Time Insertion (DTI) initialization structure.
Definition at line
451
of file
em_timer.h
.
#include <
em_timer.h
>
Data Fields |
|
| bool | activeLowOut |
| bool | autoRestart |
| bool | enable |
| bool | enableFaultSourceCoreLockup |
| bool | enableFaultSourceDebugger |
| bool | enableFaultSourcePrsSel0 |
| bool | enableFaultSourcePrsSel1 |
| bool | enablePrsSource |
| unsigned int | fallTime |
| TIMER_DtiFaultAction_TypeDef | faultAction |
| TIMER_PRSSEL_TypeDef | faultSourcePrsSel0 |
| TIMER_PRSSEL_TypeDef | faultSourcePrsSel1 |
| bool | invertComplementaryOut |
| uint32_t | outputsEnableMask |
| TIMER_Prescale_TypeDef | prescale |
| TIMER_PRSSEL_TypeDef | prsSel |
| unsigned int | riseTime |
Field Documentation
| bool TIMER_InitDTI_TypeDef::activeLowOut |
| bool TIMER_InitDTI_TypeDef::autoRestart |
Enable Automatic Start-up functionality (when debugger exits).
Definition at line
462
of file
em_timer.h
.
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::enable |
Enable DTI or leave it disabled until TIMER_EnableDTI() is called.
Definition at line
453
of file
em_timer.h
.
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::enableFaultSourceCoreLockup |
Enable core lockup as a fault source.
Definition at line
487
of file
em_timer.h
.
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::enableFaultSourceDebugger |
Enable debugger as a fault source.
Definition at line
490
of file
em_timer.h
.
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::enableFaultSourcePrsSel0 |
Enable PRS fault source 0 (
faultSourcePrsSel0
).
Definition at line
493
of file
em_timer.h
.
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::enableFaultSourcePrsSel1 |
Enable PRS fault source 1 (
faultSourcePrsSel1
).
Definition at line
499
of file
em_timer.h
.
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::enablePrsSource |
Enable/disable PRS as DTI input.
Definition at line
465
of file
em_timer.h
.
Referenced by TIMER_InitDTI() .
| unsigned int TIMER_InitDTI_TypeDef::fallTime |
| TIMER_DtiFaultAction_TypeDef TIMER_InitDTI_TypeDef::faultAction |
| TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::faultSourcePrsSel0 |
Select which PRS signal to be PRS fault source 0.
Definition at line
496
of file
em_timer.h
.
Referenced by TIMER_InitDTI() .
| TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::faultSourcePrsSel1 |
Select which PRS signal to be PRS fault source 1.
Definition at line
502
of file
em_timer.h
.
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::invertComplementaryOut |
DTI Complementary Output Invert.
Definition at line
459
of file
em_timer.h
.
Referenced by TIMER_InitDTI() .
| uint32_t TIMER_InitDTI_TypeDef::outputsEnableMask |
DTI outputs enable bit mask, consisting of one bit per DTI output signal, i.e., CC0, CC1, CC2, CDTI0, CDTI1, and CDTI2. This value should consist of one or more TIMER_DTOGEN_DTOGnnnEN flags (defined in <part_name>_timer.h) OR'ed together.
Definition at line
484
of file
em_timer.h
.
Referenced by TIMER_InitDTI() .
| TIMER_Prescale_TypeDef TIMER_InitDTI_TypeDef::prescale |
DTI prescaling factor, if HFPER / HFPERB clock used.
Definition at line
472
of file
em_timer.h
.
Referenced by TIMER_InitDTI() .
| TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::prsSel |
Select which PRS channel as DTI input. Only valid if
enablePrsSource
is enabled.
Definition at line
469
of file
em_timer.h
.
Referenced by TIMER_InitDTI() .
| unsigned int TIMER_InitDTI_TypeDef::riseTime |
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_timer.h