MacrosPlatform Middleware > USBXpress
Macros |
|
| #define | STATIC_USBX_BUF (x, y) |
|
Macro for creating WORD (4 byte) aligned static uint8_t array with size which is a multiple of WORD size.
|
|
| #define | USBX_BUF (x, y) SL_ALIGN (4) uint8_t x[((y) + 3) & ~3] SL_ATTRIBUTE_ALIGN (4) |
|
Macro for creating WORD (4 byte) aligned uint8_t array with size which is a multiple of WORD size.
|
|
| #define | USBX_STRING_DESC (_name, ...) |
|
Macro for creating USB-Compliant UTF-16LE UNICODE string descriptor.
|
|
Macro Definition Documentation
| #define STATIC_USBX_BUF | ( |
x,
|
|
y
|
|||
| ) |
em_common.h:189
em_common.h:181
Macro for creating WORD (4 byte) aligned static uint8_t array with size which is a multiple of WORD size.
Example:
STATIC_USBX_BUF(rxBuffer, 37)
; => uint8_t rxBuffer[40];
- Note
- Any data buffer which is written to or read by the USB hardware must be aligned on a WORD (4 byte) boundary. This macro provides an easy way to create static USB data buffers which are guaranteed to be correctly aligned.
Definition at line
221
of file
em_usbxpress.h
.
| #define USBX_BUF | ( |
x,
|
|
y
|
|||
| ) | SL_ALIGN (4) uint8_t x[((y) + 3) & ~3] SL_ATTRIBUTE_ALIGN (4) |
Macro for creating WORD (4 byte) aligned uint8_t array with size which is a multiple of WORD size.
Example:
USBX_BUF(rxBuffer, 37)
; => uint8_t rxBuffer[40];
- Note
- Any data buffer which is written to or read by the USB hardware must be aligned on a WORD (4 byte) boundary. This macro provides an easy way to create USB data buffers which are guaranteed to be correctly aligned.
Definition at line
207
of file
em_usbxpress.h
.
| #define USBX_STRING_DESC | ( |
_name,
|
|
...
|
|||
| ) |
em_common.h:178
em_common.h:189
em_common.h:171
em_common.h:181
em_common.h:164
Macro for creating USB-Compliant UTF-16LE UNICODE string descriptor.
Example: USBX_STRING_DESC(iManufacturer, 'S','i','l','i','c','o','n',' ' \ 'L','a','b','s');
- Note
- The size of the resulting struct will be two bytes larger than a USB string descriptor. This is to accommodate a terminating null char for the string. The value assigned to the 'len' member does not take this into account and is therefore correct USB-wise.
Definition at line
176
of file
em_usbxpress.h
.