SPIDRV_HandleData Struct ReferenceEMDRV > SPIDRV

An SPI driver instance handle data structure. The handle is allocated by the application using the SPIDRV. Several concurrent driver instances can exist in an application. The application is neither supposed to write or read the contents of the handle.

Definition at line 153 of file spidrv.h .

#include < spidrv.h >


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emdrv/spidrv/inc/ spidrv.h