EZRADIODRV_FieldLength Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Transmit_Plugin

EzRadio transmit field length sturcture. Holds length information on all available fields. Data is got from the generated radio configuration header file.

Definition at line 69 of file ezradio_transmit_plugin.h.

#include <ezradio_transmit_plugin.h>

Data Fields

uint8_t f1
 Field 1 length.
 
uint8_t f2
 Field 2 length.
 
uint8_t f3
 Field 3 length.
 
uint8_t f4
 Field 4 length.
 
uint8_t f5
 Field 5 length.
 

The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emdrv/ezradiodrv/plugins/inc/ezradio_transmit_plugin.h