Direct_Transmit_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Direct transmit plugin, see Plugin System Layer for detailed documentation.
.
Data Structures |
|
struct | EZRADIODRV_DirectTxHandle |
EzRadio direct tx plug-in instance initialization and handler structure.
|
|
Macros |
|
#define | EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio direct tx plug-in.
|
|
Typedefs |
|
typedef struct EZRADIODRV_DirectTxHandle | EZRADIODRV_DirectTxHandle_t |
EzRadio direct tx plug-in instance initialization and handler structure.
|
|
Functions |
|
Ecode_t | ezradioStartDirectTransmit ( EZRADIODRV_Handle_t radioHandle) |
Starts direct transmission with the radio configurations from the radioHandle parameter.
|
|
Ecode_t | ezradioStopDirectTransmit (void) |
Stops direct transmission.
|
|
Macro Definition Documentation
#define EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio direct tx plug-in.
Definition at line
58
of file
ezradio_direct_transmit_plugin.h
.
Function Documentation
Ecode_t ezradioStartDirectTransmit | ( | EZRADIODRV_Handle_t |
radioHandle
|
) |
Starts direct transmission with the radio configurations from the radioHandle parameter.
- Parameters
-
radioHandle
Handler of the EzRadio driver instance where channel configuration is set.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
41
of file
ezradio_direct_transmit_plugin.c
.
References EZRADIODRV_DirectTxHandle::channel , EZRADIODRV_HandleData::directTx , ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ECODE_EMDRV_EZRADIODRV_TRANSMIT_FAILED , ezradio_get_int_status() , ezradio_request_device_state() , and ezradio_start_tx() .
Ecode_t ezradioStopDirectTransmit | ( | void |
|
) |
Stops direct transmission.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
72
of file
ezradio_direct_transmit_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_OK , and ezradio_change_state() .