ADC_InitSingle_TypeDef Struct ReferenceEMLIB > ADC

Single conversion initialization structure.

Definition at line 964 of file em_adc.h .

#include < em_adc.h >

Data Fields

ADC_AcqTime_TypeDef acqTime
bool diff
bool fifoOverwrite
bool leftAdjust
ADC_NegSel_TypeDef negSel
ADC_PosSel_TypeDef posSel
bool prsEnable
ADC_PRSSEL_TypeDef prsSel
ADC_Ref_TypeDef reference
bool rep
ADC_Res_TypeDef resolution
bool singleDmaEm2Wu

Field Documentation

ADC_AcqTime_TypeDef ADC_InitSingle_TypeDef::acqTime

Acquisition time (in ADC clock cycles).

Definition at line 972 of file em_adc.h .

Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and adcInit() .

bool ADC_InitSingle_TypeDef::diff

Select if single-ended or differential input.

Definition at line 1003 of file em_adc.h .

Referenced by ADC_InitSingle() .

bool ADC_InitSingle_TypeDef::fifoOverwrite

When true, FIFO overwrites old data when full. If false, FIFO discards new data. The SCANOF IRQ is triggered in both cases.

Definition at line 1022 of file em_adc.h .

Referenced by ADC_InitSingle() .

bool ADC_InitSingle_TypeDef::leftAdjust

Select if left adjustment should be done.

Definition at line 1009 of file em_adc.h .

Referenced by ADC_InitSingle() .

ADC_NegSel_TypeDef ADC_InitSingle_TypeDef::negSel

Select negative input for single channel conversion mode. Negative input is grounded for single-ended (non-differential) converison.

Definition at line 999 of file em_adc.h .

Referenced by ADC_InitSingle() , and adcInit() .

ADC_PosSel_TypeDef ADC_InitSingle_TypeDef::posSel

Select positive input for single channel conversion mode.

Definition at line 993 of file em_adc.h .

Referenced by ADC_InitSingle() , and adcInit() .

bool ADC_InitSingle_TypeDef::prsEnable

Peripheral reflex system trigger enable.

Definition at line 1006 of file em_adc.h .

Referenced by ADC_InitSingle() , and adcInit() .

ADC_PRSSEL_TypeDef ADC_InitSingle_TypeDef::prsSel

Peripheral reflex system trigger selection. Only applicable if prsEnable is enabled.

Definition at line 969 of file em_adc.h .

Referenced by ADC_InitSingle() , and adcInit() .

ADC_Ref_TypeDef ADC_InitSingle_TypeDef::reference

Sample reference selection. Note that, for external references, the ADC calibration register must be set explicitly.

Definition at line 978 of file em_adc.h .

Referenced by ADC0_IRQHandler() , ADC_InitSingle() , adcInit() , and TOUCH_Init() .

bool ADC_InitSingle_TypeDef::rep

Select if continuous conversion until explicit stop.

Definition at line 1012 of file em_adc.h .

Referenced by ADC_InitSingle() .

ADC_Res_TypeDef ADC_InitSingle_TypeDef::resolution

Sample resolution.

Definition at line 981 of file em_adc.h .

Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and TOUCH_Init() .

bool ADC_InitSingle_TypeDef::singleDmaEm2Wu

When true, DMA is available in EM2 for single conversion

Definition at line 1016 of file em_adc.h .

Referenced by ADC_InitSingle() .


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emlib/inc/ em_adc.h