NORFLASH_Info_TypeDef Struct ReferenceKit Drivers > NORFlash
NORFLASH device information struct.
       Definition at line
       
        50
       
       of file
       
        norflash.h
       
       .
      
      
       #include <
       
     
        norflash.h
       
       >
      
| Data Fields | |
| uint32_t | baseAddress | 
| uint32_t | bootSectorCount | 
| uint32_t | bootSectorSize | 
| uint8_t | deviceArc | 
| uint32_t | deviceId | 
| uint32_t | deviceSize | 
| uint16_t | manufacturerId | 
| uint32_t | sectorCount | 
| uint32_t | sectorSize | 
| uint16_t | writeBufferSize | 
Field Documentation
| uint32_t NORFLASH_Info_TypeDef::baseAddress | 
The device base address in cpu memory map.
        Definition at line
        
         51
        
        of file
        
         norflash.h
        
        .
       
Referenced by NORFLASH_AddressValid() , and NORFLASH_EraseDevice() .
| uint32_t NORFLASH_Info_TypeDef::bootSectorCount | 
Number of boot sectors in the device.
        Definition at line
        
         57
        
        of file
        
         norflash.h
        
        .
       
| uint32_t NORFLASH_Info_TypeDef::bootSectorSize | 
Boot sector size in bytes.
        Definition at line
        
         58
        
        of file
        
         norflash.h
        
        .
       
Referenced by NORFLASH_EraseSector() , and NORFLASH_Program() .
| uint8_t NORFLASH_Info_TypeDef::deviceArc | 
The device sector architecture.
        Definition at line
        
         60
        
        of file
        
         norflash.h
        
        .
       
| uint32_t NORFLASH_Info_TypeDef::deviceId | 
The device ID.
        Definition at line
        
         52
        
        of file
        
         norflash.h
        
        .
       
| uint32_t NORFLASH_Info_TypeDef::deviceSize | 
Total device size in bytes.
        Definition at line
        
         53
        
        of file
        
         norflash.h
        
        .
       
Referenced by NORFLASH_AddressValid() .
| uint16_t NORFLASH_Info_TypeDef::manufacturerId | 
The device manufacturer ID.
        Definition at line
        
         54
        
        of file
        
         norflash.h
        
        .
       
| uint32_t NORFLASH_Info_TypeDef::sectorCount | 
Number of sectors in the device.
        Definition at line
        
         55
        
        of file
        
         norflash.h
        
        .
       
| uint32_t NORFLASH_Info_TypeDef::sectorSize | 
Sector size in bytes.
        Definition at line
        
         56
        
        of file
        
         norflash.h
        
        .
       
Referenced by NORFLASH_EraseSector() , and NORFLASH_Program() .
| uint16_t NORFLASH_Info_TypeDef::writeBufferSize | 
Write buffer size of the device.
        Definition at line
        
         59
        
        of file
        
         norflash.h
        
        .
       
Referenced by NORFLASH_Program() .
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/hardware/kit/common/drivers/
       norflash.h