Plugin_ManagerEMDRV > EZRADIODRV > Plugin_System

Detailed Description

Plugin manager, see Plugin System Layer for detailed documentation.


     

.

Data Structures

struct EZRADIODRV_HandleData

Macros

#define ECODE_EMDRV_EZRADIODRV_AUTO_ACK_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000400)
Receive plugin base error code.
#define ECODE_EMDRV_EZRADIODRV_CRC_ERROR_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000300)
CRC error plugin base error code.
#define ECODE_EMDRV_EZRADIODRV_DIRECT_RECEIVE_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000800)
Receive plugin base error code.
#define ECODE_EMDRV_EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000700)
Transmit plugin base error code.
#define ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000001)
Illegal SPI handle.
#define ECODE_EMDRV_EZRADIODRV_OK ( ECODE_OK )
Success return value.
#define ECODE_EMDRV_EZRADIODRV_PN9_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000600)
Receive plugin base error code.
#define ECODE_EMDRV_EZRADIODRV_RECEIVE_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000200)
Receive plugin base error code.
#define ECODE_EMDRV_EZRADIODRV_TRANSMIT_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000100)
Transmit plugin base error code.
#define ECODE_EMDRV_EZRADIODRV_UNMOD_CARRIER_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000500)
Receive plugin base error code.
#define EZRADIODRV_INIT_DEFAULT
Configuration data for EzRadio plugin manager.
#define RADIO_CONFIG_DATA_FIELD_LENGTH
#define RADIO_CONFIG_DATA_MAX_PACKET_LENGTH RADIO_CONFIG_DATA_FIELD1_LENGTH

Typedefs

typedef void(* EZRADIODRV_Callback_t ) ( EZRADIODRV_Handle_t handle, Ecode_t status)
EZRADIODRV feature callback function interface.
typedef EZRADIODRV_HandleData_t * EZRADIODRV_Handle_t
EZRadio driver instance handle.
typedef struct EZRADIODRV_HandleData EZRADIODRV_HandleData_t
Interface for EZRADIODRV_HandleData structure type defined below.
typedef ezradio_cmd_reply_t * EZRADIODRV_ReplyHandle_t
EZradio reply union handle.

Functions

void ezradioInit ( EZRADIODRV_Handle_t handle)
Radio Initialization.
Ecode_t ezradioPluginManager ( EZRADIODRV_Handle_t handle)
EzRadio plugin manager state machine handler. This function should be called in the application in an infinite loop, in order to manage the EzRadio plug-ins properly.
void ezradioResetTRxFifo (void)
Resets both the TX and RX FIFOs.

Macro Definition Documentation

#define EZRADIODRV_INIT_DEFAULT
Value:
{ \
EZRADIODRV_TRANSMIT_PLUGIN_INIT_DEFAULT /* Tx plugin init */ \
EZRADIODRV_RECEIVE_PLUGIN_INIT_DEFAULT /* Rx plugin init */ \
EZRADIODRV_CRC_ERROR_PLUGIN_INIT_DEFAULT /* CRC error plugin init */ \
EZRADIODRV_AUTO_ACK_PLUGIN_INIT_DEFAULT /* Auto-ack plugin init */ \
EZRADIODRV_UNMOD_CARRIER_PLUGIN_INIT_DEFAULT /* CW plugin init */ \
EZRADIODRV_PN9_PLUGIN_INIT_DEFAULT /* PN9 plugin init */ \
EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT /* Direct Tx plugin init */ \
EZRADIODRV_DIRECT_RECEIVE_PLUGIN_INIT_DEFAULT /* Direct Rx plugin init */ \
}

Configuration data for EzRadio plugin manager.

Definition at line 321 of file ezradio_plugin_manager.h .

#define RADIO_CONFIG_DATA_FIELD_LENGTH
Value:
{ \
RADIO_CONFIG_DATA_FIELD1_LENGTH, \
0u, \
0u, \
0u, \
0u, \
}

Definition at line 126 of file ezradio_plugin_manager.h .

Typedef Documentation

typedef void(* EZRADIODRV_Callback_t) ( EZRADIODRV_Handle_t handle, Ecode_t status)

EZRADIODRV feature callback function interface.

Parameters
[in] handle EZRadioDrv instance handler.
[in] status Callback status.
Returns
None

Definition at line 266 of file ezradio_plugin_manager.h .

Function Documentation

void ezradioInit ( EZRADIODRV_Handle_t handle )

Radio Initialization.

Parameters
[in] handle EzRadio driver instance handler.

Definition at line 65 of file ezradio_plugin_manager.c .

References EZRADIO_CONFIG_SUCCESS , ezradio_configuration_init() , ezradio_get_int_status() , ezradio_hal_GpioInit() , ezradio_hal_SpiInit() , USTIMER_DeInit() , USTIMER_Delay() , and USTIMER_Init() .

Ecode_t ezradioPluginManager ( EZRADIODRV_Handle_t radioHandle )

EzRadio plugin manager state machine handler. This function should be called in the application in an infinite loop, in order to manage the EzRadio plug-ins properly.

Parameters
[in] radioHandle EzRadio driver instance handler.

Definition at line 110 of file ezradio_plugin_manager.c .

References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , and ezradio_get_int_status() .