ezradio_api_lib.c File Reference
This file contains the common API library of the EZRadio and.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
Definition in file
ezradio_api_lib.c
.
#include <stddef.h>
#include <stdint.h>
#include <stdarg.h>
#include "
em_gpio.h
"
#include "
gpiointerrupt.h
"
#include "
ustimer.h
"
#include "ezradio_cmd.h"
#include "ezradio_prop.h"
#include "
ezradio_comm.h
"
#include "
ezradio_hal.h
"
#include "
ezradio_api_lib.h
"
Functions |
|
| void | ezradio_change_state (uint8_t next_state1) |
| void | ezradio_fifo_info (uint8_t fifo, ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_fifo_info_fast_read (ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_fifo_info_fast_reset (uint8_t fifo) |
| void | ezradio_frr_a_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_frr_b_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_frr_c_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_frr_d_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_func_info (ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_get_chip_status (uint8_t chip_clr_pend, ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_get_chip_status_fast_clear (void) |
| void | ezradio_get_chip_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_get_int_status (uint8_t ph_clr_pend, uint8_t modem_clr_pend, uint8_t chip_clr_pend, ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_get_int_status_fast_clear (void) |
| void | ezradio_get_int_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_get_modem_status (uint8_t modem_clr_pend, ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_get_modem_status_fast_clear (void) |
| void | ezradio_get_modem_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_get_packet_info (uint8_t field_number_mask, uint16_t len, int16_t diff_len, ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_get_ph_status (uint8_t ph_clr_pend, ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_get_ph_status_fast_clear (void) |
| void | ezradio_get_ph_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_get_property (uint8_t group, uint8_t num_props, uint8_t start_prop, ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_gpio_pin_cfg (uint8_t gpio0, uint8_t gpio1, uint8_t gpio2, uint8_t gpio3, uint8_t nirq, uint8_t sdo, uint8_t gen_config, ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_gpio_pin_cfg_fast (ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_nop (void) |
| void | ezradio_part_info (ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_power_up (uint8_t boot_options, uint8_t xtal_options, uint32_t xo_freq) |
| void | ezradio_read_cmd_buff (ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_read_rx_fifo (uint8_t numBytes, uint8_t *pRxData) |
| void | ezradio_request_device_state (ezradio_cmd_reply_t *ezradioReply) |
| void | ezradio_reset (void) |
| void | ezradio_set_property (uint8_t group, uint8_t num_props, uint8_t start_prop,...) |
| void | ezradio_start_rx (uint8_t channel, uint8_t condition, uint16_t rx_len, uint8_t next_state1, uint8_t next_state2, uint8_t next_state3) |
| void | ezradio_start_rx_fast (void) |
| void | ezradio_start_tx (uint8_t channel, uint8_t condition, uint16_t tx_len) |
| void | ezradio_start_tx_fast (void) |
| void | ezradio_write_tx_fifo (uint8_t numBytes, uint8_t *pTxData) |