ezradio_transmit_plugin.c File Reference
EzRadio transmit plug-in managed by the plug-in manager if enabled.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
Definition in file
ezradio_transmit_plugin.c
.
#include <stddef.h>
#include <stdbool.h>
#include "em_device.h"
#include "ezradio_cmd.h"
#include "ezradio_prop.h"
#include "
ezradio_api_lib.h
"
#include "ezradio_api_lib_add.h"
#include "
ezradio_plugin_manager.h
"
#include "
ezradio_transmit_plugin.h
"
Functions |
|
Ecode_t | ezradioStartTransmitBasic ( EZRADIODRV_Handle_t radioHandle, uint16_t packetLength, uint8_t *pioRadioPacket) |
Start basic transmission. Radio transmits with data only in the first field in this case.
|
|
Ecode_t | ezradioStartTransmitConfigured ( EZRADIODRV_Handle_t radioHandle, uint8_t *pioRadioPacket) |
Start transmission using the packet parameters from the generated configuration header file.
|
|
Ecode_t | ezradioStartTransmitCustom ( EZRADIODRV_Handle_t radioHandle, EZRADIODRV_PacketLengthConfig_t pktLengthConf, uint8_t *pioRadioPacket) |
Start transmission using the packet parameters from pktLengthConf.
|
|
Ecode_t | ezradioStartTransmitDefault ( EZRADIODRV_Handle_t radioHandle, uint8_t *pioRadioPacket) |
Start a default transmission using the packet information previously set to radioHandle. Depending on the information in the radioHandle parameter the function decides which transmission function has to be called.
|
|
Ecode_t | ezradioStartTransmitSmart ( EZRADIODRV_Handle_t radioHandle, EZRADIODRV_PacketLengthConfig_t pktLengthConf, uint8_t *pioRadioPacket) |
Start a smart transmission. Depending on the information in the pktLengthConf parameter the function decides which transmission function has to be called.
|
|