BURTC
Detailed Description
Backup Real Time Counter (BURTC) Peripheral API.
This module contains functions to control the BURTC peripheral of Silicon Labs 32-bit MCUs. The Backup Real Time Counter allows timekeeping in all energy modes. The Backup RTC is also available when the system is in backup mode.
Data Structures |
|
| struct | BURTC_Init_TypeDef |
Macros |
|
| #define | BURTC_INIT_DEFAULT |
| #define | burtcClkDiv_1 1 |
| #define | burtcClkDiv_128 128 |
| #define | burtcClkDiv_16 16 |
| #define | burtcClkDiv_2 2 |
| #define | burtcClkDiv_32 32 |
| #define | burtcClkDiv_4 4 |
| #define | burtcClkDiv_64 64 |
| #define | burtcClkDiv_8 8 |
Enumerations |
|
| enum |
BURTC_ClkSel_TypeDef
{
burtcClkSelULFRCO = BURTC_CTRL_CLKSEL_ULFRCO, burtcClkSelLFRCO = BURTC_CTRL_CLKSEL_LFRCO, burtcClkSelLFXO = BURTC_CTRL_CLKSEL_LFXO } |
| enum |
BURTC_LP_TypeDef
{
burtcLPDisable = BURTC_LPMODE_LPMODE_DISABLE, burtcLPEnable = BURTC_LPMODE_LPMODE_ENABLE, burtcLPBU = BURTC_LPMODE_LPMODE_BUEN } |
| enum |
BURTC_Mode_TypeDef
{
burtcModeDisable = BURTC_CTRL_MODE_DISABLE, burtcModeEM2 = BURTC_CTRL_MODE_EM2EN, burtcModeEM3 = BURTC_CTRL_MODE_EM3EN, burtcModeEM4 = BURTC_CTRL_MODE_EM4EN } |
Functions |
|
| uint32_t | BURTC_ClockFreqGet (void) |
|
Get the clock frequency of the BURTC.
|
|
| uint32_t | BURTC_CompareGet (unsigned int comp) |
|
Get the BURTC compare value.
|
|
| void | BURTC_CompareSet (unsigned int comp, uint32_t value) |
|
Set BURTC compare channel.
|
|
| __STATIC_INLINE uint32_t | BURTC_CounterGet (void) |
|
Get BURTC counter.
|
|
| void | BURTC_CounterReset (void) |
|
Reset counter.
|
|
| void | BURTC_Enable (bool enable) |
|
Enable or Disable BURTC peripheral reset and start counter.
|
|
| __STATIC_INLINE void | BURTC_FreezeEnable (bool enable) |
|
Freeze register updates until enabled.
|
|
| void | BURTC_Init (const BURTC_Init_TypeDef *burtcInit) |
|
Initialize BURTC.
|
|
| __STATIC_INLINE void | BURTC_IntClear (uint32_t flags) |
|
Clear one or more pending BURTC interrupts.
|
|
| __STATIC_INLINE void | BURTC_IntDisable (uint32_t flags) |
|
Disable one or more BURTC interrupts.
|
|
| __STATIC_INLINE void | BURTC_IntEnable (uint32_t flags) |
|
Enable one or more BURTC interrupts.
|
|
| __STATIC_INLINE uint32_t | BURTC_IntGet (void) |
|
Get pending BURTC interrupt flags.
|
|
| __STATIC_INLINE uint32_t | BURTC_IntGetEnabled (void) |
|
Get enabled and pending BURTC interrupt flags.
|
|
| __STATIC_INLINE void | BURTC_IntSet (uint32_t flags) |
|
Set one or more pending BURTC interrupts from SW.
|
|
| __STATIC_INLINE void | BURTC_Lock (void) |
|
Lock BURTC registers, will protect from writing new config settings.
|
|
| __STATIC_INLINE void | BURTC_Powerdown (bool enable) |
|
Shut down power to rentention register bank.
|
|
| void | BURTC_Reset (void) |
|
Restore BURTC to reset state.
|
|
| __STATIC_INLINE uint32_t | BURTC_RetRegGet (uint32_t num) |
|
Read a value from one of the retention registers.
|
|
| __STATIC_INLINE void | BURTC_RetRegSet (uint32_t num, uint32_t data) |
|
Set a value in one of the retention registers.
|
|
| __STATIC_INLINE uint32_t | BURTC_Status (void) |
|
Status of BURTC RAM, timestamp and LP Mode.
|
|
| __STATIC_INLINE void | BURTC_StatusClear (void) |
|
Clear and reset BURTC status register.
|
|
| __STATIC_INLINE void | BURTC_SyncWait (void) |
|
Wait for the BURTC to complete all synchronization of register changes and commands.
|
|
| __STATIC_INLINE uint32_t | BURTC_TimestampGet (void) |
|
Get BURTC timestamp for entering BU.
|
|
| __STATIC_INLINE void | BURTC_Unlock (void) |
|
Unlock BURTC registers, enable write access to change configuration.
|
|
Macro Definition Documentation
| #define BURTC_INIT_DEFAULT |
Default configuration for BURTC initialization structure.
Definition at line
130
of file
em_burtc.h
.
| #define burtcClkDiv_1 1 |
BURTC clock divisors. These values are valid for the BURTC prescaler. Divide clock by 1.
Definition at line
60
of file
em_burtc.h
.
| #define burtcClkDiv_128 128 |
Divide clock by 128.
Definition at line
67
of file
em_burtc.h
.
| #define burtcClkDiv_16 16 |
Divide clock by 16.
Definition at line
64
of file
em_burtc.h
.
| #define burtcClkDiv_2 2 |
Divide clock by 2.
Definition at line
61
of file
em_burtc.h
.
| #define burtcClkDiv_32 32 |
Divide clock by 32.
Definition at line
65
of file
em_burtc.h
.
| #define burtcClkDiv_4 4 |
Divide clock by 4.
Definition at line
62
of file
em_burtc.h
.
| #define burtcClkDiv_64 64 |
Divide clock by 64.
Definition at line
66
of file
em_burtc.h
.
| #define burtcClkDiv_8 8 |
Divide clock by 8.
Definition at line
63
of file
em_burtc.h
.
Enumeration Type Documentation
| enum BURTC_ClkSel_TypeDef |
| enum BURTC_LP_TypeDef |
| enum BURTC_Mode_TypeDef |
Function Documentation
| uint32_t BURTC_ClockFreqGet | ( | void |
|
) |
Get the clock frequency of the BURTC.
- Returns
- The current frequency in Hz.
Ultra-low frequency (1 kHz) clock.
Low-frequency RC oscillator.
Low-frequency crystal oscillator.
Definition at line
376
of file
em_burtc.c
.
References SystemLFRCOClockGet() , SystemLFXOClockGet() , and SystemULFRCOClockGet() .
| uint32_t BURTC_CompareGet | ( | unsigned int |
comp
|
) |
Get the BURTC compare value.
- Parameters
-
[in] compCompare the channel index value, must be 0 for Giant/Leopard Gecko.
- Returns
- The currently configured value for this compare channel.
Definition at line
300
of file
em_burtc.c
.
| void BURTC_CompareSet | ( | unsigned int |
comp,
|
| uint32_t |
value
|
||
| ) |
Set BURTC compare channel.
- Parameters
-
[in] compCompare the channel index, must be 0 for current devices. [in] valueNew compare value.
Definition at line
270
of file
em_burtc.c
.
| __STATIC_INLINE uint32_t BURTC_CounterGet | ( | void |
|
) |
Get BURTC counter.
- Returns
- BURTC counter value
Definition at line
372
of file
em_burtc.h
.
| void BURTC_Enable | ( | bool |
enable
|
) |
Enable or Disable BURTC peripheral reset and start counter.
- Parameters
-
[in] enableIf true; asserts reset to BURTC, halts counter, if false; deassert reset
Definition at line
252
of file
em_burtc.c
.
References BUS_RegBitWrite() .
Referenced by BURTC_Init() .
| __STATIC_INLINE void BURTC_FreezeEnable | ( | bool |
enable
|
) |
Freeze register updates until enabled.
- Parameters
-
[in] enableIf true, registers are not updated until enabled again.
Definition at line
393
of file
em_burtc.h
.
References BUS_RegBitWrite() .
Referenced by BURTC_Init() .
| void BURTC_Init | ( | const BURTC_Init_TypeDef * |
burtcInit
|
) |
Initialize BURTC.
Configures the BURTC peripheral.
- Note
-
Before initialization, BURTC module must first be enabled by clearing the reset bit in the RMU, i.e.,
* RMU_ResetControl(rmuResetBU, rmuResetModeClear); *
Compare channel 0 must be configured outside this function, before initialization if enable is set to true. The counter will always be reset.
- Parameters
-
[in] burtcInitA pointer to the BURTC initialization structure.
Definition at line
128
of file
em_burtc.c
.
References BURTC_Enable() , BURTC_FreezeEnable() , BURTC_IntClear() , BURTC_SyncWait() , burtcClkSelULFRCO , burtcLPDisable , burtcModeDisable , BURTC_Init_TypeDef::clkDiv , BURTC_Init_TypeDef::clkSel , BURTC_Init_TypeDef::compare0Top , BURTC_Init_TypeDef::debugRun , BURTC_Init_TypeDef::enable , BURTC_Init_TypeDef::lowPowerComp , BURTC_Init_TypeDef::lowPowerMode , BURTC_Init_TypeDef::mode , and BURTC_Init_TypeDef::timeStamp .
| __STATIC_INLINE void BURTC_IntClear | ( | uint32_t |
flags
|
) |
Clear one or more pending BURTC interrupts.
- Parameters
-
[in] flagsBURTC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).
Definition at line
179
of file
em_burtc.h
.
Referenced by BURTC_Init() .
| __STATIC_INLINE void BURTC_IntDisable | ( | uint32_t |
flags
|
) |
Disable one or more BURTC interrupts.
- Parameters
-
[in] flagsBURTC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).
Definition at line
197
of file
em_burtc.h
.
| __STATIC_INLINE void BURTC_IntEnable | ( | uint32_t |
flags
|
) |
Enable one or more BURTC interrupts.
- Note
- Depending on use, a pending interrupt may already be set prior to enabling the interrupt. Consider using BURTC_IntClear() prior to enabling if a pending interrupt should be ignored.
- Parameters
-
[in] flagsBURTC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).
Definition at line
220
of file
em_burtc.h
.
| __STATIC_INLINE uint32_t BURTC_IntGet | ( | void |
|
) |
Get pending BURTC interrupt flags.
- Note
- This function does not clear the event bits.
- Returns
- Pending BURTC interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
Definition at line
240
of file
em_burtc.h
.
| __STATIC_INLINE uint32_t BURTC_IntGetEnabled | ( | void |
|
) |
Get enabled and pending BURTC interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- Pending BURTC interrupt sources that is also enabled. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
Definition at line
257
of file
em_burtc.h
.
| __STATIC_INLINE void BURTC_IntSet | ( | uint32_t |
flags
|
) |
Set one or more pending BURTC interrupts from SW.
- Parameters
-
[in] flagsBURTC interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).
Definition at line
277
of file
em_burtc.h
.
| __STATIC_INLINE void BURTC_Powerdown | ( | bool |
enable
|
) |
Shut down power to rentention register bank.
- Parameters
-
[in] enableIf true, shuts off power to retention registers.
- Note
- When power rentention is disabled, it cannot be enabled again (until reset).
Definition at line
406
of file
em_burtc.h
.
References BUS_RegBitWrite() .
| void BURTC_Reset | ( | void |
|
) |
Restore BURTC to reset state.
- Note
- Before accessing the BURTC, BURSTEN in RMU->CTRL must be cleared. LOCK will not be reset to default value, as this will disable access to core BURTC registers.
Definition at line
336
of file
em_burtc.c
.
References BURTC_SyncWait() , BUS_RegBitRead() , and BUS_RegBitWrite() .
| __STATIC_INLINE uint32_t BURTC_RetRegGet | ( | uint32_t |
num
|
) |
Read a value from one of the retention registers.
- Parameters
-
[in] numRetention Register to read
Definition at line
434
of file
em_burtc.h
.
| __STATIC_INLINE void BURTC_RetRegSet | ( | uint32_t |
num,
|
| uint32_t |
data
|
||
| ) |
Set a value in one of the retention registers.
- Parameters
-
[in] numRegister to set [in] dataValue to put into register
Definition at line
420
of file
em_burtc.h
.
| __STATIC_INLINE uint32_t BURTC_Status | ( | void |
|
) |
Status of BURTC RAM, timestamp and LP Mode.
- Returns
- A mask logially OR-ed status bits
Definition at line
292
of file
em_burtc.h
.
| __STATIC_INLINE uint32_t BURTC_TimestampGet | ( | void |
|
) |
Get BURTC timestamp for entering BU.
- Returns
- BURTC Time Stamp value
Definition at line
384
of file
em_burtc.h
.