CMU
Detailed Description
Clock management unit (CMU) Peripheral API.
This module contains functions for the CMU peripheral of Silicon Labs 32-bit MCUs and SoCs. The CMU module controls oscillators, clocks gates, clock multiplexers, pre-scalers, calibration modules and wait-states.
Data Structures | |
struct | CMU_HFXOInit_TypeDef |
struct | CMU_LFXOInit_TypeDef |
Macros | |
#define | CMU_HFXOINIT_DEFAULT |
#define | CMU_HFXOINIT_EXTERNAL_CLOCK |
#define | CMU_LFXOINIT_DEFAULT |
#define | CMU_LFXOINIT_EXTERNAL_CLOCK |
#define | cmuClkDiv_1 1 |
#define | cmuClkDiv_1024 1024 |
#define | cmuClkDiv_128 128 |
#define | cmuClkDiv_16 16 |
#define | cmuClkDiv_16384 16384 |
#define | cmuClkDiv_2 2 |
#define | cmuClkDiv_2048 2048 |
#define | cmuClkDiv_256 256 |
#define | cmuClkDiv_32 32 |
#define | cmuClkDiv_32768 32768 |
#define | cmuClkDiv_4 4 |
#define | cmuClkDiv_4096 4096 |
#define | cmuClkDiv_512 512 |
#define | cmuClkDiv_64 64 |
#define | cmuClkDiv_8 8 |
#define | cmuClkDiv_8192 8192 |
Typedefs | |
typedef uint32_t | CMU_ClkDiv_TypeDef |
Functions | |
CMU_AUXHFRCOBand_TypeDef | CMU_AUXHFRCOBandGet (void) |
Get the AUXHFRCO band in use. | |
void | CMU_AUXHFRCOBandSet (CMU_AUXHFRCOBand_TypeDef band) |
Set the AUXHFRCO band and the tuning value based on the value in the calibration table made during production. | |
uint32_t | CMU_Calibrate (uint32_t HFCycles, CMU_Osc_TypeDef reference) |
Calibrate the clock. | |
void | CMU_CalibrateConfig (uint32_t downCycles, CMU_Osc_TypeDef downSel, CMU_Osc_TypeDef upSel) |
Configure the clock calibration. | |
__STATIC_INLINE void | CMU_CalibrateCont (bool enable) |
Configure continuous calibration mode. | |
uint32_t | CMU_CalibrateCountGet (void) |
Get the calibration count register. | |
__STATIC_INLINE void | CMU_CalibrateStart (void) |
Start calibration. | |
__STATIC_INLINE void | CMU_CalibrateStop (void) |
Stop the calibration counters. | |
CMU_ClkDiv_TypeDef | CMU_ClockDivGet (CMU_Clock_TypeDef clock) |
Get the clock divisor/prescaler. | |
void | CMU_ClockDivSet (CMU_Clock_TypeDef clock, CMU_ClkDiv_TypeDef div) |
Set the clock divisor/prescaler. | |
void | CMU_ClockEnable (CMU_Clock_TypeDef clock, bool enable) |
Enable/disable a clock. | |
uint32_t | CMU_ClockFreqGet (CMU_Clock_TypeDef clock) |
Get the clock frequency for a clock point. | |
CMU_Select_TypeDef | CMU_ClockSelectGet (CMU_Clock_TypeDef clock) |
Get the currently selected reference clock used for a clock branch. | |
void | CMU_ClockSelectSet (CMU_Clock_TypeDef clock, CMU_Select_TypeDef ref) |
Select the reference clock/oscillator used for a clock branch. | |
__STATIC_INLINE uint32_t | CMU_DivToLog2 (CMU_ClkDiv_TypeDef div) |
Convert dividend to logarithmic value. It only works for even numbers equal to 2^n. | |
void | CMU_FreezeEnable (bool enable) |
CMU low frequency register synchronization freeze control. | |
CMU_HFRCOBand_TypeDef | CMU_HFRCOBandGet (void) |
Get HFRCO band in use. | |
void | CMU_HFRCOBandSet (CMU_HFRCOBand_TypeDef band) |
Set HFRCO band and the tuning value based on the value in the calibration table made during production. | |
uint32_t | CMU_HFRCOStartupDelayGet (void) |
Get the HFRCO startup delay. | |
void | CMU_HFRCOStartupDelaySet (uint32_t delay) |
Set the HFRCO startup delay. | |
void | CMU_HFXOInit (const CMU_HFXOInit_TypeDef *hfxoInit) |
Set HFXO control registers. | |
__STATIC_INLINE void | CMU_IntClear (uint32_t flags) |
Clear one or more pending CMU interrupts. | |
__STATIC_INLINE void | CMU_IntDisable (uint32_t flags) |
Disable one or more CMU interrupts. | |
__STATIC_INLINE void | CMU_IntEnable (uint32_t flags) |
Enable one or more CMU interrupts. | |
__STATIC_INLINE uint32_t | CMU_IntGet (void) |
Get pending CMU interrupts. | |
__STATIC_INLINE uint32_t | CMU_IntGetEnabled (void) |
Get enabled and pending CMU interrupt flags. | |
__STATIC_INLINE void | CMU_IntSet (uint32_t flags) |
Set one or more pending CMU interrupts. | |
uint32_t | CMU_LCDClkFDIVGet (void) |
Get the LCD framerate divisor (FDIV) setting. | |
void | CMU_LCDClkFDIVSet (uint32_t div) |
Set the LCD framerate divisor (FDIV) setting. | |
void | CMU_LFXOInit (const CMU_LFXOInit_TypeDef *lfxoInit) |
Set LFXO control registers. | |
__STATIC_INLINE void | CMU_Lock (void) |
Lock the CMU to protect some of its registers against unintended modification. | |
__STATIC_INLINE uint32_t | CMU_Log2ToDiv (uint32_t log2) |
Convert logarithm of 2 prescaler to division factor. | |
void | CMU_OscillatorEnable (CMU_Osc_TypeDef osc, bool enable, bool wait) |
Enable/disable oscillator. | |
uint32_t | CMU_OscillatorTuningGet (CMU_Osc_TypeDef osc) |
Get the oscillator frequency tuning setting. | |
void | CMU_OscillatorTuningSet (CMU_Osc_TypeDef osc, uint32_t val) |
Set the oscillator frequency tuning control. | |
bool | CMU_PCNTClockExternalGet (unsigned int instance) |
Determine if the currently selected PCNTn clock used is external or LFBCLK. | |
void | CMU_PCNTClockExternalSet (unsigned int instance, bool external) |
Select the PCNTn clock. | |
__STATIC_INLINE void | CMU_Unlock (void) |
Unlock the CMU so that writing to locked registers again is possible. | |
void | CMU_UpdateWaitStates (uint32_t freq, int vscale) |
Macro Definition Documentation
#define CMU_HFXOINIT_DEFAULT |
Default HFXO initialization values for Platform 1 devices.
Definition at line 2534
of file em_cmu.h
.
#define CMU_HFXOINIT_EXTERNAL_CLOCK |
Definition at line 2541
of file em_cmu.h
.
#define CMU_LFXOINIT_DEFAULT |
Default LFXO initialization values for platform 1 devices.
Definition at line 2397
of file em_cmu.h
.
#define CMU_LFXOINIT_EXTERNAL_CLOCK |
Definition at line 2403
of file em_cmu.h
.
#define cmuClkDiv_1 1 |
Clock divisors. These values are valid for prescalers. Divide clock by 1.
Definition at line 1102
of file em_cmu.h
.
Referenced by CAPLESENSE_setupCMU(), CMU_ClockDivGet(), CMU_ClockDivSet(), and RETARGET_SerialInit().
#define cmuClkDiv_1024 1024 |
Divide clock by 1024.
Definition at line 1112
of file em_cmu.h
.
#define cmuClkDiv_128 128 |
Divide clock by 128.
Definition at line 1109
of file em_cmu.h
.
Referenced by CMU_ClockDivSet(), and CMU_LCDClkFDIVSet().
#define cmuClkDiv_16 16 |
Divide clock by 16.
Definition at line 1106
of file em_cmu.h
.
Referenced by CMU_ClockDivGet(), CMU_ClockDivSet(), and CMU_ClockFreqGet().
#define cmuClkDiv_16384 16384 |
Divide clock by 16384.
Definition at line 1116
of file em_cmu.h
.
#define cmuClkDiv_2 2 |
Divide clock by 2.
Definition at line 1103
of file em_cmu.h
.
#define cmuClkDiv_2048 2048 |
Divide clock by 2048.
Definition at line 1113
of file em_cmu.h
.
#define cmuClkDiv_256 256 |
#define cmuClkDiv_32 32 |
Divide clock by 32.
Definition at line 1107
of file em_cmu.h
.
#define cmuClkDiv_32768 32768 |
#define cmuClkDiv_4 4 |
Divide clock by 4.
Definition at line 1104
of file em_cmu.h
.
#define cmuClkDiv_4096 4096 |
Divide clock by 4096.
Definition at line 1114
of file em_cmu.h
.
#define cmuClkDiv_512 512 |
#define cmuClkDiv_64 64 |
Divide clock by 64.
Definition at line 1108
of file em_cmu.h
.
#define cmuClkDiv_8 8 |
#define cmuClkDiv_8192 8192 |
Divide clock by 8192.
Definition at line 1115
of file em_cmu.h
.
Typedef Documentation
typedef uint32_t CMU_ClkDiv_TypeDef |
Clock divider configuration
Definition at line 1120
of file em_cmu.h
.
Enumeration Type Documentation
enum CMU_Clock_TypeDef |
Clock points in CMU. See CMU overview in the reference manual.
Definition at line 1251
of file em_cmu.h
.
High-frequency system RCO bands
Definition at line 1129
of file em_cmu.h
.
LFXO Boost values.
Definition at line 2330
of file em_cmu.h
.
enum CMU_Osc_TypeDef |
Oscillator types.
Definition at line 2245
of file em_cmu.h
.
enum CMU_OscMode_TypeDef |
enum CMU_Select_TypeDef |
Selectable clock sources.
Definition at line 2273
of file em_cmu.h
.
Function Documentation
CMU_AUXHFRCOBand_TypeDef CMU_AUXHFRCOBandGet | ( | void |
| ) |
Get the AUXHFRCO band in use.
- Returns
- AUXHFRCO band in use.
Definition at line 4206
of file em_cmu.c
.
void CMU_AUXHFRCOBandSet | ( | CMU_AUXHFRCOBand_TypeDef | band | ) |
Set the AUXHFRCO band and the tuning value based on the value in the calibration table made during production.
- Parameters
-
[in] band
AUXHFRCO band to activate.
Definition at line 4223
of file em_cmu.c
.
References cmuAUXHFRCOBand_11MHz, cmuAUXHFRCOBand_14MHz, cmuAUXHFRCOBand_1MHz, cmuAUXHFRCOBand_21MHz, cmuAUXHFRCOBand_28MHz, and cmuAUXHFRCOBand_7MHz.
uint32_t CMU_Calibrate | ( | uint32_t | HFCycles, |
CMU_Osc_TypeDef | reference |
||
) |
Calibrate the clock.
Run a calibration for HFCLK against a selectable reference clock. See the reference manual, CMU chapter, for more details.
- Note
- This function will not return until the calibration measurement is completed.
- Parameters
-
[in] HFCycles
The number of HFCLK cycles to run the calibration. Increasing this number increases precision but the calibration will take more time. [in] ref
The reference clock used to compare HFCLK.
- Returns
- The number of ticks the reference clock after HFCycles ticks on the HF clock.
Definition at line 4414
of file em_cmu.c
.
References BUS_RegBitRead(), cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, cmuOsc_LFRCO, and cmuOsc_LFXO.
void CMU_CalibrateConfig | ( | uint32_t | downCycles, |
CMU_Osc_TypeDef | downSel, |
||
CMU_Osc_TypeDef | upSel |
||
) |
Configure the clock calibration.
Configure a calibration for a selectable clock source against another selectable reference clock. See the reference manual, CMU chapter, for more details.
- Note
- After configuration, a call to CMU_CalibrateStart() is required and the resulting calibration value can be read out with the CMU_CalibrateCountGet() function call.
- Parameters
-
[in] downCycles
The number of downSel clock cycles to run the calibration. Increasing this number increases precision but the calibration will take more time. [in] downSel
The clock, which will be counted down downCycles. [in] upSel
The reference clock; the number of cycles generated by this clock will be counted and added up and the result can be given with the CMU_CalibrateCountGet() function call.
Definition at line 4503
of file em_cmu.c
.
References cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, cmuOsc_LFRCO, and cmuOsc_LFXO.
__STATIC_INLINE void CMU_CalibrateCont | ( | bool | enable | ) |
Configure continuous calibration mode.
- Parameters
-
[in] enable
If true, enables continuous calibration, if false disables continuous calibration.
Definition at line 2684
of file em_cmu.h
.
References BUS_RegBitWrite().
uint32_t CMU_CalibrateCountGet | ( | void |
| ) |
Get the calibration count register.
- Note
- If continuous calibration mode is active, calibration busy will almost always be off and only the value needs to be read. In a normal case, this function call is triggered by the CALRDY interrupt flag.
- Returns
- The calibration count, the number of UPSEL clocks (see CMU_CalibrateConfig()) in the period of DOWNSEL oscillator clock cycles configured by a previous write operation to CMU->CALCNT.
Definition at line 4611
of file em_cmu.c
.
References BUS_RegBitRead().
__STATIC_INLINE void CMU_CalibrateStart | ( | void |
| ) |
Start calibration.
- Note
- This call is usually invoked after CMU_CalibrateConfig() and possibly CMU_CalibrateCont().
Definition at line 2697
of file em_cmu.h
.
CMU_ClkDiv_TypeDef CMU_ClockDivGet | ( | CMU_Clock_TypeDef | clock | ) |
Get the clock divisor/prescaler.
- Parameters
-
[in] clock
A clock point to get the divisor/prescaler for. Notice that not all clock points have a divisor/prescaler. See the CMU overview in the reference manual.
- Returns
- The current clock point divisor/prescaler. 1 is returned if
clock
specifies a clock point without a divisor/prescaler.
Definition at line 4646
of file em_cmu.c
.
References CMU_DivToLog2(), cmuClkDiv_1, cmuClkDiv_16, cmuClock_LCDpre, cmuClock_LESENSE, cmuClock_LETIMER0, cmuClock_LEUART0, cmuClock_LEUART1, cmuClock_RTC, and SL_Log2ToDiv().
Referenced by UDELAY_Calibrate().
void CMU_ClockDivSet | ( | CMU_Clock_TypeDef | clock, |
CMU_ClkDiv_TypeDef | div |
||
) |
Set the clock divisor/prescaler.
- Note
- If setting an LF clock prescaler, synchronization into the low-frequency domain is required. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. See CMU_FreezeEnable() for a suggestion on how to reduce the stalling time in some use cases.
HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.
- Parameters
-
[in] clock
Clock point to set divisor/prescaler for. Notice that not all clock points have a divisor/prescaler. See the CMU overview in the reference manual. [in] div
The clock divisor to use (<= cmuClkDiv_512).
Definition at line 4777
of file em_cmu.c
.
References CMU_DivToLog2(), cmuClkDiv_1, cmuClkDiv_128, cmuClkDiv_16, cmuClkDiv_32768, cmuClkDiv_512, cmuClkDiv_8, cmuClock_LCDpre, cmuClock_LESENSE, cmuClock_LETIMER0, cmuClock_LEUART0, cmuClock_LEUART1, cmuClock_RTC, SystemCoreClockGet(), and SystemHFClockGet().
Referenced by CAPLESENSE_setupCMU(), RETARGET_SerialInit(), RTCDRV_Init(), SegmentLCD_Init(), UARTDRV_InitLeuart(), and UDELAY_Calibrate().
void CMU_ClockEnable | ( | CMU_Clock_TypeDef | clock, |
bool | enable |
||
) |
Enable/disable a clock.
In general, module clocking is disabled after a reset. If a module clock is disabled, the registers of that module are not accessible and reading from such registers may return undefined values. Writing to registers of clock-disabled modules has no effect. Avoid accessing module registers of a module with a disabled clock.
- Note
- If enabling/disabling an LF clock, synchronization into the low-frequency domain is required. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. See CMU_FreezeEnable() for a suggestion on how to reduce the stalling time in some use cases.
HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.
- Parameters
-
[in] clock
The clock to enable/disable. Notice that not all defined clock points have separate enable/disable control. See the CMU overview in the reference manual. [in] enable
- true - enable specified clock.
- false - disable specified clock.
Definition at line 4985
of file em_cmu.c
.
References BUS_RegBitWrite(), CMU_ClockFreqGet(), and cmuClock_HFLE.
Referenced by adcInit(), BOARD_init(), BSP_BccDeInit(), BSP_BccInit(), BSP_BusControlModeSet(), BSP_EbiInit(), BSP_initBoard(), BSP_McuBoard_Init(), CAPLESENSE_setupCMU(), CAPSENSE_Init(), DMA_Init(), DMADRV_DeInit(), ezradio_hal_GpioInit(), gpioInit(), I2CSPM_Init(), ICM20648_spiInit(), initEbiCommon(), initGpio(), MIC_init(), MICROSD_Init(), MICROSD_PowerOff(), MICROSD_PowerOn(), MSDD_Init(), RETARGET_SerialInit(), RTCDRV_DeInit(), RTCDRV_Init(), SegmentLCD_Disable(), SegmentLCD_Init(), SPI_TFT_Init(), SPIDRV_DeInit(), SPIDRV_Init(), TOUCH_Init(), UARTDRV_DeInit(), UARTDRV_InitLeuart(), UARTDRV_InitUart(), UDELAY_Calibrate(), USBD_Init(), USBTIMER_Init(), USTIMER_DeInit(), USTIMER_Init(), VDDCHECK_Disable(), and VDDCHECK_Init().
uint32_t CMU_ClockFreqGet | ( | CMU_Clock_TypeDef | clock | ) |
Get the clock frequency for a clock point.
- Parameters
-
[in] clock
A clock point to fetch the frequency for.
- Returns
- The current frequency in Hz.
Definition at line 5109
of file em_cmu.c
.
References CMU_DivToLog2(), cmuClkDiv_16, cmuClock_LFA, cmuClock_LFB, SL_Log2ToDiv(), SystemCoreClockGet(), and SystemHFClockGet().
Referenced by ADC_Init(), ADC_PrescaleCalc(), ADC_TimebaseCalc(), BSP_TraceProfilerSetup(), CMU_ClockEnable(), CMU_ClockSelectSet(), CMU_HFRCOBandSet(), DAC_PrescaleCalc(), I2C_BusFreqGet(), I2C_BusFreqSet(), LESENSE_ScanFreqSet(), LEUART_BaudrateGet(), LEUART_BaudrateSet(), MIC_init(), MSC_Init(), UARTDRV_InitLeuart(), USART_BaudrateAsyncSet(), USART_BaudrateGet(), USART_BaudrateSyncSet(), USBTIMER_Init(), USTIMER_Init(), and UTIL_init().
CMU_Select_TypeDef CMU_ClockSelectGet | ( | CMU_Clock_TypeDef | clock | ) |
Get the currently selected reference clock used for a clock branch.
- Parameters
-
[in] clock
Clock branch to fetch selected ref. clock for. One of: - cmuClock_HF
- cmuClock_LFA
- cmuClock_LFB
- cmuClock_DBG
- #cmuClock_USBC
- Returns
- The reference clock used for clocking the selected branch, cmuSelect_Error if invalid
clock
provided.
Definition at line 5944
of file em_cmu.c
.
References cmuSelect_AUXHFRCO, cmuSelect_Disabled, cmuSelect_Error, cmuSelect_HFCLK, cmuSelect_HFCLKLE, cmuSelect_HFRCO, cmuSelect_HFSRCCLK, cmuSelect_HFXO, cmuSelect_LFRCO, cmuSelect_LFXO, and cmuSelect_ULFRCO.
Referenced by CMU_HFRCOBandSet(), CMU_HFXOInit(), CMU_LFXOInit(), UDELAY_Calibrate(), and USBD_Init().
void CMU_ClockSelectSet | ( | CMU_Clock_TypeDef | clock, |
CMU_Select_TypeDef | ref |
||
) |
Select the reference clock/oscillator used for a clock branch.
Notice that if a selected reference is not enabled prior to selecting its use, it will be enabled and this function will wait for the selected oscillator to be stable. It will however NOT be disabled if another reference clock is selected later.
This feature is particularly important if selecting a new reference clock for the clock branch clocking the core. Otherwise, the system may halt.
- Note
- HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.
- Parameters
-
[in] clock
A clock branch to select reference clock for. One of: [in] ref
A reference selected for clocking. See the reference manual for details about references available for a specific clock branch.
Definition at line 6507
of file em_cmu.c
.
References BUS_RegBitWrite(), CMU_ClockFreqGet(), CMU_HFRCOBandGet(), CMU_OscillatorEnable(), cmuClock_HF, cmuClock_HFLE, cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, cmuOsc_LFRCO, cmuOsc_LFXO, cmuSelect_AUXHFRCO, cmuSelect_Disabled, cmuSelect_HFCLK, cmuSelect_HFCLKLE, cmuSelect_HFRCO, cmuSelect_HFSRCCLK, cmuSelect_HFXO, cmuSelect_LFRCO, cmuSelect_LFXO, cmuSelect_ULFRCO, SL_FALLTHROUGH, SystemCoreClockGet(), and SystemHFXOClockGet().
Referenced by BSP_BccInit(), BSP_initClocks(), CAPLESENSE_setupCMU(), MIC_init(), RETARGET_SerialInit(), RTCDRV_Init(), SegmentLCD_Init(), UARTDRV_InitLeuart(), UDELAY_Calibrate(), USBD_Init(), and USBH_Init().
__STATIC_INLINE uint32_t CMU_DivToLog2 | ( | CMU_ClkDiv_TypeDef | div | ) |
Convert dividend to logarithmic value. It only works for even numbers equal to 2^n.
- Parameters
-
[in] div
An unscaled dividend.
- Returns
- Logarithm of 2, as used by fixed prescalers.
Definition at line 2724
of file em_cmu.h
.
Referenced by CMU_ClockDivGet(), CMU_ClockDivSet(), CMU_ClockFreqGet(), and RTCDRV_Init().
void CMU_FreezeEnable | ( | bool | enable | ) |
CMU low frequency register synchronization freeze control.
Some CMU registers require synchronization into the low-frequency (LF) domain. The freeze feature allows for several such registers to be modified before passing them to the LF domain simultaneously (which takes place when the freeze mode is disabled).
Another use case for this feature is using an API (such as the CMU API) for modifying several bit fields consecutively in the same register. If freeze mode is enabled during this sequence, stalling can be avoided.
- Note
- When enabling freeze mode, this function will wait for all current ongoing CMU synchronization to LF domain to complete (normally synchronization will not be in progress.) However, for this reason, when using freeze mode, modifications of registers requiring LF synchronization should be done within one freeze enable/disable block to avoid unnecessary stalling.
- Parameters
-
[in] enable
- true - enable freeze, modified registers are not propagated to the LF domain
- false - disable freeze, modified registers are propagated to the LF domain
Definition at line 7395
of file em_cmu.c
.
CMU_HFRCOBand_TypeDef CMU_HFRCOBandGet | ( | void |
| ) |
Get HFRCO band in use.
- Returns
- HFRCO band in use.
Definition at line 7422
of file em_cmu.c
.
Referenced by CMU_ClockSelectSet().
void CMU_HFRCOBandSet | ( | CMU_HFRCOBand_TypeDef | band | ) |
Set HFRCO band and the tuning value based on the value in the calibration table made during production.
- Note
- HFCLKLE prescaler is automatically modified based on the maximum HFLE frequency allowed.
- Parameters
-
[in] band
HFRCO band to activate.
Definition at line 7442
of file em_cmu.c
.
References CMU_ClockFreqGet(), CMU_ClockSelectGet(), cmuClock_HF, cmuClock_HFLE, cmuHFRCOBand_11MHz, cmuHFRCOBand_14MHz, cmuHFRCOBand_1MHz, cmuHFRCOBand_21MHz, cmuHFRCOBand_28MHz, cmuHFRCOBand_7MHz, cmuSelect_HFRCO, and SystemCoreClockGet().
uint32_t CMU_HFRCOStartupDelayGet | ( | void |
| ) |
Get the HFRCO startup delay.
See the reference manual for more details.
- Returns
- The startup delay in use.
Definition at line 7705
of file em_cmu.c
.
void CMU_HFRCOStartupDelaySet | ( | uint32_t | delay | ) |
Set the HFRCO startup delay.
See the reference manual for more details.
- Parameters
-
[in] delay
The startup delay to set (<= 31).
Definition at line 7721
of file em_cmu.c
.
void CMU_HFXOInit | ( | const CMU_HFXOInit_TypeDef * | hfxoInit | ) |
Set HFXO control registers.
- Note
- HFXO configuration should be obtained from a configuration tool, app note, or xtal data sheet. This function disables the HFXO to ensure a valid state before update.
- Parameters
-
[in] hfxoInit
HFXO setup parameters.
Definition at line 7894
of file em_cmu.c
.
References CMU_HFXOInit_TypeDef::boost, BUS_RegBitWrite(), CMU_ClockSelectGet(), CMU_OscillatorEnable(), cmuClock_HF, cmuOsc_HFXO, cmuOscMode_AcCoupled, cmuOscMode_Crystal, cmuOscMode_External, cmuSelect_HFXO, CMU_HFXOInit_TypeDef::glitchDetector, CMU_HFXOInit_TypeDef::mode, SystemHFXOClockGet(), and CMU_HFXOInit_TypeDef::timeout.
Referenced by BSP_initClocks().
__STATIC_INLINE void CMU_IntClear | ( | uint32_t | flags | ) |
Clear one or more pending CMU interrupts.
- Parameters
-
[in] flags
CMU interrupt sources to clear.
Definition at line 2757
of file em_cmu.h
.
__STATIC_INLINE void CMU_IntDisable | ( | uint32_t | flags | ) |
Disable one or more CMU interrupts.
- Parameters
-
[in] flags
CMU interrupt sources to disable.
Definition at line 2769
of file em_cmu.h
.
__STATIC_INLINE void CMU_IntEnable | ( | uint32_t | flags | ) |
Enable one or more CMU interrupts.
- Note
- Depending on use case, a pending interrupt may already be set prior to enabling the interrupt. Consider using CMU_IntClear() prior to enabling if the pending interrupt should be ignored.
- Parameters
-
[in] flags
CMU interrupt sources to enable.
Definition at line 2786
of file em_cmu.h
.
__STATIC_INLINE uint32_t CMU_IntGet | ( | void |
| ) |
Get pending CMU interrupts.
- Returns
- CMU interrupt sources pending.
Definition at line 2798
of file em_cmu.h
.
__STATIC_INLINE uint32_t CMU_IntGetEnabled | ( | void |
| ) |
Get enabled and pending CMU interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- This function does not clear event bits.
- Returns
- Pending and enabled CMU interrupt sources. The return value is the bitwise AND of
- the enabled interrupt sources in CMU_IEN and
- the pending interrupt flags CMU_IF
Definition at line 2819
of file em_cmu.h
.
__STATIC_INLINE void CMU_IntSet | ( | uint32_t | flags | ) |
Set one or more pending CMU interrupts.
- Parameters
-
[in] flags
CMU interrupt sources to set to pending.
Definition at line 2834
of file em_cmu.h
.
uint32_t CMU_LCDClkFDIVGet | ( | void |
| ) |
Get the LCD framerate divisor (FDIV) setting.
- Returns
- The LCD framerate divisor.
Definition at line 8032
of file em_cmu.c
.
void CMU_LCDClkFDIVSet | ( | uint32_t | div | ) |
Set the LCD framerate divisor (FDIV) setting.
- Note
- The FDIV field (CMU LCDCTRL register) should only be modified while the LCD module is clock disabled (CMU LFACLKEN0.LCD bit is 0). This function will NOT modify FDIV if the LCD module clock is enabled. See CMU_ClockEnable() for disabling/enabling LCD clock.
- Parameters
-
[in] div
The FDIV setting to use.
Definition at line 8054
of file em_cmu.c
.
References cmuClkDiv_128.
Referenced by SegmentLCD_Init().
void CMU_LFXOInit | ( | const CMU_LFXOInit_TypeDef * | lfxoInit | ) |
Set LFXO control registers.
- Note
- LFXO configuration should be obtained from a configuration tool, app note, or xtal data sheet. This function disables the LFXO when necessary to ensure a valid state before update.
- Parameters
-
[in] lfxoInit
LFXO setup parameters.
Definition at line 8084
of file em_cmu.c
.
References CMU_LFXOInit_TypeDef::boost, BUS_RegBitWrite(), BUS_RegMaskedWrite(), CMU_ClockSelectGet(), CMU_OscillatorEnable(), cmuClock_HF, cmuOsc_LFXO, cmuSelect_LFXO, CMU_LFXOInit_TypeDef::mode, and CMU_LFXOInit_TypeDef::timeout.
Referenced by BSP_initClocks().
__STATIC_INLINE void CMU_Lock | ( | void |
| ) |
Lock the CMU to protect some of its registers against unintended modification.
See the reference manual for CMU registers that will be locked.
- Note
- If locking the CMU registers, they must be unlocked prior to using any CMU API functions modifying CMU registers protected by the lock.
Definition at line 2852
of file em_cmu.h
.
Referenced by EMU_EnterEM3().
__STATIC_INLINE uint32_t CMU_Log2ToDiv | ( | uint32_t | log2 | ) |
Convert logarithm of 2 prescaler to division factor.
Deprecated:
- Deprecated and marked for removal in a later release. It will be replaced by SL_Log2ToDiv.
- Parameters
-
[in] log2
Logarithm of 2, as used by fixed prescalers.
- Returns
- Dividend.
Definition at line 2869
of file em_cmu.h
.
References SL_Log2ToDiv().
void CMU_OscillatorEnable | ( | CMU_Osc_TypeDef | osc, |
bool | enable, |
||
bool | wait |
||
) |
Enable/disable oscillator.
- Note
- WARNING: When this function is called to disable either cmuOsc_LFXO or cmuOsc_HFXO, the LFXOMODE or HFXOMODE fields of the CMU_CTRL register are reset to the reset value. In other words, if external clock sources are selected in either LFXOMODE or HFXOMODE fields, the configuration will be cleared and needs to be reconfigured if needed later.
- Parameters
-
[in] osc
The oscillator to enable/disable. [in] enable
- true - enable specified oscillator.
- false - disable specified oscillator.
[in] wait
Only used if enable
is true.- true - wait for oscillator start-up time to timeout before returning.
- false - do not wait for oscillator start-up time to timeout before returning.
Definition at line 8151
of file em_cmu.c
.
References BUS_RegBitRead(), CMU_OscillatorTuningGet(), CMU_OscillatorTuningSet(), cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, cmuOsc_LFRCO, and cmuOsc_LFXO.
Referenced by BSP_initClocks(), CMU_ClockSelectSet(), CMU_HFXOInit(), CMU_LFXOInit(), DBG_SWOEnable(), UDELAY_Calibrate(), USBD_Init(), and USBH_Init().
uint32_t CMU_OscillatorTuningGet | ( | CMU_Osc_TypeDef | osc | ) |
Get the oscillator frequency tuning setting.
- Parameters
-
[in] osc
An oscillator to get tuning value for, one of the following: - cmuOsc_LFRCO
- cmuOsc_HFRCO
- cmuOsc_AUXHFRCO
- cmuOsc_HFXO if CMU_HFXOCTRL_PEAKDETSHUNTOPTMODE is defined
- Returns
- The oscillator frequency tuning setting in use.
Definition at line 8340
of file em_cmu.c
.
References cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, and cmuOsc_LFRCO.
Referenced by CMU_OscillatorEnable().
void CMU_OscillatorTuningSet | ( | CMU_Osc_TypeDef | osc, |
uint32_t | val |
||
) |
Set the oscillator frequency tuning control.
- Note
- Oscillator tuning is done during production and the tuning value is automatically loaded after reset. Changing the tuning value from the calibrated value is for more advanced use. Certain oscillators also have build-in tuning optimization.
- Parameters
-
[in] osc
An oscillator to set tuning value for, one of the following: - cmuOsc_LFRCO
- cmuOsc_HFRCO
- cmuOsc_AUXHFRCO
- cmuOsc_HFXO if PEAKDETSHUNTOPTMODE is available. Note that CMD mode is set.
[in] val
The oscillator frequency tuning setting to use.
Definition at line 8408
of file em_cmu.c
.
References BUS_RegBitRead(), cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, and cmuOsc_LFRCO.
Referenced by CMU_OscillatorEnable().
bool CMU_PCNTClockExternalGet | ( | unsigned int | instance | ) |
Determine if the currently selected PCNTn clock used is external or LFBCLK.
- Parameters
-
[in] instance
PCNT instance number to get currently selected clock source for.
- Returns
- true - selected clock is external clock.
- false - selected clock is LFBCLK.
Definition at line 8621
of file em_cmu.c
.
void CMU_PCNTClockExternalSet | ( | unsigned int | instance, |
bool | external |
||
) |
Select the PCNTn clock.
- Parameters
-
[in] instance
PCNT instance number to set selected clock source for. [in] external
Set to true to select the external clock, false to select LFBCLK.
Definition at line 8661
of file em_cmu.c
.
References BUS_RegBitWrite().
Referenced by PCNT_Init(), and PCNT_Reset().