Unmod_Carrier_Plugin

Detailed Description

Unmodulated Carrier plugin, see Plugin System Layer for detailed documentation.

.

Data Structures

struct  EZRADIODRV_UnmodCarrierHandle
 EzRadio unmodulated carrier plug-in instance initialization and handler structure.
 

Macros

#define EZRADIODRV_UNMOD_CARRIER_PLUGIN_INIT_DEFAULT
 Configuration data for EzRadio unmodulated carrier plug-in.
 

Typedefs

typedef struct EZRADIODRV_UnmodCarrierHandle EZRADIODRV_UnmodCarrierHandle_t
 EzRadio unmodulated carrier plug-in instance initialization and handler structure.
 

Functions

Ecode_t ezradioStartUnmodulatedCarrier (EZRADIODRV_Handle_t radioHandle)
 Starts unmodulated carrier transmission with the radio configurations from the radioHandle parameter.
 
Ecode_t ezradioStopUnmodulatedCarrier (void)
 Stops unmodulated carrier transmission.
 

Macro Definition Documentation

#define EZRADIODRV_UNMOD_CARRIER_PLUGIN_INIT_DEFAULT
Value:
{ /* Unmodulated Carrier */ \
0, /* Channel */ \
},

Configuration data for EzRadio unmodulated carrier plug-in.

Definition at line 71 of file ezradio_unmod_carrier_plugin.h.

Function Documentation

Ecode_t ezradioStartUnmodulatedCarrier ( EZRADIODRV_Handle_t  radioHandle)

Starts unmodulated carrier transmission with the radio configurations from the radioHandle parameter.

Parameters
radioHandleHandler of the EzRadio driver instance where channel configuration is set.
Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 54 of file ezradio_unmod_carrier_plugin.c.

References EZRADIODRV_UnmodCarrierHandle::channel, ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE, ECODE_EMDRV_EZRADIODRV_OK, ECODE_EMDRV_EZRADIODRV_TRANSMIT_FAILED, ezradio_get_int_status(), ezradio_request_device_state(), ezradio_start_tx(), and EZRADIODRV_HandleData::unmodCarrier.

Ecode_t ezradioStopUnmodulatedCarrier ( void  )

Stops unmodulated carrier transmission.

Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 85 of file ezradio_unmod_carrier_plugin.c.

References ECODE_EMDRV_EZRADIODRV_OK, and ezradio_change_state().