__BAP_Config Struct Reference
Structure to configure the BMP280 device.
       Definition at line
       
        59
       
       of file
       
        bap.h
       
       .
      
      
       #include <
       
     
        bap.h
       
       >
      
| Data Fields | |
| uint8_t | oversampling | 
| uint8_t | powerMode | 
| uint8_t | standbyTime | 
Field Documentation
| uint8_t __BAP_Config::oversampling | 
| uint8_t __BAP_Config::powerMode | 
SLEEP, FORCED or NORMAL power mode setting
        Definition at line
        
         61
        
        of file
        
         bap.h
        
        .
       
Referenced by BAP_config() .
| uint8_t __BAP_Config::standbyTime | 
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/hardware/kit/common/bsp/thunderboard/
       bap.h