MCU_DISPLAY Struct Reference
Defines prototype for all segments in display.
       Definition at line
       
        189
       
       of file
       
        segmentlcd.c
       
       .
      
| Data Fields | |
| ARING_TypeDef | ARing | 
| BATTERY_TypeDef | Battery | 
| Block_TypeDef | BotBlocks [ALPHA_DIGITS] | 
| EM_TypeDef | EMode | 
| NUMBER_TypeDef | Number [NUM_DIGITS] | 
| CHAR_TypeDef | Text [ALPHA_DIGITS] | 
| Block_TypeDef | TopBlocks [ALPHA_DIGITS] | 
Field Documentation
| ARING_TypeDef MCU_DISPLAY::ARing | 
| BATTERY_TypeDef MCU_DISPLAY::Battery | 
| Block_TypeDef MCU_DISPLAY::BotBlocks[ALPHA_DIGITS] | 
| EM_TypeDef MCU_DISPLAY::EMode | 
Display energy mode
        Definition at line
        
         192
        
        of file
        
         segmentlcd.c
        
        .
       
Referenced by SegmentLCD_EnergyMode() .
| NUMBER_TypeDef MCU_DISPLAY::Number[NUM_DIGITS] | 
Numbers on display
        Definition at line
        
         191
        
        of file
        
         segmentlcd.c
        
        .
       
Referenced by SegmentLCD_Number() , and SegmentLCD_UnsignedHex() .
| CHAR_TypeDef MCU_DISPLAY::Text[ALPHA_DIGITS] | 
| Block_TypeDef MCU_DISPLAY::TopBlocks[ALPHA_DIGITS] | 
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/hardware/kit/common/drivers/
       segmentlcd.c