DAC initialization structure, common for both channels.
Definition at line
133
of file
em_dac.h
.
#include <
em_dac.h
>
Data Fields |
|
| bool | ch0ResetPre |
| DAC_ConvMode_TypeDef | convMode |
| bool | diff |
| bool | lpEnable |
| bool | outEnablePRS |
| DAC_Output_TypeDef | outMode |
| uint8_t | prescale |
| DAC_Ref_TypeDef | reference |
| DAC_Refresh_TypeDef | refresh |
| bool | sineEnable |
Field Documentation
| bool DAC_Init_TypeDef::ch0ResetPre |
Enable/disable reset of prescaler on ch0 start.
Definition at line
156
of file
em_dac.h
.
Referenced by DAC_Init() .
| DAC_ConvMode_TypeDef DAC_Init_TypeDef::convMode |
| bool DAC_Init_TypeDef::diff |
Select if single ended or differential mode.
Definition at line
165
of file
em_dac.h
.
Referenced by DAC_Init() .
| bool DAC_Init_TypeDef::lpEnable |
Enable/disable use of low pass filter on output.
Definition at line
153
of file
em_dac.h
.
| bool DAC_Init_TypeDef::outEnablePRS |
Enable/disable output enable control by CH1 PRS signal.
Definition at line
159
of file
em_dac.h
.
Referenced by DAC_Init() .
| DAC_Output_TypeDef DAC_Init_TypeDef::outMode |
| uint8_t DAC_Init_TypeDef::prescale |
Prescaler used to get DAC clock. Derived as follows: DACclk=HFPERclk/(2^prescale). The DAC clock should be <= 1MHz.
Definition at line
150
of file
em_dac.h
.
Referenced by DAC_Init() .
| DAC_Ref_TypeDef DAC_Init_TypeDef::reference |
| DAC_Refresh_TypeDef DAC_Init_TypeDef::refresh |
Refresh interval. Only used if REFREN bit set for a DAC channel.
Definition at line
135
of file
em_dac.h
.
Referenced by DAC_Init() .
| bool DAC_Init_TypeDef::sineEnable |
The documentation for this struct was generated from the following file:
-
C:/HandsOn/super/platform/emlib/inc/
em_dac.h