MicroSdKit Drivers
Detailed Description
SPI driver for micro SD card.
Simple micro SD SPI driver with power control and block transfer support.
Macros | |
#define | ACMD13 (13 | 0x80) |
#define | ACMD23 (23 | 0x80) |
#define | ACMD41 (41 | 0x80) |
#define | CMD0 (0) |
#define | CMD1 (1) |
#define | CMD10 (10) |
#define | CMD12 (12) |
#define | CMD16 (16) |
#define | CMD17 (17) |
#define | CMD18 (18) |
#define | CMD23 (23) |
#define | CMD24 (24) |
#define | CMD25 (25) |
#define | CMD41 (41) |
#define | CMD55 (55) |
#define | CMD58 (58) |
#define | CMD8 (8) |
#define | CMD9 (9) |
Functions | |
int | MICROSD_BlockRx (uint8_t *buff, uint32_t btr) |
Receive a data block from micro SD card. | |
int | MICROSD_BlockTx (const uint8_t *buff, uint8_t token) |
Send a data block to micro SD card. | |
void | MICROSD_Deinit (void) |
Deinitialize SPI peripheral. Turn off the SPI peripheral and disable SPI GPIO pins. | |
void | MICROSD_Deselect (void) |
Deselect the micro SD card and release the SPI bus. | |
void | MICROSD_Init (void) |
Initialize the SPI peripheral for microSD card usage. SPI pins and speed etc. is defined in microsdconfig.h. | |
void | MICROSD_PowerOff (void) |
Turn off micro SD card power. DK doesn't support socket power control, only disable the SPI clock. | |
void | MICROSD_PowerOn (void) |
Turn on micro SD card power. DK doesn't support socket power control, only enable the SPI clock. | |
int | MICROSD_Select (void) |
Select the micro SD card and wait for the card to become ready. | |
uint8_t | MICROSD_SendCmd (uint8_t cmd, DWORD arg) |
Send a command packet to micro SD card. | |
void | MICROSD_SpiClkFast (void) |
Set SPI clock to maximum frequency. | |
void | MICROSD_SpiClkSlow (void) |
Set SPI clock to a low frequency suitable for initial card initialization. | |
bool | MICROSD_TimeOutElapsed (void) |
Check if timeout value set with MICROSD_TimeOutSet() has elapsed. | |
void | MICROSD_TimeOutSet (uint32_t msec) |
Set a timeout value. The timeout value will be decremented towards zero when SPI traffic to/from the micro SD card takes place. Use MICROSD_TimeOutElapsed() to check if timeout has elapsed. | |
uint8_t | MICROSD_XferSpi (uint8_t data) |
Do one SPI transfer. | |
Macro Definition Documentation
#define ACMD13 (13 | 0x80) |
SD_STATUS (SDC)
Definition at line 61
of file microsd.h
.
#define ACMD23 (23 | 0x80) |
SET_WR_BLK_ERASE_COUNT (SDC)
Definition at line 66
of file microsd.h
.
#define ACMD41 (41 | 0x80) |
SEND_OP_COND (SDC)
Definition at line 56
of file microsd.h
.
#define CMD0 (0) |
#define CMD1 (1) |
SEND_OP_COND
Definition at line 55
of file microsd.h
.
#define CMD10 (10) |
SEND_CID
Definition at line 59
of file microsd.h
.
#define CMD12 (12) |
#define CMD16 (16) |
SET_BLOCKLEN
Definition at line 62
of file microsd.h
.
#define CMD17 (17) |
READ_SINGLE_BLOCK
Definition at line 63
of file microsd.h
.
#define CMD18 (18) |
READ_MULTIPLE_BLOCK
Definition at line 64
of file microsd.h
.
#define CMD23 (23) |
SET_BLOCK_COUNT
Definition at line 65
of file microsd.h
.
#define CMD24 (24) |
WRITE_BLOCK
Definition at line 67
of file microsd.h
.
#define CMD25 (25) |
WRITE_MULTIPLE_BLOCK
Definition at line 68
of file microsd.h
.
#define CMD41 (41) |
SEND_OP_COND (ACMD)
Definition at line 69
of file microsd.h
.
#define CMD55 (55) |
#define CMD58 (58) |
READ_OCR
Definition at line 71
of file microsd.h
.
#define CMD8 (8) |
#define CMD9 (9) |
SEND_CSD
Definition at line 58
of file microsd.h
.
Function Documentation
int MICROSD_BlockRx | ( | uint8_t * | buff, |
uint32_t | btr |
||
) |
Receive a data block from micro SD card.
- Parameters
-
[out] buff
Data buffer to store received data. btr
Byte count (must be multiple of 4).
- Returns
- 1:OK, 0:Failed.
Definition at line 199
of file microsd.c
.
References MICROSD_XferSpi().
int MICROSD_BlockTx | ( | const uint8_t * | buff, |
uint8_t | token |
||
) |
Send a data block to micro SD card.
- Parameters
-
[in] buff
512 bytes data block to be transmitted. token
Data token.
- Returns
- 1:OK, 0:Failed.
Definition at line 268
of file microsd.c
.
References MICROSD_XferSpi().
int MICROSD_Select | ( | void |
| ) |
Select the micro SD card and wait for the card to become ready.
- Returns
- 1:Successful, 0:Timeout.
Definition at line 157
of file microsd.c
.
References MICROSD_Deselect().
Referenced by MICROSD_PowerOff(), and MICROSD_SendCmd().
uint8_t MICROSD_SendCmd | ( | uint8_t | cmd, |
DWORD | arg |
||
) |
Send a command packet to micro SD card.
- Parameters
-
[in] cmd
Command byte. [in] arg
Argument.
- Returns
- Response value.
Definition at line 350
of file microsd.c
.
References CMD0, CMD12, CMD55, CMD8, MICROSD_Deselect(), MICROSD_Select(), and MICROSD_XferSpi().
bool MICROSD_TimeOutElapsed | ( | void |
| ) |
Check if timeout value set with MICROSD_TimeOutSet() has elapsed.
- Returns
- True if timeout has elapsed.
Definition at line 434
of file microsd.c
.
void MICROSD_TimeOutSet | ( | uint32_t | msec | ) |
Set a timeout value. The timeout value will be decremented towards zero when SPI traffic to/from the micro SD card takes place. Use MICROSD_TimeOutElapsed() to check if timeout has elapsed.
- Parameters
-
[in] msec
Millisecond timeout value (very approximate).
Definition at line 423
of file microsd.c
.
uint8_t MICROSD_XferSpi | ( | uint8_t | data | ) |
Do one SPI transfer.
- Parameters
-
data
Byte to transmit.
- Returns
- Byte received.
Definition at line 135
of file microsd.c
.
References USART_SpiTransfer().
Referenced by MICROSD_BlockRx(), MICROSD_BlockTx(), MICROSD_Deselect(), and MICROSD_SendCmd().