TIMER_InitDTI_TypeDef Struct ReferenceEMLIB > TIMER

TIMER Dead Time Insertion (DTI) initialization structure.

Definition at line 450 of file em_timer.h .

#include < em_timer.h >

Data Fields

bool activeLowOut
bool autoRestart
bool enable
bool enableFaultSourceCoreLockup
bool enableFaultSourceDebugger
bool enableFaultSourcePrsSel0
bool enableFaultSourcePrsSel1
bool enablePrsSource
unsigned int fallTime
TIMER_DtiFaultAction_TypeDef faultAction
TIMER_PRSSEL_TypeDef faultSourcePrsSel0
TIMER_PRSSEL_TypeDef faultSourcePrsSel1
bool invertComplementaryOut
uint32_t outputsEnableMask
TIMER_Prescale_TypeDef prescale
TIMER_PRSSEL_TypeDef prsSel
unsigned int riseTime

Field Documentation

bool TIMER_InitDTI_TypeDef::activeLowOut

DTI Output Polarity.

Definition at line 455 of file em_timer.h .

Referenced by TIMER_InitDTI() .

bool TIMER_InitDTI_TypeDef::autoRestart

Enable Automatic Start-up functionality (when debugger exits).

Definition at line 461 of file em_timer.h .

Referenced by TIMER_InitDTI() .

bool TIMER_InitDTI_TypeDef::enable

Enable DTI or leave it disabled until TIMER_EnableDTI() is called.

Definition at line 452 of file em_timer.h .

Referenced by TIMER_InitDTI() .

bool TIMER_InitDTI_TypeDef::enableFaultSourceCoreLockup

Enable core lockup as a fault source.

Definition at line 486 of file em_timer.h .

Referenced by TIMER_InitDTI() .

bool TIMER_InitDTI_TypeDef::enableFaultSourceDebugger

Enable debugger as a fault source.

Definition at line 489 of file em_timer.h .

Referenced by TIMER_InitDTI() .

bool TIMER_InitDTI_TypeDef::enableFaultSourcePrsSel0

Enable PRS fault source 0 ( faultSourcePrsSel0 ).

Definition at line 492 of file em_timer.h .

Referenced by TIMER_InitDTI() .

bool TIMER_InitDTI_TypeDef::enableFaultSourcePrsSel1

Enable PRS fault source 1 ( faultSourcePrsSel1 ).

Definition at line 498 of file em_timer.h .

Referenced by TIMER_InitDTI() .

bool TIMER_InitDTI_TypeDef::enablePrsSource

Enable/disable PRS as DTI input.

Definition at line 464 of file em_timer.h .

Referenced by TIMER_InitDTI() .

unsigned int TIMER_InitDTI_TypeDef::fallTime

DTI Fall Time

Definition at line 477 of file em_timer.h .

Referenced by TIMER_InitDTI() .

TIMER_DtiFaultAction_TypeDef TIMER_InitDTI_TypeDef::faultAction

Fault Action

Definition at line 504 of file em_timer.h .

Referenced by TIMER_InitDTI() .

TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::faultSourcePrsSel0

Select which PRS signal to be PRS fault source 0.

Definition at line 495 of file em_timer.h .

Referenced by TIMER_InitDTI() .

TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::faultSourcePrsSel1

Select which PRS signal to be PRS fault source 1.

Definition at line 501 of file em_timer.h .

Referenced by TIMER_InitDTI() .

bool TIMER_InitDTI_TypeDef::invertComplementaryOut

DTI Complementary Output Invert.

Definition at line 458 of file em_timer.h .

Referenced by TIMER_InitDTI() .

uint32_t TIMER_InitDTI_TypeDef::outputsEnableMask

DTI outputs enable bit mask, consisting of one bit per DTI output signal, i.e., CC0, CC1, CC2, CDTI0, CDTI1, and CDTI2. This value should consist of one or more TIMER_DTOGEN_DTOGnnnEN flags (defined in <part_name>_timer.h) OR'ed together.

Definition at line 483 of file em_timer.h .

Referenced by TIMER_InitDTI() .

TIMER_Prescale_TypeDef TIMER_InitDTI_TypeDef::prescale

DTI prescaling factor, if HFPER / HFPERB clock used.

Definition at line 471 of file em_timer.h .

Referenced by TIMER_InitDTI() .

TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::prsSel

Select which PRS channel as DTI input. Only valid if enablePrsSource is enabled.

Definition at line 468 of file em_timer.h .

Referenced by TIMER_InitDTI() .

unsigned int TIMER_InitDTI_TypeDef::riseTime

DTI Rise Time

Definition at line 474 of file em_timer.h .

Referenced by TIMER_InitDTI() .


The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/emlib/inc/ em_timer.h