UARTDRV_InitUart_t Struct ReferenceEMDRV > UARTDRV

A UART driver instance initialization structure. Contains a number of UARTDRV configuration options. It is required for driver instance initialization. This structure is passed to UARTDRV_Init() when initializing a UARTDRV instance.

Definition at line 192 of file uartdrv.h .

#include < uartdrv.h >

Data Fields

uint32_t baudRate
UART baud rate.
uint8_t ctsPin
A CTS pin number.
GPIO_Port_TypeDef ctsPort
A CTS pin port number.
UARTDRV_FlowControlType_t fcType
Flow control mode.
bool mvdis
Majority Vote Disable for 16x, 8x and 6x oversampling modes.
USART_OVS_TypeDef oversampling
Oversampling mode.
USART_Parity_TypeDef parity
Parity configuration.
USART_TypeDef * port
The peripheral used for UART.
uint8_t rtsPin
An RTS pin number.
GPIO_Port_TypeDef rtsPort
An RTS pin port number.
uint8_t rxPin
Pin number for UART Rx.
GPIO_Port_TypeDef rxPort
Port for UART Rx pin.
UARTDRV_Buffer_FifoQueue_t * rxQueue
A receive operation queue.
USART_Stopbits_TypeDef stopBits
A number of stop bits.
uint8_t txPin
Pin number for UART Tx.
GPIO_Port_TypeDef txPort
Port for UART Tx pin.
UARTDRV_Buffer_FifoQueue_t * txQueue
T transmit operation queue.
uint8_t uartNum
UART instance number.

The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/emdrv/uartdrv/inc/ uartdrv.h