This structure represents the device properties which are used for calculating the local leader weight on a device.
The parameters are set based on device's capability, whether acting as border router, its power supply config, etc.
mIsUnstable indicates operational stability of device and is determined via a vendor specific mechanism. It can include the following cases:
Device internally detects that it loses external power supply more often than usual. What is usual is determined by the vendor.
Device internally detects that it reboots more often than usual. What is usual is determined by the vendor.
Public Attributes#
Power supply config.
Whether device is a border router.
Whether device supports CCM (can act as a CCM border router).
Operational stability of device (vendor specific).
Weight adjustment. Should be -16 to +16 (clamped otherwise).