Represents an External Route configuration.
Public Attributes#
The IPv6 prefix.
The border router's RLOC16 (value ignored on config add).
A 2-bit signed int preference (OT_ROUTE_PREFERENCE_*
values).
Whether this is a NAT64 prefix.
Whether this configuration is considered Stable Network Data.
Whether the next hop is this device (value ignored on config add).
Whether or not BR is advertising a ULA prefix in PIO (AP flag).
Public Attribute Documentation#
mPrefix#
otIp6Prefix otExternalRouteConfig::mPrefix
The IPv6 prefix.
92
of file include/openthread/netdata.h
mRloc16#
uint16_t otExternalRouteConfig::mRloc16
The border router's RLOC16 (value ignored on config add).
93
of file include/openthread/netdata.h
mPreference#
signed int otExternalRouteConfig::mPreference
A 2-bit signed int preference (OT_ROUTE_PREFERENCE_*
values).
94
of file include/openthread/netdata.h
mNat64#
bool otExternalRouteConfig::mNat64
Whether this is a NAT64 prefix.
95
of file include/openthread/netdata.h
mStable#
bool otExternalRouteConfig::mStable
Whether this configuration is considered Stable Network Data.
96
of file include/openthread/netdata.h
mNextHopIsThisDevice#
bool otExternalRouteConfig::mNextHopIsThisDevice
Whether the next hop is this device (value ignored on config add).
97
of file include/openthread/netdata.h
mAdvPio#
bool otExternalRouteConfig::mAdvPio
Whether or not BR is advertising a ULA prefix in PIO (AP flag).
98
of file include/openthread/netdata.h