Represents a Network Diagnostic TLV.

Public Attribute Documentation#

mType#

uint8_t otNetworkDiagTlv::mType

The Network Diagnostic TLV type.


Definition at line 195 of file include/openthread/netdiag.h

mExtAddress#

otExtAddress otNetworkDiagTlv::mExtAddress

Definition at line 199 of file include/openthread/netdiag.h

mEui64#

otExtAddress otNetworkDiagTlv::mEui64

Definition at line 200 of file include/openthread/netdiag.h

mAddr16#

uint16_t otNetworkDiagTlv::mAddr16

Definition at line 201 of file include/openthread/netdiag.h

mMode#

otLinkModeConfig otNetworkDiagTlv::mMode

Definition at line 202 of file include/openthread/netdiag.h

mTimeout#

uint32_t otNetworkDiagTlv::mTimeout

Definition at line 203 of file include/openthread/netdiag.h

mConnectivity#

otNetworkDiagConnectivity otNetworkDiagTlv::mConnectivity

Definition at line 204 of file include/openthread/netdiag.h

mRoute#

otNetworkDiagRoute otNetworkDiagTlv::mRoute

Definition at line 205 of file include/openthread/netdiag.h

mLeaderData#

otLeaderData otNetworkDiagTlv::mLeaderData

Definition at line 206 of file include/openthread/netdiag.h

mMacCounters#

otNetworkDiagMacCounters otNetworkDiagTlv::mMacCounters

Definition at line 207 of file include/openthread/netdiag.h

mMleCounters#

otNetworkDiagMleCounters otNetworkDiagTlv::mMleCounters

Definition at line 208 of file include/openthread/netdiag.h

mBatteryLevel#

uint8_t otNetworkDiagTlv::mBatteryLevel

Definition at line 209 of file include/openthread/netdiag.h

mSupplyVoltage#

uint16_t otNetworkDiagTlv::mSupplyVoltage

Definition at line 210 of file include/openthread/netdiag.h

mMaxChildTimeout#

uint32_t otNetworkDiagTlv::mMaxChildTimeout

Definition at line 211 of file include/openthread/netdiag.h

mVersion#

uint16_t otNetworkDiagTlv::mVersion

Definition at line 212 of file include/openthread/netdiag.h

mVendorName#

char otNetworkDiagTlv::mVendorName[OT_NETWORK_DIAGNOSTIC_MAX_VENDOR_NAME_TLV_LENGTH+1]

Definition at line 213 of file include/openthread/netdiag.h

mVendorModel#

char otNetworkDiagTlv::mVendorModel[OT_NETWORK_DIAGNOSTIC_MAX_VENDOR_MODEL_TLV_LENGTH+1]

Definition at line 214 of file include/openthread/netdiag.h

mVendorSwVersion#

char otNetworkDiagTlv::mVendorSwVersion[OT_NETWORK_DIAGNOSTIC_MAX_VENDOR_SW_VERSION_TLV_LENGTH+1]

Definition at line 215 of file include/openthread/netdiag.h

mThreadStackVersion#

char otNetworkDiagTlv::mThreadStackVersion[OT_NETWORK_DIAGNOSTIC_MAX_THREAD_STACK_VERSION_TLV_LENGTH+1]

Definition at line 216 of file include/openthread/netdiag.h

mVendorAppUrl#

char otNetworkDiagTlv::mVendorAppUrl[OT_NETWORK_DIAGNOSTIC_MAX_VENDOR_APP_URL_TLV_LENGTH+1]

Definition at line 217 of file include/openthread/netdiag.h

mCount#

uint8_t otNetworkDiagTlv::mCount

Definition at line 220 of file include/openthread/netdiag.h

m8#

uint8_t otNetworkDiagTlv::m8[OT_NETWORK_BASE_TLV_MAX_LENGTH]

Definition at line 221 of file include/openthread/netdiag.h

mNetworkData#

struct otNetworkDiagTlv::@5::@6 otNetworkDiagTlv::mNetworkData

Definition at line 222 of file include/openthread/netdiag.h

mList#

otIp6Address otNetworkDiagTlv::mList[OT_NETWORK_BASE_TLV_MAX_LENGTH/sizeof(otIp6Address)]

Definition at line 226 of file include/openthread/netdiag.h

mIp6AddrList#

struct otNetworkDiagTlv::@5::@7 otNetworkDiagTlv::mIp6AddrList

Definition at line 227 of file include/openthread/netdiag.h

mTable#

otNetworkDiagChildEntry otNetworkDiagTlv::mTable[OT_NETWORK_BASE_TLV_MAX_LENGTH/sizeof(otNetworkDiagChildEntry)]

Definition at line 231 of file include/openthread/netdiag.h

mChildTable#

struct otNetworkDiagTlv::@5::@8 otNetworkDiagTlv::mChildTable

Definition at line 232 of file include/openthread/netdiag.h

mChannelPages#

struct otNetworkDiagTlv::@5::@9 otNetworkDiagTlv::mChannelPages

Definition at line 237 of file include/openthread/netdiag.h

mData#

union otNetworkDiagTlv::@5 otNetworkDiagTlv::mData

Definition at line 238 of file include/openthread/netdiag.h