Alternate PHY configuration entry structure, which gathers some info on the alternate PHY in the context of concurrent mode.
Public Attributes#
uint32_t
A base frequency in Hz of this channel set.
uint32_t
A channel spacing in Hz of this channel set.
uint16_t
The number of channels (and not the channel number !)
uint16_t
minimum IF for the alternate PHY in kHz.
uint16_t
minimum IF for the base PHY in kHz.
bool
Indicates that OFDM modem is used by this alternate PHY.
Public Attribute Documentation#
baseFrequency#
uint32_t RAIL_AlternatePhy_t::baseFrequency
A base frequency in Hz of this channel set.
channelSpacing#
uint32_t RAIL_AlternatePhy_t::channelSpacing
A channel spacing in Hz of this channel set.
numberOfChannels#
uint16_t RAIL_AlternatePhy_t::numberOfChannels
The number of channels (and not the channel number !)
isOfdmModem#
bool RAIL_AlternatePhy_t::isOfdmModem
Indicates that OFDM modem is used by this alternate PHY.