Modules#
RAIL_RxChannelHoppingConfigMultiMode_t
RAIL_RxChannelHoppingConfigEntry_t
RX Channel Hopping#
Hardware accelerated hopping between channels while waiting for a packet in receive.
Channel hopping provides a hardware accelerated method for scanning across multiple channels quickly, as part of a receive protocol. While it is possible to call RAIL_StartRx on different channels, back to back, and listen on many channels sequentially in that way, the time it takes to switch channels with that method may be too long for some protocols. This API pre-computes necessary channel change operations for a given list of channels, so that the radio can move from channel to channel much faster. Additionally, it leads to more succinct code as channel changes will be done implicitly, without requiring numerous calls to RAIL_StartRx. Currently, while this feature is enabled, the radio will hop channels in the given sequence each time it enters RX.
The channel hopping buffer requires RAIL_CHANNEL_HOPPING_BUFFER_SIZE_PER_CHANNEL number of 32-bit words of overhead per channel, plus 3 words overall plus the twice the size of the radioConfigDeltaSubtract of the whole radio configuration, plus the twice the sum of the sizes of all the radioConfigDeltaAdds of all the channel hopping channels.
The following code gives an example of how to use the RX Channel Hopping API.
#define CHANNEL_HOPPING_NUMBER_OF_CHANNELS 4
#define CHANNEL_HOPPING_BUFFER_SIZE do { \
3 + \
(RAIL_CHANNEL_HOPPING_BUFFER_SIZE_PER_CHANNEL \
* CHANNEL_HOPPING_NUMBER_OF_CHANNELS) + \
2 * (SIZEOF_UINT32_DELTA_SUBTRACT + \
SIZEOF_UINT32_DELTA_ADD_0 + \
SIZEOF_UINT32_DELTA_ADD_1 + \
SIZEOF_UINT32_DELTA_ADD_2 + \
SIZEOF_UINT32_DELTA_ADD_3) \
} while (0)
RAIL_RxChannelHoppingConfigEntry_t channelHoppingEntries[CHANNEL_HOPPING_NUMBER_OF_CHANNELS];
uint32_t channelHoppingBuffer[CHANNEL_HOPPING_BUFFER_SIZE];
RAIL_RxChannelHoppingConfig_t channelHoppingConfig = {
.buffer = channelHoppingBuffer,
.bufferLength = CHANNEL_HOPPING_BUFFER_SIZE,
.numberOfChannels = CHANNEL_HOPPING_NUMBER_OF_CHANNELS,
.entries = channelHoppingEntries
};
channelHoppingEntries[0].channel = 1;
channelHoppingEntries[1].channel = 2;
channelHoppingEntries[2].channel = 3;
RAIL_ConfigRxChannelHopping(railHandle, &channelHoppingConfig);
RAIL_EnableRxChannelHopping(railHandle, true, true)
Enumerations#
Modes by which RAIL can determine when to proceed to the next channel during channel hopping.
Options that can customize channel hopping behavior on a per-hop basis.
Typedefs#
Rx channel hopping on-channel time.
Functions#
Configure RX Channel Hopping.
Enable RX channel hopping.
Get RSSI of one channel in the channel hopping sequence, during channel hopping.
Configure RX duty cycle mode.
Enable RX duty cycle mode.
Get the default RX duty cycle configuration.
Macros#
The maximum sense time supported for those RAIL_RxChannelHoppingMode_t modes whose parameter(s) specify a sensing time.
A value representing no options enabled.
All options disabled by default.
DeprecatedPlease use RAIL_RX_CHANNEL_HOPPING_OPTIONS_DEFAULT instead.
An option to skip synth calibration while hopping into the channel specified in the current entry.
An option to skip DC calibration while hopping into the channel specified in the current entry.
An option to check RSSI after hopping into the channel specified in the current entry and hop if that RSSI is below the threshold specified in RAIL_RxChannelHoppingConfigEntry_t::rssiThresholdDbm.
An option to stop the hopping sequence at this entry in the hop table.
A sentinel value to flag an invalid channel hopping index.
The static amount of memory needed per channel for channel hopping, measured in 32 bit words, regardless of the size of radio configuration structures.
Enumeration Documentation#
RAIL_RxChannelHoppingMode_t#
RAIL_RxChannelHoppingMode_t
Modes by which RAIL can determine when to proceed to the next channel during channel hopping.
| Enumerator | |
|---|---|
| RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL | Switch to the next channel each time the radio enters RX. |
| RAIL_RX_CHANNEL_HOPPING_MODE_TIMEOUT | Switch to the next channel after a certain amount of time passes. |
| RAIL_RX_CHANNEL_HOPPING_MODE_TIMING_SENSE | Listen in receive RX for at least a specified timeout. |
| RAIL_RX_CHANNEL_HOPPING_MODE_PREAMBLE_SENSE | Listen in receive RX for at least a specified timeout. |
| RAIL_RX_CHANNEL_HOPPING_MODE_RESERVED1 | Placeholder for a reserved hopping mode that is not supported. |
| RAIL_RX_CHANNEL_HOPPING_MODE_MULTI_SENSE | A mode that combines modes TIMING_SENSE, PREAMBLE_SENSE, and TIMEOUT (sync detect) all running in parallel. |
| RAIL_RX_CHANNEL_HOPPING_MODE_SQ | Switch to the next channel based on the demodulation settings in the PHY config. |
| RAIL_RX_CHANNEL_HOPPING_MODE_CONC | Marks that the channel is concurrent with another channel, and otherwise behaves identically to RAIL_RX_CHANNEL_HOPPING_MODE_SQ. |
| RAIL_RX_CHANNEL_HOPPING_MODE_VT | Indicates that this channel is a virtual channel that is concurrently detected with the channel indicated by the RAIL_RxChannelHoppingConfigEntry_t::parameter. |
| RAIL_RX_CHANNEL_HOPPING_MODE_TX | This is the transmit channel used for auto-ACK if the regular channel, specified in RAIL_RxChannelHoppingConfigEntry::parameter, is optimized for RX which may degrade some TX performance. |
| RAIL_RX_CHANNEL_HOPPING_MODES_COUNT | A count of the basic choices in this enumeration. |
| RAIL_RX_CHANNEL_HOPPING_MODES_WITH_OPTIONS_BASE | The start of equivalent modes requiring non-default RAIL_RxDutyCycleConfig_t::options, needed for backwards-compatibility with earlier RAIL_RxDutyCycleConfig_t format. |
| RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_TIMEOUT_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_TIMEOUT with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_TIMING_SENSE_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_TIMING_SENSE with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_PREAMBLE_SENSE_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_PREAMBLE_SENSE with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_RESERVED1_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_RESERVED1 with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_MULTI_SENSE_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_MULTI_SENSE with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_SQ_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_SQ with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_CONC_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_CONC with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_VT_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_VT with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_TX_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_TX with options. |
RAIL_RxChannelHoppingDelayMode_t#
RAIL_RxChannelHoppingDelayMode_t
DeprecatedSet only to RAIL_RX_CHANNEL_DELAY_MODE_STATIC
| Enumerator | |
|---|---|
| RAIL_RX_CHANNEL_HOPPING_DELAY_MODE_STATIC | Always delay for exactly the amount of time specified in the delay parameter, regardless of how other channel hopping channels were extended via preamble sense or other means. |
RAIL_RxChannelHoppingOptions_t#
RAIL_RxChannelHoppingOptions_t
Options that can customize channel hopping behavior on a per-hop basis.
| Enumerator | |
|---|---|
| RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_SYNTH_CAL_SHIFT | Shift position of RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_SYNTH_CAL bit. |
| RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_DC_CAL_SHIFT | Shift position of RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_DC_CAL bit. |
| RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD_SHIFT | Shift position of RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD bit. |
| RAIL_RX_CHANNEL_HOPPING_OPTION_STOP_SHIFT | Stop hopping on this hop. |
| RAIL_RX_CHANNEL_HOPPING_OPTIONS_COUNT | A count of the choices in this enumeration. |
Typedef Documentation#
RAIL_RxChannelHoppingParameter_t#
RAIL_RxChannelHoppingParameter_t
Rx channel hopping on-channel time.
Function Documentation#
RAIL_ConfigRxChannelHopping#
RAIL_Status_t RAIL_ConfigRxChannelHopping (RAIL_Handle_t railHandle, RAIL_RxChannelHoppingConfig_t * config)
Configure RX Channel Hopping.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| RAIL_RxChannelHoppingConfig_t * | [in] | config | Configuration parameters for RX Channel Hopping. |
Returns
Status code indicating success of the function call.
Configure Channel Hopping channels, conditions, and parameters. This API must be called before RAIL_EnableRxChannelHopping(). This API must never be called while the radio is on with RX Duty Cycle or Channel Hopping enabled.
Note
This feature/API is not supported on the EFR32XG1 family of chips. Use the compile time symbol RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call RAIL_SupportsChannelHopping() to check whether the platform supports this feature.
Calling this function will overwrite any settings configured with RAIL_ConfigRxDutyCycle.
RAIL_EnableRxChannelHopping#
RAIL_Status_t RAIL_EnableRxChannelHopping (RAIL_Handle_t railHandle, bool enable, bool reset)
Enable RX channel hopping.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| bool | [in] | enable | Enable (true) or disable (false) RX Channel Hopping. |
| bool | [in] | reset | Start from the first channel of the channel hopping sequence (true) or from wherever hopping left off last time the code left RX. |
Returns
Status code indicating success of the function call.
Enable or disable Channel Hopping. Additionally, specify whether hopping should be reset to start from the channel at index zero, or continue from the channel last hopped to. The radio should not be on when this API is called. RAIL_ConfigRxChannelHopping must be called successfully before this API is called.
Note
This feature/API is not supported on the EFR32XG1 family of chips. Use the compile time symbol RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call RAIL_SupportsChannelHopping() to check whether the platform supports this feature.
RX Channel Hopping may not be enabled while auto-ACKing is enabled.
Calling this function will overwrite any settings configured with RAIL_EnableRxDutyCycle.
RAIL_GetChannelHoppingRssi#
int16_t RAIL_GetChannelHoppingRssi (RAIL_Handle_t railHandle, uint8_t channelIndex)
Get RSSI of one channel in the channel hopping sequence, during channel hopping.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| uint8_t | [in] | channelIndex | Index in the channel hopping sequence of the channel of interest |
Returns
Latest RSSI for the channel at the specified index.
Note
This feature/API is not supported on the EFR32XG1 family of chips. Use the compile time symbol RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call RAIL_SupportsChannelHopping() to check whether the platform supports this feature.
In multiprotocol, this function returns RAIL_RSSI_INVALID immediately if railHandle is not the current active RAIL_Handle_t.
RAIL_ConfigRxChannelHopping must be called successfully before this API is called.
When the Z-Wave protocol is active, it is expected that after RAIL_ConfigRxChannelHopping is called successfully on EFR32XG1 family of chips, running RAIL_GetChannelHoppingRssi() on a 40kbps PHY will not work well. Plan to use the 9.6kbps PHY for estimating channel noise instead. On EFR32XG2 family of chips, running RAIL_GetChannelHoppingRssi() on the 9.6kbps PHY returns the RSSI measurement of the 40kpbs PHY. This is because the 9.6kbps PHY has trouble with RSSI measurements on EFR32XG2 family of chips.
RAIL_ConfigRxDutyCycle#
RAIL_Status_t RAIL_ConfigRxDutyCycle (RAIL_Handle_t railHandle, const RAIL_RxDutyCycleConfig_t * config)
Configure RX duty cycle mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| const RAIL_RxDutyCycleConfig_t * | [in] | config | Configuration structure to specify duty cycle parameters. |
Returns
Status code indicating success of the function call.
Configure RX duty cycle mode. With this mode enabled, every time the radio enters RX, it will duty cycle on and off to save power. The duty cycle ratio can be altered dynamically and intelligently by the hardware by staying on longer if a preamble or other packet segments are detected in the air. This API must never be called while the radio is on with RX Duty Cycle or Channel Hopping enabled. For short delays (in the order of microseconds), RAIL_RxDutyCycleConfig_t::delay, this can be used to save receive current while having little impact on the radio performance, for protocols with long preambles. For long delays (in the order of milliseconds or higher) the chip can be put into EM2 energy mode before re-entering RX, to save extra power, with some application hooks as shown below.
#include <rail.h>
#include <rail_types.h>
extern RAIL_Handle_t railHandle;
RAIL_Time_t periodicWakeupUs;
void RAILCb_Event(RAIL_Handle_t railHandle, RAIL_Events_t events) {
// Omitting other event handlers
if (events & RAIL_EVENT_RX_DUTY_CYCLE_RX_END) {
// Schedule the next receive.
RAIL_ScheduleRxConfig_t rxCfg = {
.start = periodicWakeupUs,
.startMode = RAIL_TIME_DELAY,
.end = 0U,
.endMode = RAIL_TIME_DISABLED,
.rxTransitionEndSchedule = 0U,
.hardWindowEnd = 0U
};
RAIL_Idle(railHandle, RAIL_IDLE_ABORT, true);
RAIL_ScheduleRx(railHandle, channel, &rxCfg, NULL);
}
}
void main(void) {
RAIL_Status_t status;
bool shouldSleep = false;
// This function depends on your board/chip but it must enable the LFCLK
// you intend to use for RTCC sync before we configure sleep as that
// function will attempt to auto detect the clock.
BoardSetupLFCLK();
// Initialize Power Manager module
sl_power_manager_init();
// Initialize RAIL Power Manager
RAIL_InitPowerManager();
// Configure sleep for timer synchronization
status = RAIL_ConfigSleep(railHandle, RAIL_SLEEP_CONFIG_TIMERSYNC_ENABLED);
assert(status == RAIL_STATUS_NO_ERROR);
// Application main loop
while(1) {
// ... do normal app stuff and set shouldSleep when we want to sleep
if (shouldSleep) {
// Let the CPU go to sleep if the system allows it.
sl_power_manager_sleep();
}
}
}
Note
This feature/API is not supported on the EFR32XG1 family of chips. Use the compile time symbol RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call RAIL_SupportsChannelHopping() to check whether the platform supports this feature.
Calling this function will overwrite any settings configured with RAIL_ConfigRxChannelHopping.
RAIL_EnableRxDutyCycle#
RAIL_Status_t RAIL_EnableRxDutyCycle (RAIL_Handle_t railHandle, bool enable)
Enable RX duty cycle mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| bool | [in] | enable | Enable (true) or disable (false) RX Duty Cycling. |
Returns
Status code indicating success of the function call.
Enable or disable RX duty cycle mode. After this is called, the radio will begin duty cycling each time it enters RX, based on the configuration passed to RAIL_ConfigRxDutyCycle. This API must not be called while the radio is on.
Note
This feature/API is not supported on the EFR32XG1 family of chips. Use the compile time symbol RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call RAIL_SupportsChannelHopping() to check whether the platform supports this feature.
Calling this function will overwrite any settings configured with RAIL_EnableRxChannelHopping.
RAIL_GetDefaultRxDutyCycleConfig#
RAIL_Status_t RAIL_GetDefaultRxDutyCycleConfig (RAIL_Handle_t railHandle, RAIL_RxDutyCycleConfig_t * config)
Get the default RX duty cycle configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| RAIL_RxDutyCycleConfig_t * | [out] | config | An application-provided non-NULL pointer to store the default RX duty cycle configuration. |
Returns
Status code indicating success of the function call. Note that RAIL_STATUS_INVALID_PARAMETER will be returned if the current channel's radio configuration does not support the requested information.
To save power during RX, an application may want to go to low power as long as possible by periodically waking up and trying to "sense" if there are any incoming packets. This API returns the recommended RX duty cycle configuration, so the application can enter low power mode periodically without missing packets. To wake up earlier, the application can reduce the delay parameter. Note that these value might be different if any configuration / channel has changed.