Structure that parameterizes RAIL_RX_CHANNEL_HOPPING_MODE_MULTI_SENSE.
Every RAIL_RxChannelHoppingConfigEntry_t or RAIL_RxDutyCycleConfig_t that uses RAIL_RX_CHANNEL_HOPPING_MODE_MULTI_SENSE must allocate one of these structures in global read-write memory to provide the settings for this mode and for RAIL to use during hopping or duty cycling. A pointer to this structure, cast appropriately, is what is passed in the corresponding RAIL_RxChannelHoppingConfigEntry_t::parameter or RAIL_RxDutyCycleConfig_t::parameter.
The contents of this structure must be initialized prior to each RAIL_ConfigRxChannelHopping() or RAIL_ConfigRxDutyCycle() call and must not be touched thereafter until the next such call. RAIL may change these contents during configuration or operation.
This mode of operation functions algorithmically like this pseudocode:
extern bool channelHopping; // true if channel hopping, false if duty cycling
extern RAIL_RxChannelHoppingConfigEntry_t *hopConfigEntry; // current channel
static RAIL_RxChannelHoppingConfigMultiMode_t *multiParams;
static RAIL_Time_t rxStartTime;
static bool preambleSensed;
static void hopOrSuspendRx(uint32_t delay)
{
disableDemodEvents();
disableTimerEvents();
stopTimer();
if (channelHopping) {
hopToNextChannel(delay, &hopConfigEntry); // updates hopConfigEntry
} else {
suspendRx(delay);
}
onStartRx(); // resume receive after delay (on new channel if hopping)
}
void onStartRx(void) // called upon entry to receive
{
rxStartTime = RAIL_GetTime();
multiParams = (RAIL_RxChannelHoppingConfigMultiMode_t *)
(void *)hopConfigEntry->parameter;
startTimer(rxStartTime + multiParams->timingSense);
preambleSensed = false;
enableTimerEvents(); // timer will trigger onTimerEvent() handler
enableDemodEvents(); // demod will trigger onDemodEvent() handler
}
void onTimerEvent(void) // called when timer expires
{
hopOrSuspendRx(hopConfigEntry->delay);
}
void onDemodEvent(void) // called when demodulator state changes
{
if (DEMOD_TIMING_SENSED) {
stopTimer();
startTimer(rxStartTime + multiParams->syncDetect);
}
if (DEMOD_TIMING_LOST) {
stopTimer();
uint32_t newTimeout = RAIL_GetTime() + multiParams->timingReSense;
uint32_t limitTimeout;
if (preambleSensed) {
limitTimeout = rxStartTime + multiParams->syncDetect;
} else {
limitTimeout = rxStartTime + multiParams->preambleSense;
}
if (newTimeout > limitTimeout) {
newTimeout = limitTimeout;
}
if (newTimeout > RAIL_GetTime()) {
startTimer(newTimeout);
} else {
hopOrSuspendRx(hopConfigEntry->delay);
}
}
if (DEMOD_PREAMBLE_SENSED) {
preambleSensed = true;
}
if (DEMOD_PREAMBLE_LOST) {
preambleSensed = false;
}
if (DEMOD_SYNC_DETECTED) {
disableDemodEvents();
disableTimerEvents();
stopTimer();
receivePacket(); // stay on channel to receive frame
hopOrSuspendRx(0); // continue RX per state transitions with no delay
}
}
Public Attributes#
Switch to the next channel if sync is not detected before this time, in microseconds, measured from entry to Rx.
Switch to the next channel if timing was sensed but then lost after this time, in microseconds, measured from entry to Rx – unless preamble had been sensed in which case any switching is deferred to timingReSense and, if timing is regained, to syncDetect.
Switch to the next channel if timing is not sensed before this time, in microseconds, measured from entry to Rx.
Switch to the next channel if timing was sensed but then lost and not regained before this time, in microseconds, measured from when timing was lost.
Set this to 0.
Public Attribute Documentation#
syncDetect#
uint32_t RAIL_RxChannelHoppingConfigMultiMode_t::syncDetect
Switch to the next channel if sync is not detected before this time, in microseconds, measured from entry to Rx.
This must be greater than preambleSense and less than RAIL_RX_CHANNEL_HOPPING_MAX_SENSE_TIME_US.
4177
of file common/rail_types.h
preambleSense#
uint32_t RAIL_RxChannelHoppingConfigMultiMode_t::preambleSense
Switch to the next channel if timing was sensed but then lost after this time, in microseconds, measured from entry to Rx – unless preamble had been sensed in which case any switching is deferred to timingReSense and, if timing is regained, to syncDetect.
This must be greater than timingSense and less than RAIL_RX_CHANNEL_HOPPING_MAX_SENSE_TIME_US.
4186
of file common/rail_types.h
timingSense#
uint32_t RAIL_RxChannelHoppingConfigMultiMode_t::timingSense
Switch to the next channel if timing is not sensed before this time, in microseconds, measured from entry to Rx.
This must be greater than 2 and less than RAIL_RX_CHANNEL_HOPPING_MAX_SENSE_TIME_US.
4193
of file common/rail_types.h
timingReSense#
uint32_t RAIL_RxChannelHoppingConfigMultiMode_t::timingReSense
Switch to the next channel if timing was sensed but then lost and not regained before this time, in microseconds, measured from when timing was lost.
This must be less than RAIL_RX_CHANNEL_HOPPING_MAX_SENSE_TIME_US.
4200
of file common/rail_types.h
status#
uint32_t RAIL_RxChannelHoppingConfigMultiMode_t::status
Set this to 0.
This field, along with the others, may be used internally by RAIL during configuration or operation.
4205
of file common/rail_types.h