Wrapper struct that will contain the sequence of RAIL_RxChannelHoppingConfigEntry_t that represents the channel sequence to use during RX Channel Hopping.
Public Attributes#
Pointer to contiguous global read-write memory that will be used by RAIL to store channel hopping information throughout its operation.
This parameter must be set to the length of the buffer array, in 32 bit words.
The number of channels in the channel hopping sequence, which is the number of elements in the array that entries points to.
A pointer to the first element of an array of RAIL_RxChannelHoppingConfigEntry_t that represents the channels used during channel hopping.
Public Attribute Documentation#
buffer#
uint32_t* RAIL_RxChannelHoppingConfig_t::buffer
Pointer to contiguous global read-write memory that will be used by RAIL to store channel hopping information throughout its operation.
It need not be initialized and applications should never write data anywhere in this buffer.
Note
the size of this buffer must be at least as large as 3 + 30 * numberOfChannels, plus the sum of the sizes of the radioConfigDeltaAdd's of the required channels, plus the size of the radioConfigDeltaSubtract. In the case that one channel appears two or more times in your channel sequence (e.g., 1, 2, 1, 3), you must account for the radio configuration size that number of times (i.e., need to count channel 1's radio configuration size twice for the given example). The overall 3 words and 30 words per channel needed in this buffer are for internal use to the library.
4278
of file common/rail_types.h
bufferLength#
uint16_t RAIL_RxChannelHoppingConfig_t::bufferLength
This parameter must be set to the length of the buffer array, in 32 bit words.
This way, during configuration, the software can confirm it's writing within the range of the buffer. The configuration API will return an error if bufferLength is insufficient.
4285
of file common/rail_types.h
numberOfChannels#
uint8_t RAIL_RxChannelHoppingConfig_t::numberOfChannels
The number of channels in the channel hopping sequence, which is the number of elements in the array that entries points to.
4290
of file common/rail_types.h
entries#
RAIL_RxChannelHoppingConfigEntry_t* RAIL_RxChannelHoppingConfig_t::entries
A pointer to the first element of an array of RAIL_RxChannelHoppingConfigEntry_t that represents the channels used during channel hopping.
The length of this array must be numberOfChannels.
4297
of file common/rail_types.h